<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic android hangs in open_devnull_stdio() ( inside init) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210280#M12500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a imx6q based hardware ) .I am trying to port&amp;nbsp; android on it. I am using&amp;nbsp; freescale r13.3&amp;nbsp; android .&lt;/P&gt;&lt;P&gt;With NFS its works fine..&lt;/P&gt;&lt;P&gt;But booting from SD cards fails.After digging through init code I found it hangs in side&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;open_devnull_stdio().. function at&amp;nbsp; dup2(fd,1);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see bootargs below,&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc0 , 115200 init=/init rw video=mxcfb0&amp;nbsp; fbmem=5M vmalloc=400M root=/dev/mmcblk0p4 androidboot.console=ttymxc0 ..&lt;/P&gt;&lt;P&gt;( Using UART1 for debugging )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please help me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Oct 2012 05:58:00 GMT</pubDate>
    <dc:creator>VAISAKH</dc:creator>
    <dc:date>2012-10-05T05:58:00Z</dc:date>
    <item>
      <title>android hangs in open_devnull_stdio() ( inside init)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210280#M12500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a imx6q based hardware ) .I am trying to port&amp;nbsp; android on it. I am using&amp;nbsp; freescale r13.3&amp;nbsp; android .&lt;/P&gt;&lt;P&gt;With NFS its works fine..&lt;/P&gt;&lt;P&gt;But booting from SD cards fails.After digging through init code I found it hangs in side&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;open_devnull_stdio().. function at&amp;nbsp; dup2(fd,1);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see bootargs below,&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc0 , 115200 init=/init rw video=mxcfb0&amp;nbsp; fbmem=5M vmalloc=400M root=/dev/mmcblk0p4 androidboot.console=ttymxc0 ..&lt;/P&gt;&lt;P&gt;( Using UART1 for debugging )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please help me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Oct 2012 05:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210280#M12500</guid>
      <dc:creator>VAISAKH</dc:creator>
      <dc:date>2012-10-05T05:58:00Z</dc:date>
    </item>
    <item>
      <title>Re: android hangs in open_devnull_stdio() ( inside init)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210281#M12501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anybody,Please help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Oct 2012 08:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210281#M12501</guid>
      <dc:creator>VAISAKH</dc:creator>
      <dc:date>2012-10-07T08:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: android hangs in open_devnull_stdio() ( inside init)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210282#M12502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you prove full log and memory size? And you can also try to decrease vmalloc=xxx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2012 03:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210282#M12502</guid>
      <dc:creator>RichardZhao</dc:creator>
      <dc:date>2012-10-08T03:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: android hangs in open_devnull_stdio() ( inside init)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210283#M12503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks for the reply.I have tried&amp;nbsp; with&amp;nbsp; the vmalloc = 128 and 64 M but hanged at the same place .)&lt;/P&gt;&lt;P&gt;Please see my logs attached with this post&lt;/P&gt;&lt;P&gt;Memory is 2GB ....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With thanks&lt;/P&gt;&lt;P&gt;Vaisakh N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2012 03:59:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210283#M12503</guid>
      <dc:creator>VAISAKH</dc:creator>
      <dc:date>2012-10-08T03:59:29Z</dc:date>
    </item>
    <item>
      <title>Re: android hangs in open_devnull_stdio() ( inside init)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210284#M12504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Hi Vaisakh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;In reviewing your kernel boot arguments, I don't know if you have provided the complete set, but I would suggest removing the 'root=/dev/mmcblk0p4' option.&amp;nbsp; This is not necessary to explicitly define the root file system since the root file system is a composite of the RAM disk and mounted file systems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;If the above suggestion does not work, it would also be helpful to attach the output of the console when the kernel boots.&amp;nbsp; This would provide the entire kernel command line and potential insight into what might be happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;On a side note, we are moving away from supporting R13.3 release for i.MX 6 since the supported release is the R13.4 GA release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 02:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-hangs-in-open-devnull-stdio-inside-init/m-p/210284#M12504</guid>
      <dc:creator>imxcommunitysco</dc:creator>
      <dc:date>2012-10-26T02:42:26Z</dc:date>
    </item>
  </channel>
</rss>