<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810335#M124953</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at sect.4 Run a demo application using IAR, sect.5 Run a demo using ARM® GCC&lt;/P&gt;&lt;P&gt;attached Getting Started with MCUXpresso SDK document from this package.&lt;/P&gt;&lt;P&gt;I am afraid direct link is not available as package is built&lt;/P&gt;&lt;P&gt;when customer press "Download SDK" button.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 30 Sep 2018 13:29:08 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-30T13:29:08Z</dc:date>
    <item>
      <title>Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810332#M124950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to determine if the i.MX 8MQ is suitable for our needs which involve streaming video from two MIPI CSI cameras to an HDMI output.&amp;nbsp; The MCIMX8M-EVK evaluation kit seems to suit this purpose nicely, with dual CSI inputs and "out of the box" HDMI output (at least with the default pre-built Android software). There is also an available MIPI-CSI camera module from NXP (MINISASOCSI).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I have downloaded the sample code for the EVK and I don't see any CSI example code (perhaps I overlooked it or it is a separate download).&amp;nbsp; Also, it seems this processor/board is not supported by MCUXpresso, so I will have to either build a development environment around ARM GCC or purchase IAR Embedded Workbench.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there example code to go from MIPI-CSI to HDMI with the MCIMX8M-EVK?&amp;nbsp; If so, where?&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Is there a better evaluation kit option from NXP for this purpose?&amp;nbsp; (Perhaps one that is supported by MCUXpresso.)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 20:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810332#M124950</guid>
      <dc:creator>jstewart1</dc:creator>
      <dc:date>2018-09-28T20:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810333#M124951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is MCUXpresso ("SDK 2.3 for i.MX 8MQuad GA") for i.MX8M EVK on below link,&lt;/P&gt;&lt;P&gt;but seems such examples are available only in linux. Except EVK there are no other i.MX8M&lt;/P&gt;&lt;P&gt;NXP reference designs.&lt;/P&gt;&lt;P&gt;Linux example codes are described in linux documentation package ("Linux L4.9.51 8MQuad GA Documentation")&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;May be useful to look on third party designs&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/product/nitrogen8m-imx8/" title="https://boundarydevices.com/product/nitrogen8m-imx8/"&gt;Nitrogen8M - An NXP i.MX8 M Single Board Computer Platform&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 23:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810333#M124951</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-28T23:48:00Z</dc:date>
    </item>
    <item>
      <title>Re: Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810334#M124952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I've chased that link before:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SDK23forIMX screen cap.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73631i9F6EDECC0F2FB9A5/image-size/large?v=v2&amp;amp;px=999" role="button" title="SDK23forIMX screen cap.PNG" alt="SDK23forIMX screen cap.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The link does NOT go directly to the file I was never able to find that file. I can eventually get a link that indicates "Build MCUXpresso SDK":&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NXP build mcuxpresso.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73721iA140381BC5FF49B6/image-size/large?v=v2&amp;amp;px=999" role="button" title="NXP build mcuxpresso.PNG" alt="NXP build mcuxpresso.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you click on the link, the only options are for GCC ARM and IAR Embedded Workbench, not for MCUXpresso IDE [edit, originally wrote MCUXpresso SDK]:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NXP build mcuxpresso GCC or IAR.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73859iE610B22C8313D211/image-size/large?v=v2&amp;amp;px=999" role="button" title="NXP build mcuxpresso GCC or IAR.PNG" alt="NXP build mcuxpresso GCC or IAR.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the referenced file "&lt;SPAN style="color: #6f6f73; background-color: #ffffff; font-size: 16px;"&gt;SDK 2.3 for i.MX 8MQuad GA."&lt;/SPAN&gt;&amp;nbsp;does exist, can you provide a direct link to it?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2018 01:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810334#M124952</guid>
      <dc:creator>jstewart1</dc:creator>
      <dc:date>2018-09-29T01:12:17Z</dc:date>
    </item>
    <item>
      <title>Re: Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810335#M124953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at sect.4 Run a demo application using IAR, sect.5 Run a demo using ARM® GCC&lt;/P&gt;&lt;P&gt;attached Getting Started with MCUXpresso SDK document from this package.&lt;/P&gt;&lt;P&gt;I am afraid direct link is not available as package is built&lt;/P&gt;&lt;P&gt;when customer press "Download SDK" button.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Sep 2018 13:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810335#M124953</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-30T13:29:08Z</dc:date>
    </item>
    <item>
      <title>Re: Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810336#M124954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&amp;nbsp; The MCUXpresso naming convention is confusing as is some of the text on the website.&amp;nbsp; The natural assumption is that the MCUXpresso SDK would work with the MCUXpresso IDE and I thought you were trying to tell me that there is a MCUXpresso SDK for this part that works with the MCUXpresso IDE.&amp;nbsp; I understand now you were referring me to the MCUXpresso SDK for use with the ARM GCC compiler or with IAR Embedded Workbench.&amp;nbsp; I had already downloaded the SDK for this EVK on the ARM GCC compiler (although the filename I received is "SDK_2.3.0_EVK-MIMX8MQ.zip").&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Back to my original questions:&lt;/P&gt;&lt;UL style="color: #51626f; background-color: #ffffff; border: 0px; padding: 0px 0px 0px 30px;"&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0.5ex 0px;"&gt;Is there example code to go from MIPI-CSI to HDMI with the MCIMX8M-EVK?&amp;nbsp; If so, where? (i.e., what specific example code within the SDK as I don't see that any of the examples specifically list this capability.&amp;nbsp; However, since NXP specifically sells a CSI camera board just for this&amp;nbsp;EVK, I assume there must be example code somewhere.)&lt;BR /&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 16:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810336#M124954</guid>
      <dc:creator>jstewart1</dc:creator>
      <dc:date>2018-10-01T16:42:10Z</dc:date>
    </item>
    <item>
      <title>Re: Fast path from MIPI CSI to HDMI using MCIMX8M-EVK?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810337#M124955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think I found a partial answer to my question in this application note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12187.pdf" title="https://www.nxp.com/docs/en/application-note/AN12187.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12187.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[It is perplexing why this application note is&amp;nbsp;NOT linked from the product page it is about: &lt;A href="https://www.nxp.com/part/MINISASTOCSI" title="https://www.nxp.com/part/MINISASTOCSI"&gt;MINISASTOCSI Product Information|NXP&lt;/A&gt;&amp;nbsp;.&amp;nbsp; You might contact your webmaster to&amp;nbsp;link this important application note to the product page.]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 19:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-path-from-MIPI-CSI-to-HDMI-using-MCIMX8M-EVK/m-p/810337#M124955</guid>
      <dc:creator>jstewart1</dc:creator>
      <dc:date>2018-10-01T19:01:05Z</dc:date>
    </item>
  </channel>
</rss>