<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8 gpu crash when playing video</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810200#M124943</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There must be a memory leak somewhere, Do this happens with video only?&lt;/P&gt;&lt;P&gt;Did you try to change the gpu memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Oct 2018 18:17:08 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-10-01T18:17:08Z</dc:date>
    <item>
      <title>imx8 gpu crash when playing video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810199#M124942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&amp;nbsp; anyone:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I face a problem of gpu crash when playing video (the testing video is 1080p ,hdmi output).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;platform: mx8mq ,&amp;nbsp;fsl-yocto-L4.9.51_mx8mq-ga (xwaylan).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the&amp;nbsp;phenomenon happens about every one hour, at most time it had no log, just system hang up quietly .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;here is part log(complete log in the attachment):&lt;/P&gt;&lt;P&gt;====== AIUR: 4.3.4 build on Aug 23 2018 15:19:16. ======&lt;BR /&gt; Core: MPEG4PARSER_06.13.06 build on Feb 6 2018 07:43:39&lt;BR /&gt; file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2&lt;BR /&gt;------------------------&lt;BR /&gt; Track 00 [video_0] Enabled&lt;BR /&gt; Duration: 0:01:00.143411000&lt;BR /&gt; Language: eng&lt;BR /&gt; Mime:&lt;BR /&gt; video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1920, height=(int)1080, framerate=(fraction)24000/1001, codec_data=(buffer)014d0033ffe10031674d4033965280f0044fcb80b4400000fa40002ee03840000f03c0001b775fc638c20000781e0000dbbafe31c3b430632c01000568e9093520 &lt;BR /&gt;------------------------&lt;BR /&gt;====== VPUDEC: 4.3.4 build on Aug 23 2018 15:19:29. ======&lt;BR /&gt; wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Aug 23 2018 14:27:18)&lt;BR /&gt; vpulib: 1.1.1&lt;BR /&gt; firmware: 1.1.1.65535&lt;BR /&gt;------------------------&lt;BR /&gt; Track 01 [audio_0] Enabled&lt;BR /&gt; Duration: 0:01:00.186122000&lt;BR /&gt; Language: eng&lt;BR /&gt; Mime:&lt;BR /&gt; audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)61615, stream-format=(string)raw, codec_data=(buffer)12100000 &lt;BR /&gt;------------------------&lt;BR /&gt;[12926.162132] function:imx_hifi_hw_params line:85 params_rate(params):44100 &lt;BR /&gt;[12926.169197] sample_rate:44100 sample_format:2 &lt;BR /&gt;[12926.175787] function:imx_hifi_hw_params line:120 priv-&amp;gt;clk_frequency :24576000 &lt;BR /&gt;[12926.183453] rt5640 0-001c: bclk is 1411200Hz and lrck is 44100Hz&lt;BR /&gt;[12926.189478] rt5640 0-001c: bclk_ms is 0 and pre_div is 1 for iis 0&lt;/P&gt;&lt;P&gt;====== BEEP: 4.3.4 build on Aug 23 2018 15:19:21. ======&lt;BR /&gt; Core: AAC decoder Wrapper build on Dec 7 2017 18:13:51&lt;BR /&gt; file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm_elinux.so.3&lt;BR /&gt;CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.09.00_ARMV8 build on Sep 20 2017 15:02:50.&lt;BR /&gt;Redistribute latency...&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;New clock: GstAudioSinkClock&lt;BR /&gt;Got EOS from element "playbin0".&lt;BR /&gt;Execution ended after 0:00:55.297515425&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;Setting pipeline to READY ...&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Freeing pipeline ...&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;[13009.799393] **************************&lt;BR /&gt;[13009.803159] *** GPU DRV CONFIG ***&lt;BR /&gt;[13009.807159] **************************&lt;BR /&gt;[13009.811072] Galcore version 6.2.4.150331&lt;BR /&gt;[13009.815103] Galcore options:&lt;BR /&gt;[13009.818113] irqLine = 49&lt;BR /&gt;[13009.821759] registerMemBase = 0x38000000&lt;BR /&gt;[13009.826102] registerMemSize = 0x00040000&lt;BR /&gt;[13009.830440] contiguousSize = 0x08000000&lt;BR /&gt;[13009.834781] contiguousBase = 0x00000000&lt;BR /&gt;[13009.839120] externalSize = 0x00000000&lt;BR /&gt;[13009.843463] externalBase = 0x00000000&lt;BR /&gt;[13009.847802] bankSize = 0x00000000&lt;BR /&gt;[13009.852143] fastClear = -1&lt;BR /&gt;[13009.855788] compression = 13&lt;BR /&gt;[13009.859434] signal = 48&lt;BR /&gt;[13009.863010] powerManagement = 1&lt;BR /&gt;[13009.866582] baseAddress = 0x40000000&lt;BR /&gt;[13009.871058] physSize = 0xC0000000&lt;BR /&gt;[13009.875419] logFileSize = 0 KB &lt;BR /&gt;[13009.879270] recovery = 0&lt;BR /&gt;[13009.882843] stuckDump = 0&lt;BR /&gt;[13009.886412] gpuProfiler = 0&lt;BR /&gt;[13009.889991] irqs = [13009.893289] -1, &lt;BR /&gt;-1, [13009.895561] -1, &lt;BR /&gt;-1, [13009.897763] -1, &lt;BR /&gt;-1, [13009.900032] -1, &lt;BR /&gt;-1, [13009.902233] -1,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2018 02:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810199#M124942</guid>
      <dc:creator>jiangyaqiang</dc:creator>
      <dc:date>2018-09-29T02:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 gpu crash when playing video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810200#M124943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There must be a memory leak somewhere, Do this happens with video only?&lt;/P&gt;&lt;P&gt;Did you try to change the gpu memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 18:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810200#M124943</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-10-01T18:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 gpu crash when playing video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810201#M124944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Bio:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, currently , it happened only when playing video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GPU memory ? you means CMA size ? I did change it, but it happened again(It did could not duplicate less). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The device DDR is 2GB, and CMA is setted to 512MB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;江亚强&lt;/P&gt;&lt;P&gt;软件工程师&lt;/P&gt;&lt;P&gt;Shenzhen Huameishi Technology Co., Ltd&lt;/P&gt;&lt;P&gt;深圳市华美视科技有限公司&lt;/P&gt;&lt;P&gt;深圳市南山区科苑路6号科技园工业大厦605&lt;/P&gt;&lt;P&gt;Tel：0755-26037882-616&lt;/P&gt;&lt;P&gt;Mail:yaqiang.jiang@huameishi.com&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 06:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/810201#M124944</guid>
      <dc:creator>jiangyaqiang</dc:creator>
      <dc:date>2018-10-02T06:09:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 gpu crash when playing video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/1729013#M213116</link>
      <description>&lt;P&gt;Hi, Even this issues still persist in kernel v5.15.71 in NXP BSP - kirkstone branch.&lt;BR /&gt;&lt;BR /&gt;We faced it with one of our customer for sway compositor.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;[   27.464790] etnaviv-gpu 38000000.gpu: AXI bus error&lt;/SPAN&gt;
&lt;SPAN class=""&gt;[   27.469745] etnaviv-gpu 38000000.gpu: MMU fault status 0x00000000&lt;/SPAN&gt;
&lt;SPAN class=""&gt;[   27.970450] etnaviv-gpu 38000000.gpu: recover hung GPU!&lt;/SPAN&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;However we were able to resolve the issue and now its running smooth with the weston and sway compositor with 4GiB RAM usage.&lt;BR /&gt;&lt;BR /&gt;As this was done for the customer we are unable to share the details, in case of support please reach-out to us on &lt;A href="mailto:rutvij.trivedi@siliconsignals.io" target="_blank" rel="noopener"&gt;rutvij.trivedi@siliconsignals.io&lt;/A&gt; or visit &lt;A href="http://www.siliconsignals.io" target="_blank" rel="noopener"&gt;www.siliconsignals.io&lt;/A&gt;.&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;BR&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 14:37:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-gpu-crash-when-playing-video/m-p/1729013#M213116</guid>
      <dc:creator>r_trivedi123</dc:creator>
      <dc:date>2023-09-25T14:37:05Z</dc:date>
    </item>
  </channel>
</rss>