<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8 Display Port Interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809829#M124881</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi José,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The lane order in DP is different than in HDMI: &lt;BR /&gt;-&amp;nbsp; HDMI D0 goes to DP2&lt;BR /&gt;-&amp;nbsp; HDMI D1 goes to DP1&lt;BR /&gt;-&amp;nbsp; HDMI D2 goes to DP0&lt;BR /&gt;-&amp;nbsp; HDMI CK goes to DP3&lt;/LI&gt;&lt;LI&gt;The pulldowns on the HDMI lines on the 8M EVK must be removed when used for DP purposes&lt;/LI&gt;&lt;LI&gt;Yes, if you work with an add-on plug converter you need to change these pull-ups into pull-downs, so remove them from the 8M EVK&lt;/LI&gt;&lt;LI&gt;I don't have a clear date yet, but I will keep you informed.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The connection based on this adapter looks like this:&lt;/P&gt;&lt;P&gt;-&amp;nbsp; an 8M EVK is prepared for this setup (resistors mentioned above changed/removed)&lt;/P&gt;&lt;P&gt;-&amp;nbsp; from the 8M board a short HDMI cable goes to the HDMI-DP adapter board (HDMI-A to HDMI-A)&lt;/P&gt;&lt;P&gt;-&amp;nbsp; the required remapping of the signals take place on the adapter board&lt;/P&gt;&lt;P&gt;-&amp;nbsp; the DP jack on the adapter board connects directly to a DP connector of a monitor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Feb 2019 13:41:39 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2019-02-05T13:41:39Z</dc:date>
    <item>
      <title>i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809824#M124876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with the MCIMX8M-EVK and I need to use Display Port (DP). The i.MX8 processor supports DP through interface HDMI Display Interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My first question is aboug this interface. I was unable to find any information about DP pins in i.MX8 documents. However, in some SOMs (System-On-Module) datasheets this information can be find. In the Figure 1 it is possible see this relation. Are these pins correct to DP connection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69982i5B2706BEF01A295A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My second question is related the MCIMX8M-EVK HDMI connector. My intent is used this connector (with a adapter) to use like DP output. But in the schematics it is possible see that HDMI_HPD and HDMI_AUX_N are tied together. Is it possible use some adaptor with this limitation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70019i2287AAC2D1940AFE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2018 23:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809824#M124876</guid>
      <dc:creator>joséviníciusmel</dc:creator>
      <dc:date>2018-12-17T23:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809825#M124877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi José&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for eDP signal descriptions and connections one can look at eDP specification&lt;/P&gt;&lt;P&gt;since Reference Manual sect.13.4 described that hdmi module complies with DisplayPort Specification,&lt;/P&gt;&lt;P&gt;Version 1.3. As for HDMI_HPD and HDMI_AUX_N, there are no issues for eDP usage, as they muxed&lt;/P&gt;&lt;P&gt;with eDP_HPD and eDP_AUX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Dec 2018 08:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809825#M124877</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-20T08:23:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809826#M124878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Besides the physical conversion between the HDMI and the DP signal mapping, the software BSP needs to support the Display Port as well.&lt;/P&gt;&lt;P&gt;And this is not the case, neither in the current Linux BSP nor in Android. It might come in the future, but for now it's not supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For basic system verification during validation we used a small plug which converts the HDMI plug into a DP plug:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="HDMI-DP_Bridge.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76624i5CAF9F3206CAE4E3/image-size/large?v=v2&amp;amp;px=999" role="button" title="HDMI-DP_Bridge.png" alt="HDMI-DP_Bridge.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 17:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809826#M124878</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2019-01-09T17:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809827#M124879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys!&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;P&gt;I will use this HDMI-DP Bridge like model, but I have some questions.&lt;/P&gt;&lt;P&gt;1) In my first figure, the pair&amp;nbsp;HDMI_TX_M_LN_0/HDMI_TX_P_LN_0 is referred like DP LANE 0 NEG/DP LANE 0 POS, but in the&amp;nbsp;&lt;SPAN&gt;HDMI-DP Bridge example the HDMI_TX_M_LN_0/&lt;SPAN&gt;HDMI_TX_P_LN_0 was used to this lane. Do I need be careful with this pins?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;2) In&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MCIMX8M-EVK the four DP lanes are pulled down through 604 ohms resistors. Is it a problem to used this DP adaptor with these pulldown resistors?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;3) In the&amp;nbsp;&lt;SPAN style="color: #3d3d3d;"&gt;HDMI-DP Bridge example the we can be see that DDC and CEC pins need be pulled down, but in the&amp;nbsp;MCIMX8M-EVK these pins are pulled up. Is it a problem keep these pins pulled up?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN style="background-color: #ffffff; color: #3d3d3d;"&gt;4) The fact that software support to DP will be released in the future is not a problem, but the do NXP have some date to this software release?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 19:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809827#M124879</guid>
      <dc:creator>joséviníciusmel</dc:creator>
      <dc:date>2019-01-21T19:23:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809828#M124880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor! Can you answer the questions below?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 00:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809828#M124880</guid>
      <dc:creator>joséviníciusmel</dc:creator>
      <dc:date>2019-02-01T00:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809829#M124881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi José,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The lane order in DP is different than in HDMI: &lt;BR /&gt;-&amp;nbsp; HDMI D0 goes to DP2&lt;BR /&gt;-&amp;nbsp; HDMI D1 goes to DP1&lt;BR /&gt;-&amp;nbsp; HDMI D2 goes to DP0&lt;BR /&gt;-&amp;nbsp; HDMI CK goes to DP3&lt;/LI&gt;&lt;LI&gt;The pulldowns on the HDMI lines on the 8M EVK must be removed when used for DP purposes&lt;/LI&gt;&lt;LI&gt;Yes, if you work with an add-on plug converter you need to change these pull-ups into pull-downs, so remove them from the 8M EVK&lt;/LI&gt;&lt;LI&gt;I don't have a clear date yet, but I will keep you informed.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The connection based on this adapter looks like this:&lt;/P&gt;&lt;P&gt;-&amp;nbsp; an 8M EVK is prepared for this setup (resistors mentioned above changed/removed)&lt;/P&gt;&lt;P&gt;-&amp;nbsp; from the 8M board a short HDMI cable goes to the HDMI-DP adapter board (HDMI-A to HDMI-A)&lt;/P&gt;&lt;P&gt;-&amp;nbsp; the required remapping of the signals take place on the adapter board&lt;/P&gt;&lt;P&gt;-&amp;nbsp; the DP jack on the adapter board connects directly to a DP connector of a monitor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 13:41:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809829#M124881</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2019-02-05T13:41:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809830#M124882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Bernhard!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 19:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809830#M124882</guid>
      <dc:creator>joséviníciusmel</dc:creator>
      <dc:date>2019-02-05T19:23:01Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809831#M124883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/bernhardfink"&gt;bernhardfink&lt;/A&gt;‌ are there any gerbers / boms for the above adapter that i could grab to build one?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2020 17:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809831#M124883</guid>
      <dc:creator>guido_gunther</dc:creator>
      <dc:date>2020-04-24T17:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809832#M124884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, sorry, just the schematic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2020 11:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/809832#M124884</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-04-27T11:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1150413#M161455</link>
      <description>&lt;P&gt;Hi. I`m working with my own board with IMX8M and want to use DisplayPort inteface through usb type-c alt mode. Is attached schematic right for my case? Are there any news about linux bsp updates for dp support? Thanks!&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot_2020-09-08 i MX8 QM i MX8 QXPHardware Developer’s Guide - IMX8MEKHDG pdf.png" style="width: 711px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124638iE4261AEA4FE020D1/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot_2020-09-08 i MX8 QM i MX8 QXPHardware Developer’s Guide - IMX8MEKHDG pdf.png" alt="Screenshot_2020-09-08 i MX8 QM i MX8 QXPHardware Developer’s Guide - IMX8MEKHDG pdf.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 14:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1150413#M161455</guid>
      <dc:creator>Alex1990</dc:creator>
      <dc:date>2020-09-08T14:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1391256#M184935</link>
      <description>&lt;P&gt;Hi Bernhard,&lt;BR /&gt;&lt;BR /&gt;Does your answer to point 1. remain the same if using a 2-lane displayport (eDP) connection?&lt;BR /&gt;i.e:&lt;BR /&gt;- HDMI D2 goes to DP0&lt;BR /&gt;- HDMI D1 goes to DP1&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Dec 2021 09:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1391256#M184935</guid>
      <dc:creator>Banderson</dc:creator>
      <dc:date>2021-12-23T09:14:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1657779#M206573</link>
      <description>&lt;P&gt;Hi Banderson,&lt;/P&gt;&lt;P&gt;Was this found to be true? It should be. I currently have a two-lane setup with eDP. The auxiliary communication works well, and the link training detects two lanes. However, I am unable to get transmission.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 15:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1657779#M206573</guid>
      <dc:creator>smusserRosen</dc:creator>
      <dc:date>2023-05-25T15:02:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Display Port Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1892083#M225337</link>
      <description>&lt;P&gt;Could you please provide any information on whether the software BSP now supports DisplayPort?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jun 2024 10:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Display-Port-Interface/m-p/1892083#M225337</guid>
      <dc:creator>sanum19</dc:creator>
      <dc:date>2024-06-21T10:45:52Z</dc:date>
    </item>
  </channel>
</rss>