<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808887#M124766</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Taking in consideration that the board has pass the DDR calibration with version 1.0.3 and also DDR testing under&amp;nbsp;controlled environmental conditions (-10 to 45C) during 24hr (to mention a few),&amp;nbsp;any thought or suggestion regarding this situation with 2.92 version?&lt;/P&gt;&lt;P&gt;I could use previous version and support my production decisions on additional testing, but I would like to be sure I'm not dismissing a possible issue based on the improved new tool revision.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 20 Oct 2018 00:34:09 GMT</pubDate>
    <dc:creator>juliocruz</dc:creator>
    <dc:date>2018-10-20T00:34:09Z</dc:date>
    <item>
      <title>DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808883#M124762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Some time ago I used &lt;STRONG&gt;DDR_Stress_Tester_V1.0.3&lt;/STRONG&gt; in a custom board without issues. Recently, in a new board I used the same version without issue neither.&lt;/P&gt;&lt;P&gt;I just decided to update the tools to &lt;STRONG&gt;ddr_stress_tester_v2.92&lt;/STRONG&gt; and the application shows&amp;nbsp;&lt;STRONG&gt;HW WL cal status: no suitable delay value found for byte 5&lt;/STRONG&gt; and later&amp;nbsp;&lt;STRONG&gt;Error: failed during write leveling calibration&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Appreciated any suggestion.&lt;/P&gt;&lt;P&gt;Below more details:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/75976i4B4D054F9A4E7DAF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3 
Data width: 64, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used 
Density per chip select: 1024MB 
============================================

Current Temperature: 51
============================================

DDR Freq: 396 MHz

ddr_mr1=0x00000004
Start write leveling calibration...
running Write level HW calibration
 MPWLHWERR register read out for factory diagnostics: 
 MPWLHWERR PHY0 = 0x3c7c7878
 MPWLHWERR PHY1 = 0x3e00003c


HW WL cal status: no suitable delay value found for byte 5

HW WL cal status: no suitable delay value found for byte 6 
Write leveling calibration completed but failed, the following results were found:
 MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00430043
 MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x0033003B
 MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x001F0024
 MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x001C001F
Write DQS delay result:
 Write DQS0 delay: 67/256 CK
 Write DQS1 delay: 67/256 CK
 Write DQS2 delay: 59/256 CK
 Write DQS3 delay: 51/256 CK
 Write DQS4 delay: 36/256 CK
 Write DQS5 delay: 31/256 CK
 Write DQS6 delay: 31/256 CK
 Write DQS7 delay: 28/256 CK

Error: failed during write leveling calibration&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;In other hand, the result using the version 1.0.3 is as below:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;DDR_Stress_Tester_V1.0.3\Binary&amp;gt;DDR_Stress_Tester.exe -t mx6x -df "DualLite.inc"
MX6DL opened.
HAB_TYPE: DEVELOP
Image loading...
download Image to IRAM OK

Re-open MX6x device.
Running DDR test..., press "ESC" key to exit.





******************************
 DDR Stress Test (1.0.3) for MX6DL
 Build: Jun 25 2014, 12:09:29
 Freescale Semiconductor, Inc.
******************************

=======DDR configuration==========
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
==================================


What ARM core speed would you like to run?
Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz
 ARM set to 1GHz

Please select the DDR density per chip select (in bytes) on the board
Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6 for 32MB
For maximum supported density (4GB), we can only access up to 3.75GB. Type 9 to select this
 DDR density selected (MB): 1024


Calibration will run at DDR frequency 400MHz. Type 'y' to continue.
If you want to run at other DDR frequency. Type 'n'
 DDR Freq: 396 MHz

Would you like to run the write leveling calibration? (y/n)
 Please enter the MR1 value on the initilization script
 This will be re-programmed into MR1 after write leveling calibration
 Enter as a 4-digit HEX value, example 0004, then hit enter
0004 You have entered: 0x0004
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x00420041
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x0032003A
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x001F0024
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x001C001F

Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .
BYTE 0:
 Start: HC=0x00 ABS=0x14
 End: HC=0x03 ABS=0x48
 Mean: HC=0x01 ABS=0x6D
 End-0.5*tCK: HC=0x02 ABS=0x48
 Final: HC=0x02 ABS=0x48
BYTE 1:
 Start: HC=0x00 ABS=0x18
 End: HC=0x03 ABS=0x48
 Mean: HC=0x01 ABS=0x6F
 End-0.5*tCK: HC=0x02 ABS=0x48
 Final: HC=0x02 ABS=0x48
BYTE 2:
 Start: HC=0x00 ABS=0x04
 End: HC=0x03 ABS=0x38
 Mean: HC=0x01 ABS=0x5D
 End-0.5*tCK: HC=0x02 ABS=0x38
 Final: HC=0x02 ABS=0x38
BYTE 3:
 Start: HC=0x01 ABS=0x00
 End: HC=0x03 ABS=0x34
 Mean: HC=0x02 ABS=0x1A
 End-0.5*tCK: HC=0x02 ABS=0x34
 Final: HC=0x02 ABS=0x34
BYTE 4:
 Start: HC=0x00 ABS=0x7C
 End: HC=0x03 ABS=0x30
 Mean: HC=0x02 ABS=0x16
 End-0.5*tCK: HC=0x02 ABS=0x30
 Final: HC=0x02 ABS=0x30
BYTE 5:
 Start: HC=0x00 ABS=0x70
 End: HC=0x03 ABS=0x2C
 Mean: HC=0x02 ABS=0x0E
 End-0.5*tCK: HC=0x02 ABS=0x2C
 Final: HC=0x02 ABS=0x2C
BYTE 6:
 Start: HC=0x00 ABS=0x00
 End: HC=0x03 ABS=0x24
 Mean: HC=0x01 ABS=0x51
 End-0.5*tCK: HC=0x02 ABS=0x24
 Final: HC=0x02 ABS=0x24
BYTE 7:
 Start: HC=0x00 ABS=0x58
 End: HC=0x03 ABS=0x20
 Mean: HC=0x01 ABS=0x7B
 End-0.5*tCK: HC=0x02 ABS=0x20
 Final: HC=0x02 ABS=0x20

DQS calibration MMDC0 MPDGCTRL0 = 0x02480248, MPDGCTRL1 = 0x02340238

DQS calibration MMDC1 MPDGCTRL0 = 0x022C0230, MPDGCTRL1 = 0x02200224

Note: Array result[] holds the DRAM test result of each byte.
 0: test pass. 1: test fail
 4 bits respresent the result of 1 byte.
 result 00000001:byte 0 fail.
 result 00000011:byte 0, 1 fail.

Starting Read calibration...

ABS_OFFSET=0x00000000 result[00]=0x11111111
ABS_OFFSET=0x04040404 result[01]=0x11111111
ABS_OFFSET=0x08080808 result[02]=0x11111111
ABS_OFFSET=0x0C0C0C0C result[03]=0x11111111
ABS_OFFSET=0x10101010 result[04]=0x11111111
ABS_OFFSET=0x14141414 result[05]=0x11111111
ABS_OFFSET=0x18181818 result[06]=0x11111111
ABS_OFFSET=0x1C1C1C1C result[07]=0x00100010
ABS_OFFSET=0x20202020 result[08]=0x00100000
ABS_OFFSET=0x24242424 result[09]=0x00000000
ABS_OFFSET=0x28282828 result[0A]=0x00000000
ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000
ABS_OFFSET=0x30303030 result[0C]=0x00000000
ABS_OFFSET=0x34343434 result[0D]=0x00000000
ABS_OFFSET=0x38383838 result[0E]=0x00000000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000
ABS_OFFSET=0x40404040 result[10]=0x00000000
ABS_OFFSET=0x44444444 result[11]=0x00000000
ABS_OFFSET=0x48484848 result[12]=0x00000000
ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000
ABS_OFFSET=0x50505050 result[14]=0x00000000
ABS_OFFSET=0x54545454 result[15]=0x00000000
ABS_OFFSET=0x58585858 result[16]=0x00000000
ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000
ABS_OFFSET=0x60606060 result[18]=0x00000000
ABS_OFFSET=0x64646464 result[19]=0x00000000
ABS_OFFSET=0x68686868 result[1A]=0x00001000
ABS_OFFSET=0x6C6C6C6C result[1B]=0x00011111
ABS_OFFSET=0x70707070 result[1C]=0x01011111
ABS_OFFSET=0x74747474 result[1D]=0x11011111
ABS_OFFSET=0x78787878 result[1E]=0x11111111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111

MMDC0 MPRDDLCTL = 0x40424442, MMDC1 MPRDDLCTL = 0x46444C42

Starting Write calibration...

ABS_OFFSET=0x00000000 result[00]=0x11111111
ABS_OFFSET=0x04040404 result[01]=0x00101000
ABS_OFFSET=0x08080808 result[02]=0x00000000
ABS_OFFSET=0x0C0C0C0C result[03]=0x00000000
ABS_OFFSET=0x10101010 result[04]=0x00000000
ABS_OFFSET=0x14141414 result[05]=0x00000000
ABS_OFFSET=0x18181818 result[06]=0x00000000
ABS_OFFSET=0x1C1C1C1C result[07]=0x00000000
ABS_OFFSET=0x20202020 result[08]=0x00000000
ABS_OFFSET=0x24242424 result[09]=0x00000000
ABS_OFFSET=0x28282828 result[0A]=0x00000000
ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000
ABS_OFFSET=0x30303030 result[0C]=0x00000000
ABS_OFFSET=0x34343434 result[0D]=0x00000000
ABS_OFFSET=0x38383838 result[0E]=0x00000000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000
ABS_OFFSET=0x40404040 result[10]=0x00000000
ABS_OFFSET=0x44444444 result[11]=0x00000000
ABS_OFFSET=0x48484848 result[12]=0x00000000
ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000
ABS_OFFSET=0x50505050 result[14]=0x00000000
ABS_OFFSET=0x54545454 result[15]=0x00000000
ABS_OFFSET=0x58585858 result[16]=0x00000000
ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000
ABS_OFFSET=0x60606060 result[18]=0x00010010
ABS_OFFSET=0x64646464 result[19]=0x00110111
ABS_OFFSET=0x68686868 result[1A]=0x10110111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x11111111
ABS_OFFSET=0x70707070 result[1C]=0x11111111
ABS_OFFSET=0x74747474 result[1D]=0x11111111
ABS_OFFSET=0x78787878 result[1E]=0x11111111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111

MMDC0 MPWRDLCTL = 0x38323032,MMDC1 MPWRDLCTL = 0x34363430


 MMDC registers updated from calibration

Read DQS Gating calibration
 MPDGCTRL0 PHY0 (0x021b083c) = 0x02480248
 MPDGCTRL1 PHY0 (0x021b0840) = 0x02340238
 MPDGCTRL0 PHY1 (0x021b483c) = 0x022C0230
 MPDGCTRL1 PHY1 (0x021b4840) = 0x02200224

Read calibration
 MPRDDLCTL PHY0 (0x021b0848) = 0x40424442
 MPRDDLCTL PHY1 (0x021b4848) = 0x46444C42

Write calibration
 MPWRDLCTL PHY0 (0x021b0850) = 0x38323032
 MPWRDLCTL PHY1 (0x021b4850) = 0x34363430


The DDR stress test can run with an incrementing frequency or at a static freq
To run at a static freq, simply set the start freq and end freq to the same value
Would you like to run the DDR Stress Test (y/n)?&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:11:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808883#M124762</guid>
      <dc:creator>juliocruz</dc:creator>
      <dc:date>2020-11-02T14:11:50Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808884#M124763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;old version did not have ICache and DCache turned on, so newer version provide&lt;/P&gt;&lt;P&gt;more accurate results. You can try to increase WALAT and verify ddr layout with&lt;/P&gt;&lt;P&gt;recommendations given by i.MX6 System Development User’s Guide&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fuser-guide%2FIMX6DQ6SDLHDG.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 08:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808884#M124763</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-19T08:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808885#M124764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;Thanks for your feedback and suggestion.&lt;/P&gt;&lt;P&gt;For&amp;nbsp;the&amp;nbsp;version 1.0.3, I used the guide&amp;nbsp;&lt;STRONG&gt;Freescale i.MX6 DRAM Port Application&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Guide – DDR3.&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please, may I know which documentation is available for the&amp;nbsp;2.92 version?&lt;/P&gt;&lt;P&gt;According with your suggestion, I would need to check further details.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;About the suggested guide, I review&amp;nbsp;it a lot. In other hand, I had&amp;nbsp;been using previous boards (with same layout) without issues.&lt;/LI&gt;&lt;LI&gt;About the WALAT suggestion, the default value of WALAT is 1.&amp;nbsp;After&amp;nbsp;set to&amp;nbsp;2 and 3, the results are similar:&amp;nbsp;&lt;STRONG&gt;no suitable delay value found for byte 5 and 6&lt;/STRONG&gt;.&amp;nbsp;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Regards and Thanks,&lt;/P&gt;&lt;P&gt;Julio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 10:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808885#M124764</guid>
      <dc:creator>juliocruz</dc:creator>
      <dc:date>2018-10-19T10:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808886#M124765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After re-check again the post by &lt;A _jive_internal="true" data-content-finding="Community" data-userid="203527" data-username="OliverChen" href="https://community.nxp.com/people/OliverChen" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 600; text-decoration: none; font-size: 11.9994px;"&gt;Oliver Chen&lt;/A&gt;&amp;nbsp;at&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.92&lt;/A&gt;,&amp;nbsp;I&amp;nbsp;wondering&amp;nbsp;if the error during my testing has something to do with fix in previous release 2.91:&lt;/P&gt;&lt;UL style="color: #51626f; background-color: #ffffff; border: 0px; padding: 0px 0px 0px 30px;"&gt;&lt;LI style="border: 0px; font-weight: inherit; margin: 0.2em 0px;"&gt;Resolved issue with write leveling calibration code where a race condition in the code may result in the calibration routine &lt;STRONG&gt;not being able to find any delay values&lt;/STRONG&gt;.&amp;nbsp; Only applies to MX6 series SoCs that support DDR3.&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 10:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808886#M124765</guid>
      <dc:creator>juliocruz</dc:creator>
      <dc:date>2018-10-19T10:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808887#M124766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Taking in consideration that the board has pass the DDR calibration with version 1.0.3 and also DDR testing under&amp;nbsp;controlled environmental conditions (-10 to 45C) during 24hr (to mention a few),&amp;nbsp;any thought or suggestion regarding this situation with 2.92 version?&lt;/P&gt;&lt;P&gt;I could use previous version and support my production decisions on additional testing, but I would like to be sure I'm not dismissing a possible issue based on the improved new tool revision.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Oct 2018 00:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808887#M124766</guid>
      <dc:creator>juliocruz</dc:creator>
      <dc:date>2018-10-20T00:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: DDR Test tool 1.0.3 pass while 2.92 fail. Which setting is wrong?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808888#M124767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if boards are working fine with parameters got from version 1.0.3&lt;/P&gt;&lt;P&gt;one can stay with them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2018 09:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-Test-tool-1-0-3-pass-while-2-92-fail-Which-setting-is-wrong/m-p/808888#M124767</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-22T09:41:44Z</dc:date>
    </item>
  </channel>
</rss>