<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to enable 180 degree rotation from framebuffer driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-180-degree-rotation-from-framebuffer-driver/m-p/808862#M124755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on android O nxp BSP.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to get to the homescreen but the problem I am facing is that the screen is 180 degree rotated. If I try to rotate it I can't do it as only vertical flip is possible.&amp;nbsp;&lt;BR /&gt;I went to older threads for this problem but they are irrelevant now as structure of many functions are changed.&lt;/P&gt;&lt;P&gt;Is there any way or patch to be applied to get this rotation functionality without too much hassle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way in android that we can handle rotation of screen or any workaround involving gpu and ipu?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mrigendra Chaubey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 12:53:27 GMT</pubDate>
    <dc:creator>mrigendra_chaub</dc:creator>
    <dc:date>2018-08-01T12:53:27Z</dc:date>
    <item>
      <title>How to enable 180 degree rotation from framebuffer driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-180-degree-rotation-from-framebuffer-driver/m-p/808862#M124755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on android O nxp BSP.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am able to get to the homescreen but the problem I am facing is that the screen is 180 degree rotated. If I try to rotate it I can't do it as only vertical flip is possible.&amp;nbsp;&lt;BR /&gt;I went to older threads for this problem but they are irrelevant now as structure of many functions are changed.&lt;/P&gt;&lt;P&gt;Is there any way or patch to be applied to get this rotation functionality without too much hassle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way in android that we can handle rotation of screen or any workaround involving gpu and ipu?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mrigendra Chaubey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 12:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-180-degree-rotation-from-framebuffer-driver/m-p/808862#M124755</guid>
      <dc:creator>mrigendra_chaub</dc:creator>
      <dc:date>2018-08-01T12:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable 180 degree rotation from framebuffer driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-180-degree-rotation-from-framebuffer-driver/m-p/808863#M124756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the link as below:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/311058?commentID=345218#comment-345218" title="https://community.nxp.com/thread/311058?commentID=345218#comment-345218"&gt;https://community.nxp.com/thread/311058?commentID=345218#comment-345218&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Aug 2018 08:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-180-degree-rotation-from-framebuffer-driver/m-p/808863#M124756</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-08-08T08:14:04Z</dc:date>
    </item>
  </channel>
</rss>