<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem while compiling android p for imx6dl sabresd board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-while-compiling-android-p-for-imx6dl-sabresd-board/m-p/807047#M124539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am compiling android P source beta version for imx6dl sabresd board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my kernel version is 4.9.17&amp;nbsp; (same as Oreo)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While doing make I am getting below error ---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;build/make/core/Makefile was modified, regenerating...&lt;BR /&gt;[100% 1/1] initializing build system ...&lt;BR /&gt;/bin/bash: line 0: [: Q: integer expression expected&lt;BR /&gt;[ 62% 543/869] including system/sepolicy/Android.mk ...&lt;BR /&gt;system/sepolicy/Android.mk:79: warning: BOARD_SEPOLICY_VERS not specified, assuming current platform version&lt;BR /&gt;[ 98% 859/869] including vendor/nxp/fsl-codec/Android.mk ...&lt;BR /&gt;/bin/bash: line 0: [: Q: integer expression expected&lt;BR /&gt;[ 99% 868/869] finishing build rules ...&lt;BR /&gt;No private recovery resources for TARGET_DEVICE sabresd_6dq&lt;BR /&gt;platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module TelecomUnitTests &lt;BR /&gt;platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module TeleServiceTests &lt;BR /&gt;[100% 869/869] writing build rules ...&lt;BR /&gt;build/make/core/Makefile:34: warning: overriding commands for target `out/target/product/sabresd_6dq/root/init.rc'&lt;BR /&gt;build/make/core/base_rules.mk:413: warning: ignoring old commands for target `out/target/product/sabresd_6dq/root/init.rc'&lt;BR /&gt;[ 98% 872/884] build out/target/product/sabresd_6dq/obj/KERNEL_OBJ/.config&lt;BR /&gt;FAILED: out/target/product/sabresd_6dq/obj/KERNEL_OBJ/.config&lt;BR /&gt;/bin/bash -c "(make -j3 -C vendor/nxp-opensource/kernel_imx imx_v7_android_defconfig ARCH=arm CROSS_COMPILE=/home/ptg/Desktop/arm-linux-androideabi-4.9/bin/arm-linux-androideabi- LOADADDR=0x10008000 KCFLAGS=-mno-android ) &amp;amp;&amp;amp; (install -D vendor/nxp-opensource/kernel_imx/.config out/target/product/sabresd_6dq/obj/KERNEL_OBJ/.config )"&lt;BR /&gt;make: Entering directory `/media/ptg/600e2f3c-f78b-42be-ab60-581dab9159ce/android_p/vendor/nxp-opensource/kernel_imx'&lt;BR /&gt;&amp;nbsp; HOSTCC&amp;nbsp; scripts/basic/fixdep&lt;BR /&gt;/bin/sh: 1: gcc: not found&lt;BR /&gt;make[1]: *** [scripts/basic/fixdep] Error 127&lt;BR /&gt;make: *** [scripts_basic] Error 2&lt;BR /&gt;make: Leaving directory `/media/ptg/600e2f3c-f78b-42be-ab60-581dab9159ce/android_p/vendor/nxp-opensource/kernel_imx'&lt;BR /&gt;17:38:33 ninja failed with: exit status 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to solve this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 12:25:21 GMT</pubDate>
    <dc:creator>vivektol</dc:creator>
    <dc:date>2018-08-01T12:25:21Z</dc:date>
    <item>
      <title>Problem while compiling android p for imx6dl sabresd board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-while-compiling-android-p-for-imx6dl-sabresd-board/m-p/807047#M124539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am compiling android P source beta version for imx6dl sabresd board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my kernel version is 4.9.17&amp;nbsp; (same as Oreo)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While doing make I am getting below error ---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;build/make/core/Makefile was modified, regenerating...&lt;BR /&gt;[100% 1/1] initializing build system ...&lt;BR /&gt;/bin/bash: line 0: [: Q: integer expression expected&lt;BR /&gt;[ 62% 543/869] including system/sepolicy/Android.mk ...&lt;BR /&gt;system/sepolicy/Android.mk:79: warning: BOARD_SEPOLICY_VERS not specified, assuming current platform version&lt;BR /&gt;[ 98% 859/869] including vendor/nxp/fsl-codec/Android.mk ...&lt;BR /&gt;/bin/bash: line 0: [: Q: integer expression expected&lt;BR /&gt;[ 99% 868/869] finishing build rules ...&lt;BR /&gt;No private recovery resources for TARGET_DEVICE sabresd_6dq&lt;BR /&gt;platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module TelecomUnitTests &lt;BR /&gt;platform_testing/build/tasks/tests/instrumentation_test_list.mk: warning: continuous_instrumentation_tests: Unknown installed file for module TeleServiceTests &lt;BR /&gt;[100% 869/869] writing build rules ...&lt;BR /&gt;build/make/core/Makefile:34: warning: overriding commands for target `out/target/product/sabresd_6dq/root/init.rc'&lt;BR /&gt;build/make/core/base_rules.mk:413: warning: ignoring old commands for target `out/target/product/sabresd_6dq/root/init.rc'&lt;BR /&gt;[ 98% 872/884] build out/target/product/sabresd_6dq/obj/KERNEL_OBJ/.config&lt;BR /&gt;FAILED: out/target/product/sabresd_6dq/obj/KERNEL_OBJ/.config&lt;BR /&gt;/bin/bash -c "(make -j3 -C vendor/nxp-opensource/kernel_imx imx_v7_android_defconfig ARCH=arm CROSS_COMPILE=/home/ptg/Desktop/arm-linux-androideabi-4.9/bin/arm-linux-androideabi- LOADADDR=0x10008000 KCFLAGS=-mno-android ) &amp;amp;&amp;amp; (install -D vendor/nxp-opensource/kernel_imx/.config out/target/product/sabresd_6dq/obj/KERNEL_OBJ/.config )"&lt;BR /&gt;make: Entering directory `/media/ptg/600e2f3c-f78b-42be-ab60-581dab9159ce/android_p/vendor/nxp-opensource/kernel_imx'&lt;BR /&gt;&amp;nbsp; HOSTCC&amp;nbsp; scripts/basic/fixdep&lt;BR /&gt;/bin/sh: 1: gcc: not found&lt;BR /&gt;make[1]: *** [scripts/basic/fixdep] Error 127&lt;BR /&gt;make: *** [scripts_basic] Error 2&lt;BR /&gt;make: Leaving directory `/media/ptg/600e2f3c-f78b-42be-ab60-581dab9159ce/android_p/vendor/nxp-opensource/kernel_imx'&lt;BR /&gt;17:38:33 ninja failed with: exit status 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to solve this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 12:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-while-compiling-android-p-for-imx6dl-sabresd-board/m-p/807047#M124539</guid>
      <dc:creator>vivektol</dc:creator>
      <dc:date>2018-08-01T12:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problem while compiling android p for imx6dl sabresd board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-while-compiling-android-p-for-imx6dl-sabresd-board/m-p/807048#M124540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vivek Tol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As of right now there is not an Android P BSP for NXP boards so I’m afraid we cannot provide much help on this matter. I would recommend looking for help on the Android forums as Android P is still in beta.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reagrds,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 16:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-while-compiling-android-p-for-imx6dl-sabresd-board/m-p/807048#M124540</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-08-01T16:21:30Z</dc:date>
    </item>
  </channel>
</rss>