<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Some problem using combo box, drag and drop in Wayland.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Some-problem-using-combo-box-drag-and-drop-in-Wayland/m-p/806932#M124534</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please follow exactly the attached document to build various graphics configurations of the L4.1.15 BSP.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2018 11:17:10 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-06-26T11:17:10Z</dc:date>
    <item>
      <title>Some problem using combo box, drag and drop in Wayland.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Some-problem-using-combo-box-drag-and-drop-in-Wayland/m-p/806931#M124533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the i.mx6 quad. And software environment is Linux kernel 4.1.15 and SabreSD.&lt;/P&gt;&lt;P&gt;Filesystem include qt5 and wayland. But it has problem. Didn't work combo box and drag and drop. To be precise, using a combo box, drag and drop stops the application.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems to be a problem for my application, I used the qt example inside the filesystem, but the symptoms are the same.&lt;/P&gt;&lt;P&gt;Also, if you use the weston binary created with bitbake, the screen does not appear.&lt;/P&gt;&lt;P&gt;What can I do to resolve this issue? If you need to build a new file system, please tell me the address, commands and bitbake commands you need to repo git. (Command for example,&amp;nbsp;repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.1.0.xml,&amp;nbsp;&amp;nbsp;DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland-sabresd, bitbake fsl-image-qt5)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2018 23:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Some-problem-using-combo-box-drag-and-drop-in-Wayland/m-p/806931#M124533</guid>
      <dc:creator>huhyangjae</dc:creator>
      <dc:date>2018-06-21T23:49:23Z</dc:date>
    </item>
    <item>
      <title>Re: Some problem using combo box, drag and drop in Wayland.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Some-problem-using-combo-box-drag-and-drop-in-Wayland/m-p/806932#M124534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please follow exactly the attached document to build various graphics configurations of the L4.1.15 BSP.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 11:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Some-problem-using-combo-box-drag-and-drop-in-Wayland/m-p/806932#M124534</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-06-26T11:17:10Z</dc:date>
    </item>
  </channel>
</rss>