<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 EMMC BOOT</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EMMC-BOOT/m-p/806852#M124515</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now we are developing android 8.0.0 using imx6q board,and is successful to build the android image.&lt;/P&gt;&lt;P&gt;But &amp;nbsp;usiing mfgtools to download images,it appear to "&amp;nbsp;Jumping to OS image.&amp;nbsp;"&lt;/P&gt;&lt;P&gt;Because we use emmc boot ,so I think we should modify u-boot to emmc boot in android o source code,but it doesn't work.&lt;/P&gt;&lt;P&gt;How to modify to emmc boot?&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 01:15:34 GMT</pubDate>
    <dc:creator>jeffery</dc:creator>
    <dc:date>2018-08-01T01:15:34Z</dc:date>
    <item>
      <title>EMMC BOOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EMMC-BOOT/m-p/806852#M124515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now we are developing android 8.0.0 using imx6q board,and is successful to build the android image.&lt;/P&gt;&lt;P&gt;But &amp;nbsp;usiing mfgtools to download images,it appear to "&amp;nbsp;Jumping to OS image.&amp;nbsp;"&lt;/P&gt;&lt;P&gt;Because we use emmc boot ,so I think we should modify u-boot to emmc boot in android o source code,but it doesn't work.&lt;/P&gt;&lt;P&gt;How to modify to emmc boot?&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 01:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EMMC-BOOT/m-p/806852#M124515</guid>
      <dc:creator>jeffery</dc:creator>
      <dc:date>2018-08-01T01:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: EMMC BOOT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EMMC-BOOT/m-p/806853#M124516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 贻才 林&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;such error happens when manufacturing firmware (files in mfg tools /firmware folder)&lt;/P&gt;&lt;P&gt;were not rebuilt for custom board. Steps are described in sect.6.2 Manufacturing Tool, MFGTool&lt;/P&gt;&lt;P&gt;attached Yocto Guide. Also had board passed ddr test&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.90&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and boot linux. New calibration coefficients found from test should be put in uboot/board/..mx6sabresd&lt;/P&gt;&lt;P&gt;/mx6q_4x_mt41j128.cfg file and image should be rebuilt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2018 00:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EMMC-BOOT/m-p/806853#M124516</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-02T00:52:31Z</dc:date>
    </item>
  </channel>
</rss>