<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic qmake error when used for target in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/qmake-error-when-used-for-target/m-p/209921#M12451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having built Qt for Embedded [Qt_Everywhere_Opensource] on i.MX5X successfully, an Application has been tried on Qt Creator IDE [from Qt_SDK_4.8.0] on Host-PC, with the build, qmake being done well.&lt;/P&gt;&lt;P&gt;The application binary has been generated with a makefile, that uses the native-gcc as the work is being done on Host. The binary has been successfully run on the Qt_Simulator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now that, I wanted to try this on Target, I did this&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Cross-Compile&lt;/STRONG&gt; [ Using arm-none-linux-gnueabi- YYY ] &lt;STRONG&gt;the Project files with the qmake binary for i.MX5X&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;post4pavan@ubuntu:&lt;STRONG&gt;/usr/local/Trolltech/Qt-target-version/bin&lt;/STRONG&gt;$ &lt;STRONG&gt;./qmake&lt;/STRONG&gt; /home/post4pavan/Work/hi/&lt;STRONG&gt;hi.pro&lt;/STRONG&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Failure to open file&lt;/STRONG&gt;: /usr/local/Trolltech/Qt-target-version/bin/&lt;STRONG&gt;Makefile&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Unable to generate makefile&lt;/STRONG&gt; for: /home/post4pavan/Work/hi/&lt;STRONG&gt;hi.pro&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Please Suggest :: Krishna Pavan&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Feb 2012 10:55:59 GMT</pubDate>
    <dc:creator>KrishnaPavan</dc:creator>
    <dc:date>2012-02-13T10:55:59Z</dc:date>
    <item>
      <title>qmake error when used for target</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qmake-error-when-used-for-target/m-p/209921#M12451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having built Qt for Embedded [Qt_Everywhere_Opensource] on i.MX5X successfully, an Application has been tried on Qt Creator IDE [from Qt_SDK_4.8.0] on Host-PC, with the build, qmake being done well.&lt;/P&gt;&lt;P&gt;The application binary has been generated with a makefile, that uses the native-gcc as the work is being done on Host. The binary has been successfully run on the Qt_Simulator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now that, I wanted to try this on Target, I did this&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Cross-Compile&lt;/STRONG&gt; [ Using arm-none-linux-gnueabi- YYY ] &lt;STRONG&gt;the Project files with the qmake binary for i.MX5X&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;post4pavan@ubuntu:&lt;STRONG&gt;/usr/local/Trolltech/Qt-target-version/bin&lt;/STRONG&gt;$ &lt;STRONG&gt;./qmake&lt;/STRONG&gt; /home/post4pavan/Work/hi/&lt;STRONG&gt;hi.pro&lt;/STRONG&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Failure to open file&lt;/STRONG&gt;: /usr/local/Trolltech/Qt-target-version/bin/&lt;STRONG&gt;Makefile&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Unable to generate makefile&lt;/STRONG&gt; for: /home/post4pavan/Work/hi/&lt;STRONG&gt;hi.pro&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Please Suggest :: Krishna Pavan&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2012 10:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qmake-error-when-used-for-target/m-p/209921#M12451</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2012-02-13T10:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: qmake error when used for target</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/qmake-error-when-used-for-target/m-p/209922#M12452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yeah! Solved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One thing was to add the dependencies properly to hi.pro&lt;/P&gt;&lt;P&gt;Second was to build in the project directory and not in /usr/local/Trolltech/... as it is meant for root only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards :: Krishna Pavan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2012 12:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/qmake-error-when-used-for-target/m-p/209922#M12452</guid>
      <dc:creator>KrishnaPavan</dc:creator>
      <dc:date>2012-02-14T12:14:54Z</dc:date>
    </item>
  </channel>
</rss>