<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic running gstreamer without a v4l2 device on ARM dual-core in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/running-gstreamer-without-a-v4l2-device-on-ARM-dual-core/m-p/805644#M124364</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I would like to run gstreamer to create a video streaming application but I do not use a v4l2 camera or other device.&lt;/P&gt;&lt;P&gt;Instead I have running&amp;nbsp; a FreeRTOS on the other core and there the frames are copied in the memory. Because the camera is controlled and configured from that core.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I have a shared memory pool between the 2 cores and would like to fetch the frames from the memory using a char device driver and then have a gstreamer app running on top of it. The first core runs an embedded Linux and the second a FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Is this a feasible scenario?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have came across this v4l2 plugin for mem-to-mem transfers:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/igel-oss/v4l-gst" title="https://github.com/igel-oss/v4l-gst"&gt;GitHub - igel-oss/v4l-gst: A v4l plugin to bridge V4L2 APIs and GStreamer&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Does anybody has experience with this approach?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Mihaita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Sep 2018 16:34:09 GMT</pubDate>
    <dc:creator>mihaitaivascu</dc:creator>
    <dc:date>2018-09-07T16:34:09Z</dc:date>
    <item>
      <title>running gstreamer without a v4l2 device on ARM dual-core</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/running-gstreamer-without-a-v4l2-device-on-ARM-dual-core/m-p/805644#M124364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I would like to run gstreamer to create a video streaming application but I do not use a v4l2 camera or other device.&lt;/P&gt;&lt;P&gt;Instead I have running&amp;nbsp; a FreeRTOS on the other core and there the frames are copied in the memory. Because the camera is controlled and configured from that core.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I have a shared memory pool between the 2 cores and would like to fetch the frames from the memory using a char device driver and then have a gstreamer app running on top of it. The first core runs an embedded Linux and the second a FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Is this a feasible scenario?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have came across this v4l2 plugin for mem-to-mem transfers:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/igel-oss/v4l-gst" title="https://github.com/igel-oss/v4l-gst"&gt;GitHub - igel-oss/v4l-gst: A v4l plugin to bridge V4L2 APIs and GStreamer&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Does anybody has experience with this approach?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Mihaita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2018 16:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/running-gstreamer-without-a-v4l2-device-on-ARM-dual-core/m-p/805644#M124364</guid>
      <dc:creator>mihaitaivascu</dc:creator>
      <dc:date>2018-09-07T16:34:09Z</dc:date>
    </item>
  </channel>
</rss>