<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question, i.MX8M external clock sources</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX8M-external-clock-sources/m-p/804428#M124237</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; Yes, the mentioned in the Datasheet(s) "four clock inputs to the CCM from normal GPIO pads via IOMUX &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;can be used as the clock sources in the CCM", are the following:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;CCM_EXT_CLK1 on GPIO1_IO00 &lt;BR /&gt;CCM_EXT_CLK2 on GPIO1_IO01 &lt;BR /&gt;CCM_EXT_CLK3 on GPIO1_IO06&lt;BR /&gt;CCM_EXT_CLK4 on GPIO1_IO07 &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Nov 2018 08:36:18 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-11-06T08:36:18Z</dc:date>
    <item>
      <title>Question, i.MX8M external clock sources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX8M-external-clock-sources/m-p/804427#M124236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I understand that the external clock sources which is written in your datasheet of i.MX8M(IMX8MDQLQCEC Rev.1, 3.1.4 External clock sources) are referred to the following pins?&lt;/P&gt;&lt;P&gt;CCM_EXT_CLK1 GPIO1_IO00 ALT6&lt;BR /&gt;CCM_EXT_CLK2 GPIO1_IO01 ALT6&lt;BR /&gt;CCM_EXT_CLK3 GPIO1_IO06 ALT6&lt;BR /&gt;CCM_EXT_CLK4 GPIO1_IO07 ALT6&lt;BR /&gt;(From RM, IMX8MDQLQRM, Rev.0, 8.1.1.1 Muxing Options)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 06:06:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX8M-external-clock-sources/m-p/804427#M124236</guid>
      <dc:creator>SLICE</dc:creator>
      <dc:date>2018-11-06T06:06:21Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX8M external clock sources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX8M-external-clock-sources/m-p/804428#M124237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; Yes, the mentioned in the Datasheet(s) "four clock inputs to the CCM from normal GPIO pads via IOMUX &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;can be used as the clock sources in the CCM", are the following:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;CCM_EXT_CLK1 on GPIO1_IO00 &lt;BR /&gt;CCM_EXT_CLK2 on GPIO1_IO01 &lt;BR /&gt;CCM_EXT_CLK3 on GPIO1_IO06&lt;BR /&gt;CCM_EXT_CLK4 on GPIO1_IO07 &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 08:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX8M-external-clock-sources/m-p/804428#M124237</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-11-06T08:36:18Z</dc:date>
    </item>
  </channel>
</rss>