<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6QuadPlus: VDD_HIGH_IN voltage range</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803652#M124141</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ishii&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it changed for more power design flexibility as allows more freedom&lt;/P&gt;&lt;P&gt;for input voltage and possible input voltage changes (instability) during power up&lt;/P&gt;&lt;P&gt;sequence. There is no special need to increase typical voltage as it increase power consumption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Dec 2018 23:05:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-12-17T23:05:40Z</dc:date>
    <item>
      <title>IMX6QuadPlus: VDD_HIGH_IN voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803651#M124140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer ask us about reason of the specification change about VDD_SNVS_IN/VDD_HIGH_IN maximum&lt;/P&gt;&lt;P&gt;voltage range from 3.3V to 3.6V from imx6quad to imx6quadplus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In EB810. it can show in section 18 Power.&lt;/P&gt;&lt;P&gt;By this document, it seems that reason is a max power consumption on VDD_SOC and NVDD_DRAM.&lt;/P&gt;&lt;P&gt;If both typical and maximum voltage are changed, I can understand.&lt;/P&gt;&lt;P&gt;But typical voltage keep a 3.0V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why does it change only maximum voltage range to 3.6V by max power consumption of VDD_SOC and&lt;/P&gt;&lt;P&gt;NVDD_DRAM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2018 11:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803651#M124140</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2018-12-17T11:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6QuadPlus: VDD_HIGH_IN voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803652#M124141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ishii&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it changed for more power design flexibility as allows more freedom&lt;/P&gt;&lt;P&gt;for input voltage and possible input voltage changes (instability) during power up&lt;/P&gt;&lt;P&gt;sequence. There is no special need to increase typical voltage as it increase power consumption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2018 23:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803652#M124141</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-17T23:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6QuadPlus: VDD_HIGH_IN voltage range</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803653#M124142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your quick reply.&lt;/P&gt;&lt;P&gt;I understood why it was changed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 00:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6QuadPlus-VDD-HIGH-IN-voltage-range/m-p/803653#M124142</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2018-12-18T00:02:37Z</dc:date>
    </item>
  </channel>
</rss>