<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing mpg123 command to playback mp3 file would be failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-mpg123-command-to-playback-mp3-file-would-be-failed/m-p/803499#M124112</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use mpg123 to playback mp3 file on i.MX6SX, and I have added below configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;===&lt;BR /&gt;[fsl-image-qt5-validation-imx.bb]&lt;BR /&gt;CORE_IMAGE_EXTRA_INSTALL += " \&lt;BR /&gt;mpg123 \&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;[local.conf]&lt;BR /&gt;LICENSE_FLAGS_WHITELIST += "commercial commercial_mpg123"&lt;/P&gt;&lt;P&gt;===&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And then I could use mpg123 command, but &lt;STRONG&gt;it would have some errors while using mpg123 MyFile.mp3&lt;/STRONG&gt;&lt;BR /&gt;How to resolve this problem on i.MX6SX?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[error lpog]&lt;BR /&gt;root@imx6sxsabresd:/usr/share/sounds/alsa# mpg123 MyFile.mp3&lt;BR /&gt;High Performance MPEG 1.0/2.0/2.5 Audio Player for Layers 1, 2 and 3&lt;BR /&gt;version 1.25.6; written and copyright by Michael Hipp and others&lt;BR /&gt;free software (LGPL) without any warranty but with best wishes&lt;BR /&gt;[../mpg123-1.25.6/src/libout123/modules/pulse.c:107]&lt;STRONG&gt; error: Failed to open pulse audio output: Connection refused&lt;/STRONG&gt;&lt;BR /&gt;[../mpg123-1.25.6/src/libout123/libout123.c:451] error: Found no driver out of [pulse] working with device &amp;lt;default&amp;gt;.&lt;BR /&gt;main: [../mpg123-1.25.6/src/mpg123.c:308] error: out123 error 3: failure loading driver module&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is one more question:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is&amp;nbsp;LICENSE_FLAGS_WHITELIST += "commercial commercial_mpg123" could only be added in local.conf?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have tried to add it in my&amp;nbsp;fsl-image-qt5-validation-imx.bb, and I want to add this kind of configuration in my bb file, not in local.conf, but it would have the bitbake error:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Resolving any missing task queue dependencies&lt;BR /&gt;&lt;STRONG&gt;ERROR: Nothing RPROVIDES 'mpg123'&lt;/STRONG&gt; (but /home/sevenl/FPA/1016-FPA/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5-validation-imx.bb RDEPENDS on or otherwise requires it)&lt;BR /&gt;mpg123 was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST&lt;BR /&gt;NOTE: Runtime target 'mpg123' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['mpg123']&lt;BR /&gt;ERROR: Required build target 'fsl-image-qt5-validation-imx' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-qt5-validation-imx', 'mpg123']&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Nov 2018 01:36:31 GMT</pubDate>
    <dc:creator>sevenlin</dc:creator>
    <dc:date>2018-11-06T01:36:31Z</dc:date>
    <item>
      <title>Using mpg123 command to playback mp3 file would be failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-mpg123-command-to-playback-mp3-file-would-be-failed/m-p/803499#M124112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use mpg123 to playback mp3 file on i.MX6SX, and I have added below configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;===&lt;BR /&gt;[fsl-image-qt5-validation-imx.bb]&lt;BR /&gt;CORE_IMAGE_EXTRA_INSTALL += " \&lt;BR /&gt;mpg123 \&lt;BR /&gt;"&lt;/P&gt;&lt;P&gt;[local.conf]&lt;BR /&gt;LICENSE_FLAGS_WHITELIST += "commercial commercial_mpg123"&lt;/P&gt;&lt;P&gt;===&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And then I could use mpg123 command, but &lt;STRONG&gt;it would have some errors while using mpg123 MyFile.mp3&lt;/STRONG&gt;&lt;BR /&gt;How to resolve this problem on i.MX6SX?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[error lpog]&lt;BR /&gt;root@imx6sxsabresd:/usr/share/sounds/alsa# mpg123 MyFile.mp3&lt;BR /&gt;High Performance MPEG 1.0/2.0/2.5 Audio Player for Layers 1, 2 and 3&lt;BR /&gt;version 1.25.6; written and copyright by Michael Hipp and others&lt;BR /&gt;free software (LGPL) without any warranty but with best wishes&lt;BR /&gt;[../mpg123-1.25.6/src/libout123/modules/pulse.c:107]&lt;STRONG&gt; error: Failed to open pulse audio output: Connection refused&lt;/STRONG&gt;&lt;BR /&gt;[../mpg123-1.25.6/src/libout123/libout123.c:451] error: Found no driver out of [pulse] working with device &amp;lt;default&amp;gt;.&lt;BR /&gt;main: [../mpg123-1.25.6/src/mpg123.c:308] error: out123 error 3: failure loading driver module&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is one more question:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is&amp;nbsp;LICENSE_FLAGS_WHITELIST += "commercial commercial_mpg123" could only be added in local.conf?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have tried to add it in my&amp;nbsp;fsl-image-qt5-validation-imx.bb, and I want to add this kind of configuration in my bb file, not in local.conf, but it would have the bitbake error:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Resolving any missing task queue dependencies&lt;BR /&gt;&lt;STRONG&gt;ERROR: Nothing RPROVIDES 'mpg123'&lt;/STRONG&gt; (but /home/sevenl/FPA/1016-FPA/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5-validation-imx.bb RDEPENDS on or otherwise requires it)&lt;BR /&gt;mpg123 was skipped: because it has a restricted license not whitelisted in LICENSE_FLAGS_WHITELIST&lt;BR /&gt;NOTE: Runtime target 'mpg123' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['mpg123']&lt;BR /&gt;ERROR: Required build target 'fsl-image-qt5-validation-imx' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['fsl-image-qt5-validation-imx', 'mpg123']&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 01:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-mpg123-command-to-playback-mp3-file-would-be-failed/m-p/803499#M124112</guid>
      <dc:creator>sevenlin</dc:creator>
      <dc:date>2018-11-06T01:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using mpg123 command to playback mp3 file would be failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-mpg123-command-to-playback-mp3-file-would-be-failed/m-p/803500#M124113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the topic as below, hope helpful for you&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/898591"&gt;https://community.nxp.com/message/898591&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 08:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-mpg123-command-to-playback-mp3-file-would-be-failed/m-p/803500#M124113</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-11-06T08:42:52Z</dc:date>
    </item>
  </channel>
</rss>