<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HDMI reference clock in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-reference-clock/m-p/802739#M124017</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; ajay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That clock feed a lot of modules running to 24 Mhz. so ideally the MX8m can run HDMI with only XTLAI_27MHz and not use an external REFCLK. But it is not verified yet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Sep 2018 15:59:57 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-09-28T15:59:57Z</dc:date>
    <item>
      <title>HDMI reference clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-reference-clock/m-p/802738#M124016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;For HDMI in i.MX 8M there is two Reference clock input (crystal at XTALI/O at pin no V25/V24 and Differential HDMI_REFCLK_N/P at Pin No R1/R2), both are used for HDMI PHY.&amp;nbsp;are both clocks required or anyone clock is sufficient?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 10:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-reference-clock/m-p/802738#M124016</guid>
      <dc:creator>ajaykumar_d</dc:creator>
      <dc:date>2018-09-27T10:11:17Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI reference clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-reference-clock/m-p/802739#M124017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; ajay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That clock feed a lot of modules running to 24 Mhz. so ideally the MX8m can run HDMI with only XTLAI_27MHz and not use an external REFCLK. But it is not verified yet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 15:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-reference-clock/m-p/802739#M124017</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-09-28T15:59:57Z</dc:date>
    </item>
  </channel>
</rss>