<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does NXP i.MX6ULL SDK support Debian? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802453#M123978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you are referring to the SDK package for i.MX6ULL, it could be installed on Windows, and on Linux versions with support for the toolchain (GCC), and the downloadable code for i.MX is running bare-metal or FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are referring to the BSPs available for the i.MX6ULL, they are Linux, built on Yocto project.&lt;/P&gt;&lt;P&gt;Debian or other Linux distribution could run on i.MX processors, but they are not released nor supported by NXP. You could take a look at the following Community documents with such kind of implementations, just for reference:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-330147"&gt;https://community.nxp.com/docs/DOC-330147&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-328362"&gt;https://community.nxp.com/docs/DOC-328362&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Oct 2018 20:44:38 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-10-18T20:44:38Z</dc:date>
    <item>
      <title>Does NXP i.MX6ULL SDK support Debian?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802452#M123977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that NXP SDK developed its own Linux Yocto, but I am interested in using Debian, anyone knows if NXP SDK supports Debian for i.MX6ULL or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 10:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802452#M123977</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2018-10-17T10:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: Does NXP i.MX6ULL SDK support Debian?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802453#M123978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you are referring to the SDK package for i.MX6ULL, it could be installed on Windows, and on Linux versions with support for the toolchain (GCC), and the downloadable code for i.MX is running bare-metal or FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are referring to the BSPs available for the i.MX6ULL, they are Linux, built on Yocto project.&lt;/P&gt;&lt;P&gt;Debian or other Linux distribution could run on i.MX processors, but they are not released nor supported by NXP. You could take a look at the following Community documents with such kind of implementations, just for reference:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-330147"&gt;https://community.nxp.com/docs/DOC-330147&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-328362"&gt;https://community.nxp.com/docs/DOC-328362&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2018 20:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802453#M123978</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-10-18T20:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: Does NXP i.MX6ULL SDK support Debian?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802454#M123979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using MYIR's &lt;A href="http://www.myirtech.com/list.asp?id=561"&gt;MYS-6ULX&lt;/A&gt; board, it&amp;nbsp;Supports Linux with Debian distribution or by Yocto Project with ported QT. The board comes with yocto by default.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.myirtech.com/list.asp?id=561" title="http://www.myirtech.com/list.asp?id=561"&gt;MYS-6ULX | NXP i.MX 6UltraLite, 6ull, IoT, IND, ARM Cortex-A7, Linux, Debian, Yocto, Single Board Computer-Welcome to MY…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 03:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-NXP-i-MX6ULL-SDK-support-Debian/m-p/802454#M123979</guid>
      <dc:creator>linda_zhang</dc:creator>
      <dc:date>2018-10-31T03:51:34Z</dc:date>
    </item>
  </channel>
</rss>