<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Issue on PCIE REFCLK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802090#M123929</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for quick reply. I'll check my design about power supply with reference of your link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Oct 2018 04:09:43 GMT</pubDate>
    <dc:creator>x10</dc:creator>
    <dc:date>2018-10-18T04:09:43Z</dc:date>
    <item>
      <title>Issue on PCIE REFCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802088#M123927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, NXP&lt;/P&gt;&lt;P&gt;A Si52112-B3 pcie clock generator is used in my iMX7D based board with Linux-4.9.11 kernel. 100MHz PCIE_REFCLKIN_P/N waveform is shown as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75721iC536E9FDAE9CD365/image-size/large?v=v2&amp;amp;px=999" title="20181017-ESM7100-4-Si52112-B4-PCIECLK-R26-1.png" alt="20181017-ESM7100-4-Si52112-B4-PCIECLK-R26-1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After kernel booting up, I got following message about pcie driver loading:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75758i42E5C16BAB9DF33C/image-size/large?v=v2&amp;amp;px=999" title="20181017-ESM7100-pcie-driver-msg.JPG" alt="20181017-ESM7100-pcie-driver-msg.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As my understood, PCIE_PHY is not work properly, but can not figure out what issue with it.&lt;/P&gt;&lt;P&gt;It's appreciated for any help about this issue. Thanks!&lt;/P&gt;&lt;P&gt;BTW, the same kernel can run on iMX7D Sabre Board, and PCIE interface works fine with NVMe module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;P&gt;Emtronix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 09:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802088#M123927</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2018-10-17T09:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: Issue on PCIE REFCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802089#M123928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cheng&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at suggestions provided for similar issue on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/446903"&gt;PCI Express PLL cannot lock on about 5% of all IMX7D CPUs.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 10:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802089#M123928</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-17T10:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: Issue on PCIE REFCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802090#M123929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for quick reply. I'll check my design about power supply with reference of your link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2018 04:09:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802090#M123929</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2018-10-18T04:09:43Z</dc:date>
    </item>
    <item>
      <title>Re: Issue on PCIE REFCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802091#M123930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PCIe is working with NMVe module in my customized iMX7D board. The problem is the PCMIC not set properly. Both Si5112-B3 and Si5112-B4 are okay. PCIE_REFCLK going through with 0R instead of 0.1uF is required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 03:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-on-PCIE-REFCLK/m-p/802091#M123930</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2018-11-14T03:20:46Z</dc:date>
    </item>
  </channel>
</rss>