<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX233 Power Supply!!!</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX233-Power-Supply/m-p/209710#M12389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, the DCDC converters use DCDC_BATT pin as input. In your application, you can simply feed the 3.3V to DCDC_BATT for powering the i.MX233.&lt;/P&gt;&lt;P&gt;When using DCDC_BATT, you need to assert PSWITCH to power up the i.MX233. You can refer to Section 32.3.3 on the datasheet for more information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Oct 2012 04:29:46 GMT</pubDate>
    <dc:creator>arthur_lai</dc:creator>
    <dc:date>2012-10-16T04:29:46Z</dc:date>
    <item>
      <title>IMX233 Power Supply!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX233-Power-Supply/m-p/209709#M12388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am IMX233 for one of the projects.&lt;/P&gt;&lt;P&gt;As per the datasheet for powering up the IMX233 I need a 5.0V power supply. IMX233 contains internal DC - DC Converters to generate 1.8V, 1.2V and 3.3V and a Regulator to generate 2.5V from 3.3V. These regulators and DC-DC converters will take care of power sequencing as well.&lt;/P&gt;&lt;P&gt;Problem: I don't have a 5.0V on board to power-up DC-DC converter of IMX233 and I don't want to use a boost regulator to generate 5.0V from 3.3V and feed to IMX233.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I am thinking to power-up internal regulator to generate 2.5V from 3.3V.&amp;nbsp; &lt;/LI&gt;&lt;LI&gt;Using diodes or some regulators I will generate 1.8V and 1.2V from 3.3V to power up the analog and digital core of IMX233&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Anyone please suggest whether it is correct way of powering the IMX233 or I need to follow some other method and how can I take care of power sequencing which is required for IMX233.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;-Anand&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Oct 2012 06:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX233-Power-Supply/m-p/209709#M12388</guid>
      <dc:creator>Anan</dc:creator>
      <dc:date>2012-10-05T06:54:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMX233 Power Supply!!!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX233-Power-Supply/m-p/209710#M12389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, the DCDC converters use DCDC_BATT pin as input. In your application, you can simply feed the 3.3V to DCDC_BATT for powering the i.MX233.&lt;/P&gt;&lt;P&gt;When using DCDC_BATT, you need to assert PSWITCH to power up the i.MX233. You can refer to Section 32.3.3 on the datasheet for more information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2012 04:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX233-Power-Supply/m-p/209710#M12389</guid>
      <dc:creator>arthur_lai</dc:creator>
      <dc:date>2012-10-16T04:29:46Z</dc:date>
    </item>
  </channel>
</rss>