<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Get test image</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Get-test-image/m-p/801185#M123792</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. I think the data in memory represents a black-white-picture, doesn't it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Typically, the Bayer format contains the grayscale data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. What do I have to do to get such a picture in a format like bitmap or png?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. There is no ready to use solution to convert the captured CSI frame to a file. Try to set up a camera preview via gstreamer software as described in the Chapter 7 "Multimedia" of the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Aug 2018 11:40:41 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-08-27T11:40:41Z</dc:date>
    <item>
      <title>Get test image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-test-image/m-p/801184#M123791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I'm very new to that thematic and I hope that you can give me some hints.&lt;BR /&gt;&lt;BR /&gt;For an application I designed a PCB that can interface a camera. The camera sends bayer12, so i my IPU can only save the data without any converting. I use the parallel 16-bit-Port.&lt;BR /&gt;&lt;BR /&gt;For the first step i only want to know if my hardware is designed in a right way, so I want to see a picture.&amp;nbsp; I think the data in memory represents a black-white-picture, doesn't it?&lt;BR /&gt;What do I have to do to get such a picture in a format like bitmap or png?&lt;BR /&gt;&lt;BR /&gt;Thanks for Help!&lt;BR /&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Aug 2018 06:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-test-image/m-p/801184#M123791</guid>
      <dc:creator>michael_irsfeld</dc:creator>
      <dc:date>2018-08-20T06:08:31Z</dc:date>
    </item>
    <item>
      <title>Re: Get test image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Get-test-image/m-p/801185#M123792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. I think the data in memory represents a black-white-picture, doesn't it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Typically, the Bayer format contains the grayscale data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. What do I have to do to get such a picture in a format like bitmap or png?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. There is no ready to use solution to convert the captured CSI frame to a file. Try to set up a camera preview via gstreamer software as described in the Chapter 7 "Multimedia" of the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 11:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Get-test-image/m-p/801185#M123792</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-08-27T11:40:41Z</dc:date>
    </item>
  </channel>
</rss>