<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: MFG tool usage for NAND Flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800341#M123694</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MFG tool package is having minimal Linux system images in it. &lt;BR /&gt; How this minimal Linux system knows the address and size of NAND in a custom board?&lt;BR /&gt; It seems for either NAND or NOR there won't be any partition table on the device, the flash partitions only exist in the MTD sub system.&lt;BR /&gt; How the minimal Linux system knows the flash partitions info, so that it can write each image within at specific address for the respective image?&lt;BR /&gt; Actual NAND partition info is available in the U-boot(environment variable)/dtb and these U-boot and dtb has to be flashed on the NAND. How MFG tool will get this info?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Nov 2018 08:00:45 GMT</pubDate>
    <dc:creator>kravik</dc:creator>
    <dc:date>2018-11-28T08:00:45Z</dc:date>
    <item>
      <title>MFG tool usage for NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800339#M123692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the MFG Tool Documentation, Initially board will boot with uImage_mfg and enumerate as UMS device, then copies all images for NAND to DDR. After copying to DDR it will write all images to NAND Flash.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How MFG Tool will know the NAND partition info? so that it will write all images(U-boot, Dtb, zImage and rootfs) to NAND flash. The .vbs file is mentioning only the partition numbers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2018 12:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800339#M123692</guid>
      <dc:creator>kravik</dc:creator>
      <dc:date>2018-11-26T12:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: MFG tool usage for NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800340#M123693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The MFG loads and run minimal Linux system to memory of a target board.&lt;/P&gt;&lt;P&gt;This system is minimal, but it supports the same, including specific for the board,&lt;/P&gt;&lt;P&gt;features and parameters; in this sense it knows NAND partitioning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 04:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800340#M123693</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-11-27T04:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: MFG tool usage for NAND Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800341#M123694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MFG tool package is having minimal Linux system images in it. &lt;BR /&gt; How this minimal Linux system knows the address and size of NAND in a custom board?&lt;BR /&gt; It seems for either NAND or NOR there won't be any partition table on the device, the flash partitions only exist in the MTD sub system.&lt;BR /&gt; How the minimal Linux system knows the flash partitions info, so that it can write each image within at specific address for the respective image?&lt;BR /&gt; Actual NAND partition info is available in the U-boot(environment variable)/dtb and these U-boot and dtb has to be flashed on the NAND. How MFG tool will get this info?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 08:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-tool-usage-for-NAND-Flash/m-p/800341#M123694</guid>
      <dc:creator>kravik</dc:creator>
      <dc:date>2018-11-28T08:00:45Z</dc:date>
    </item>
  </channel>
</rss>