<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: QSPI boot from ROM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-boot-from-ROM/m-p/799879#M123642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are right, the QSPI boot is not supported in the current Boot ROM code revision. Most likely, will be implemented in further silicon releases.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jul 2018 11:37:36 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-07-31T11:37:36Z</dc:date>
    <item>
      <title>QSPI boot from ROM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-boot-from-ROM/m-p/799878#M123641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In iMX8M reference schematics, it is mentioned that QSPI boot is not supported by ROM. Does it mean that QSPI booting has some issues ? I didn't find any information on this in Errata or RM. Please confirm.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 10:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-boot-from-ROM/m-p/799878#M123641</guid>
      <dc:creator>ani10c89</dc:creator>
      <dc:date>2018-07-30T10:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI boot from ROM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-boot-from-ROM/m-p/799879#M123642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are right, the QSPI boot is not supported in the current Boot ROM code revision. Most likely, will be implemented in further silicon releases.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 11:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-boot-from-ROM/m-p/799879#M123642</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-07-31T11:37:36Z</dc:date>
    </item>
  </channel>
</rss>