<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 uboot mfgtool failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uboot-mfgtool-failed/m-p/798156#M123449</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Community:&lt;/P&gt;&lt;P&gt;I will to burn uboot into the board for&amp;nbsp;i.MX6Solo/DualLite by MFGTools(Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER), errors :&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: CmdOpreation[0]--set m_hDeviceArriveEvent.&lt;BR /&gt;ModuleID[2] LevelID[10]: CmdOpreation[0]--WaitforEvents device arrive1&lt;BR /&gt;ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0&lt;BR /&gt;ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)&lt;BR /&gt;ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\likangmao\imx6\L3.14.52_1.1.0_ga-mfg-tools\mfgtools\Profiles\Linux\OS Firmware\firmware\u-boot-imx6dlsabreauto_nand.imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;stop here,&lt;/P&gt;&lt;P&gt;There are no outputs in serial port&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Aug 2018 06:36:19 GMT</pubDate>
    <dc:creator>likangmao</dc:creator>
    <dc:date>2018-08-17T06:36:19Z</dc:date>
    <item>
      <title>uboot mfgtool failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-mfgtool-failed/m-p/798156#M123449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Community:&lt;/P&gt;&lt;P&gt;I will to burn uboot into the board for&amp;nbsp;i.MX6Solo/DualLite by MFGTools(Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER), errors :&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[1]: CmdOpreation[0]--set m_hDeviceArriveEvent.&lt;BR /&gt;ModuleID[2] LevelID[10]: CmdOpreation[0]--WaitforEvents device arrive1&lt;BR /&gt;ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0&lt;BR /&gt;ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)&lt;BR /&gt;ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\likangmao\imx6\L3.14.52_1.1.0_ga-mfg-tools\mfgtools\Profiles\Linux\OS Firmware\firmware\u-boot-imx6dlsabreauto_nand.imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;stop here,&lt;/P&gt;&lt;P&gt;There are no outputs in serial port&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 06:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-mfgtool-failed/m-p/798156#M123449</guid>
      <dc:creator>likangmao</dc:creator>
      <dc:date>2018-08-17T06:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: uboot mfgtool failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-mfgtool-failed/m-p/798157#M123450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 康茂 李&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for new board mfg tools firmware (files in /firmware folder) should be&lt;BR /&gt;updated with new ddr calibration coefficients found from ddr test:&lt;BR /&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.90&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;put them to uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg and&lt;BR /&gt;rebuild firmware using procedure described in sect.6.2 Manufacturing Tool, MFGTool&lt;BR /&gt;attached Yocto Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Aug 2018 22:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-mfgtool-failed/m-p/798157#M123450</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-19T22:56:39Z</dc:date>
    </item>
  </channel>
</rss>