<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6D Kernel display flicker</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797721#M123406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jiu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check that both lvds clocks are enabled using procedure described in&lt;/P&gt;&lt;P&gt;EB821 LDB Clock Switch Procedure &amp;amp; i.MX6 Asynchronous Clock Switching Guidelines&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf" title="https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can check if lvds clock was not used by other module, as for example below&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/465848"&gt;https://community.nxp.com/thread/465848&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jul 2018 10:27:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-10T10:27:31Z</dc:date>
    <item>
      <title>imx6D Kernel display flicker</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797720#M123405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware support 2 LVDS Display, BSP support them adaptively. But one of them flicker in Linux kernel stage. If reboot through reboot cmd(WDOG1), it will not flicker.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that this is consistence issue which generate by U-boot/Kernel IPU/Clock settings?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BSP:&lt;/P&gt;&lt;P&gt;Linux 4.1.15&amp;nbsp; (Original BSP, not apply any patch)&lt;/P&gt;&lt;P&gt;U-boot 2015.4 (have applied U-boot patch from &lt;A href="https://community.nxp.com/docs/DOC-98109"&gt;https://community.nxp.com/docs/DOC-98109&lt;/A&gt;&amp;nbsp; ).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2018 09:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797720#M123405</guid>
      <dc:creator>jiujinhong</dc:creator>
      <dc:date>2018-07-10T09:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: imx6D Kernel display flicker</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797721#M123406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jiu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check that both lvds clocks are enabled using procedure described in&lt;/P&gt;&lt;P&gt;EB821 LDB Clock Switch Procedure &amp;amp; i.MX6 Asynchronous Clock Switching Guidelines&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf" title="https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can check if lvds clock was not used by other module, as for example below&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/465848"&gt;https://community.nxp.com/thread/465848&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2018 10:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797721#M123406</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-10T10:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: imx6D Kernel display flicker</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797722#M123407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked both,&amp;nbsp; there are init_ldb_clocks in&amp;nbsp; clk-imx6q.c which do you mentioned, and there are no other use LDB clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WHY the other display is good without flicker?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jul 2018 06:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6D-Kernel-display-flicker/m-p/797722#M123407</guid>
      <dc:creator>jiujinhong</dc:creator>
      <dc:date>2018-07-11T06:02:54Z</dc:date>
    </item>
  </channel>
</rss>