<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックdocker in imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/docker-in-imx6/m-p/797361#M123385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&amp;nbsp; i want to run docker at I.mx6，but more errors，can you hlpe me？kernel 4.1.15&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;INFO[0000] libcontainerd: new containerd process, pid: 292 &lt;BR /&gt;WARN[0000] containerd: low RLIMIT_NOFILE changing to max current=1024 max=4096&lt;BR /&gt;ERRO[0001] Failed to built-in GetDriver graph zfs /var/lib/docker &lt;BR /&gt;INFO[0001] Graph migration to content-addressability took 0.00 seconds &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio weight &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio weight_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.read_bps_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.write_bps_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.read_iops_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.write_iops_device &lt;BR /&gt;WARN[0001] mountpoint for pids not found &lt;BR /&gt;INFO[0001] Loading containers: start. &lt;BR /&gt;WARN[0001] Running modprobe bridge br_netfilter failed with message: modprobe: can't change directory to '/lib/modules': No such file or directory&lt;BR /&gt;, error: exit status 1 &lt;BR /&gt;WARN[0001] Running modprobe nf_nat failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1 &lt;BR /&gt;WARN[0001] Running modprobe xt_conntrack failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1 &lt;BR /&gt;ERRO[0001] could not get initial namespace: no such file or directory &lt;BR /&gt;WARN[0001] Could not load necessary modules for IPSEC rules: Running modprobe xfrm_user failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1 &lt;BR /&gt;ERRO[0001] failed to set to initial namespace, readlink /proc/286/task/303/ns/net: no such file or directory, initns fd -1: bad file descriptor &lt;BR /&gt;INFO[0001] Default bridge (docker0) is assigned with an IP address 172.17.0.0/16. Daemon option --bip can be used to set a preferred IP address &lt;BR /&gt;ERRO[0001] failed to set to initial namespace, readlink /proc/286/task/303/ns/net: no such file or directory, initns fd -1: bad file descriptor &lt;BR /&gt;Error starting daemon: Error initializing network controller: Error creating default "bridge" network: package not installed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 25 Nov 2018 04:01:12 GMT</pubDate>
    <dc:creator>haifeng_jin</dc:creator>
    <dc:date>2018-11-25T04:01:12Z</dc:date>
    <item>
      <title>docker in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/docker-in-imx6/m-p/797361#M123385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&amp;nbsp; i want to run docker at I.mx6，but more errors，can you hlpe me？kernel 4.1.15&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;INFO[0000] libcontainerd: new containerd process, pid: 292 &lt;BR /&gt;WARN[0000] containerd: low RLIMIT_NOFILE changing to max current=1024 max=4096&lt;BR /&gt;ERRO[0001] Failed to built-in GetDriver graph zfs /var/lib/docker &lt;BR /&gt;INFO[0001] Graph migration to content-addressability took 0.00 seconds &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio weight &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio weight_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.read_bps_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.write_bps_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.read_iops_device &lt;BR /&gt;WARN[0001] Your kernel does not support cgroup blkio throttle.write_iops_device &lt;BR /&gt;WARN[0001] mountpoint for pids not found &lt;BR /&gt;INFO[0001] Loading containers: start. &lt;BR /&gt;WARN[0001] Running modprobe bridge br_netfilter failed with message: modprobe: can't change directory to '/lib/modules': No such file or directory&lt;BR /&gt;, error: exit status 1 &lt;BR /&gt;WARN[0001] Running modprobe nf_nat failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1 &lt;BR /&gt;WARN[0001] Running modprobe xt_conntrack failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1 &lt;BR /&gt;ERRO[0001] could not get initial namespace: no such file or directory &lt;BR /&gt;WARN[0001] Could not load necessary modules for IPSEC rules: Running modprobe xfrm_user failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1 &lt;BR /&gt;ERRO[0001] failed to set to initial namespace, readlink /proc/286/task/303/ns/net: no such file or directory, initns fd -1: bad file descriptor &lt;BR /&gt;INFO[0001] Default bridge (docker0) is assigned with an IP address 172.17.0.0/16. Daemon option --bip can be used to set a preferred IP address &lt;BR /&gt;ERRO[0001] failed to set to initial namespace, readlink /proc/286/task/303/ns/net: no such file or directory, initns fd -1: bad file descriptor &lt;BR /&gt;Error starting daemon: Error initializing network controller: Error creating default "bridge" network: package not installed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Nov 2018 04:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/docker-in-imx6/m-p/797361#M123385</guid>
      <dc:creator>haifeng_jin</dc:creator>
      <dc:date>2018-11-25T04:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: docker in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/docker-in-imx6/m-p/797362#M123386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to play with version of docker. Possibly previous one can help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2018 02:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/docker-in-imx6/m-p/797362#M123386</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-11-26T02:20:23Z</dc:date>
    </item>
  </channel>
</rss>