<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: core-image-* (minimal) with cmake</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-with-cmake/m-p/797299#M123379</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erik Raynolds,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The steps for adding cmake look correct. Have you checked on the bitbake log that this task was run correctly? I haven’t tested it but this would install cmake but not configure it so you would need to setup the toolchain, paths and flags in order to use cmake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Dec 2018 23:39:52 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-12-21T23:39:52Z</dc:date>
    <item>
      <title>core-image-* (minimal) with cmake</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-with-cmake/m-p/797298#M123378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am building core-image-minimal where I wanna include cmake but by building it with local.conf configured to include cmake it's not enabled and present on image&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;MACHINE ??= 'imx8qmmek'&lt;/P&gt;&lt;P&gt;DISTRO ?= 'fsl-imx-xwayland'&lt;BR /&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;BR /&gt;EXTRA_IMAGE_FEATURES ?= "debug-tweaks"&lt;BR /&gt;USER_CLASSES ?= "buildstats image-mklibs image-prelink"&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;BR /&gt;BB_DISKMON_DIRS = "\&lt;BR /&gt; STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt; STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt; STOPTASKS,/tmp,100M,100K \&lt;BR /&gt; ABORT,${TMPDIR},100M,1K \&lt;BR /&gt; ABORT,${DL_DIR},100M,1K \&lt;BR /&gt; ABORT,${SSTATE_DIR},100M,1K \&lt;BR /&gt; ABORT,/tmp,10M,1K"&lt;BR /&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;BR /&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;BR /&gt;CONF_VERSION = "1"&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;BR /&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;EXTRA_IMAGE_FEATURES_append = " debug-tweaks eclipse-debug dev-pkgs tools-debug tools-sdk ssh-server-openssh"&lt;BR /&gt;TOOLCHAIN_HOST_TASK_append = " nativesdk-cmake nativesdk-make"&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " cmake"&lt;BR /&gt;IMAGE_INSTALL_append = " openssh-sftp-server tcf-agent sshfs-fuse" &lt;BR /&gt;IMAGE_INSTALL_append = " net-tools iputils dhcpcd"&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;How to get cmake on core-image-minimal?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2018 10:59:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-with-cmake/m-p/797298#M123378</guid>
      <dc:creator>erikraynolds</dc:creator>
      <dc:date>2018-12-14T10:59:39Z</dc:date>
    </item>
    <item>
      <title>Re: core-image-* (minimal) with cmake</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-with-cmake/m-p/797299#M123379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erik Raynolds,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The steps for adding cmake look correct. Have you checked on the bitbake log that this task was run correctly? I haven’t tested it but this would install cmake but not configure it so you would need to setup the toolchain, paths and flags in order to use cmake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Dec 2018 23:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/core-image-minimal-with-cmake/m-p/797299#M123379</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-12-21T23:39:52Z</dc:date>
    </item>
  </channel>
</rss>