<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797295#M123375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes there are plans to support i.MX8M in Linux Kernel 4.14.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2018 01:49:30 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-27T01:49:30Z</dc:date>
    <item>
      <title>Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797294#M123374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I understand that currently i.MX8M BSP is only supported in Linux kernel 4.9.x. Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 06:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797294#M123374</guid>
      <dc:creator>harrytan</dc:creator>
      <dc:date>2018-09-26T06:19:55Z</dc:date>
    </item>
    <item>
      <title>Re: Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797295#M123375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes there are plans to support i.MX8M in Linux Kernel 4.14.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 01:49:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797295#M123375</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-27T01:49:30Z</dc:date>
    </item>
    <item>
      <title>Re: Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797296#M123376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know when is estimated release date for the BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Harry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 01:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797296#M123376</guid>
      <dc:creator>harrytan</dc:creator>
      <dc:date>2018-09-27T01:58:59Z</dc:date>
    </item>
    <item>
      <title>Re: Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797297#M123377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems by the end of year.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 01:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Do-NXP-has-plan-to-support-i-MX8M-in-Linux-Kernel-4-14-x/m-p/797297#M123377</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-28T01:43:22Z</dc:date>
    </item>
  </channel>
</rss>