<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: do_image_sdcard in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/do-image-sdcard/m-p/797049#M123344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello 无为 无,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The recommended Ubuntu version is 14.04, as it’s the one that has been tested. However, there is a workaround on the i.MX Yocto Project Guide on the Host Setup section for Ubuntu 16.04. Have you installed all required packages listed on this document?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Sep 2018 21:53:48 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-09-28T21:53:48Z</dc:date>
    <item>
      <title>do_image_sdcard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/do-image-sdcard/m-p/797048#M123343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI：&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I use yocto with Ubtun16.04 ,what should i do?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69623i5001E38A4BF3ADB0/image-size/large?v=v2&amp;amp;px=999" title="ui.png" alt="ui.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 04:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/do-image-sdcard/m-p/797048#M123343</guid>
      <dc:creator>无为无</dc:creator>
      <dc:date>2018-09-26T04:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: do_image_sdcard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/do-image-sdcard/m-p/797049#M123344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello 无为 无,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The recommended Ubuntu version is 14.04, as it’s the one that has been tested. However, there is a workaround on the i.MX Yocto Project Guide on the Host Setup section for Ubuntu 16.04. Have you installed all required packages listed on this document?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 21:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/do-image-sdcard/m-p/797049#M123344</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-09-28T21:53:48Z</dc:date>
    </item>
  </channel>
</rss>