<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックNo graphical output after updating GPU vivante driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796481#M123252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after updating from Linux kernel 3.14 to 4.9, I had to also update the GPU vivante driver from version imx-gpu-viv-5.0.11.p4.4-hfp to imx-gpu-viv-6.2.4.p1.8-aarch32.&lt;/P&gt;&lt;P&gt;To install the new driver, I used the following guide;&amp;nbsp;&lt;A _jive_internal="true" class="jivelink1" href="https://community.nxp.com/thread/477594" title="https://community.nxp.com/thread/477594"&gt;https://community.nxp.com/thread/477594&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is, with the new driver my graphical application does not draw anymore, and instead presents the following message that comes from the closed source library:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ES30: some draw get error and skipped during validation&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application worked properly with the old driver and the error message does not help either.&lt;/P&gt;&lt;P&gt;What does the error message mean? Why does the library throw it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a custom iMX6 dual board with new Linux kernel 4.9.88.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the link I provided the author suggests using gpu-viv kernel module version 6.2.4 with gpu-viv-driver imx-gpu-viv-5.0.11.p8.3-hfp. Unfortunately, this did not work for me at all, as the example apps threw errors and segmentation faults.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the kernel module version have to match the gpu driver version, e.g. both 6.2.4?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Sep 2018 06:42:02 GMT</pubDate>
    <dc:creator>david_schmidt</dc:creator>
    <dc:date>2018-09-26T06:42:02Z</dc:date>
    <item>
      <title>No graphical output after updating GPU vivante driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796481#M123252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after updating from Linux kernel 3.14 to 4.9, I had to also update the GPU vivante driver from version imx-gpu-viv-5.0.11.p4.4-hfp to imx-gpu-viv-6.2.4.p1.8-aarch32.&lt;/P&gt;&lt;P&gt;To install the new driver, I used the following guide;&amp;nbsp;&lt;A _jive_internal="true" class="jivelink1" href="https://community.nxp.com/thread/477594" title="https://community.nxp.com/thread/477594"&gt;https://community.nxp.com/thread/477594&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is, with the new driver my graphical application does not draw anymore, and instead presents the following message that comes from the closed source library:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ES30: some draw get error and skipped during validation&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application worked properly with the old driver and the error message does not help either.&lt;/P&gt;&lt;P&gt;What does the error message mean? Why does the library throw it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a custom iMX6 dual board with new Linux kernel 4.9.88.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the link I provided the author suggests using gpu-viv kernel module version 6.2.4 with gpu-viv-driver imx-gpu-viv-5.0.11.p8.3-hfp. Unfortunately, this did not work for me at all, as the example apps threw errors and segmentation faults.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the kernel module version have to match the gpu driver version, e.g. both 6.2.4?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 06:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796481#M123252</guid>
      <dc:creator>david_schmidt</dc:creator>
      <dc:date>2018-09-26T06:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: No graphical output after updating GPU vivante driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796482#M123253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why not installed all the 4.9BSP? basically the GPU 6.2 has support on GC7000 for the i.MX8Q but you don´t need it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 14:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796482#M123253</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-10-01T14:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: No graphical output after updating GPU vivante driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796483#M123254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bio_TICFSL,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where can I download the GPU driver sources for 4.9BSP? What versions of the GPU driver belong to 4.9BSP?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 05:36:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/796483#M123254</guid>
      <dc:creator>david_schmidt</dc:creator>
      <dc:date>2018-10-02T05:36:30Z</dc:date>
    </item>
    <item>
      <title>Re: No graphical output after updating GPU vivante driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/1243247#M170629</link>
      <description>&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;I encounter the same error message ([1] ES30: some draw get error and skipped during validation) in one of our devices during long run and I was curious to understand what this error message mean? Did you perform any investigation to understand about the error and its background? Please share your inputs on this case.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The device which we are working on is a custom platform based out of i.MX6 Dual core processor. The software running on the platform is Yocto thud with QT 5.15.2. The Linux kernel version is 4.9.168 and the GPU driver version is&amp;nbsp;6.2.4.p1.8-r0 (&lt;A href="https://github.com/Freescale/kernel-module-imx-gpu-viv.git" target="_blank"&gt;https://github.com/Freescale/kernel-module-imx-gpu-viv.git&lt;/A&gt; Tag - 6.2.4.p1.8).&amp;nbsp;We have observed this error after six hours of usage, On the console, we have observed this error and Qt fails to render frame to the display.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your time.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shajin &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 12:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-graphical-output-after-updating-GPU-vivante-driver/m-p/1243247#M170629</guid>
      <dc:creator>shajin</dc:creator>
      <dc:date>2021-03-10T12:03:50Z</dc:date>
    </item>
  </channel>
</rss>