<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 ULL PowerUpSeuence in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796472#M123249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please tell us about the following points in Power-Up Sequence of i.MX6ULL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. IMX6ULLIEC.pdf (DataSheet) has no sequence description for the following power supply.Would you mind thinking that there is no sequence order if it is after VDD_SNVS_IN?&lt;BR /&gt;-NVCC_DRAM&lt;BR /&gt;-NVCC_GPIO,NVCC_UART,NVCC_ENET,NVCC_SD1,NVCC_NAND,NVCC_CSI,NVCC_LCD&lt;BR /&gt;-VDDA_ADC_3P3,ADC_VREFH&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Is there any problem with the POWER UP sequence(Step) below?&lt;/P&gt;&lt;P&gt;Also, at Step 4, the NVCC (* 1) power supply is still OFF, but can not leak to the NVCC (* 1) power supply terminal (* 2)?&lt;BR /&gt;-Step1 : VDD_SNVS_IN (+3.3V)&lt;BR /&gt;-Step2 : VDD_HIGH_IN (+3.3V)&lt;BR /&gt;-Step3 : VDD_SOC_IN (+1.35V)&lt;BR /&gt;-Step4 : NVCC_DRAM (+1.35V)&lt;BR /&gt;-Step5 : NVCC(*1) / VDDA_ADC_3P3 / ADC_VREF(+3.3V)&lt;BR /&gt; (*1)NVCC : NVCC_GPIO,NVCC_UART,NVCC_ENET,NVCC_SD1,NVCC_NAND,NVCC_CSI,NVCC_LCD&lt;/P&gt;&lt;P&gt;(*2)e.g. GPIO1 , GPIO2 , GPIO3 , GPIO4 , GPIO5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanking you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Oct 2018 08:09:13 GMT</pubDate>
    <dc:creator>mikitakashi</dc:creator>
    <dc:date>2018-10-16T08:09:13Z</dc:date>
    <item>
      <title>i.MX6 ULL PowerUpSeuence</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796472#M123249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please tell us about the following points in Power-Up Sequence of i.MX6ULL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. IMX6ULLIEC.pdf (DataSheet) has no sequence description for the following power supply.Would you mind thinking that there is no sequence order if it is after VDD_SNVS_IN?&lt;BR /&gt;-NVCC_DRAM&lt;BR /&gt;-NVCC_GPIO,NVCC_UART,NVCC_ENET,NVCC_SD1,NVCC_NAND,NVCC_CSI,NVCC_LCD&lt;BR /&gt;-VDDA_ADC_3P3,ADC_VREFH&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Is there any problem with the POWER UP sequence(Step) below?&lt;/P&gt;&lt;P&gt;Also, at Step 4, the NVCC (* 1) power supply is still OFF, but can not leak to the NVCC (* 1) power supply terminal (* 2)?&lt;BR /&gt;-Step1 : VDD_SNVS_IN (+3.3V)&lt;BR /&gt;-Step2 : VDD_HIGH_IN (+3.3V)&lt;BR /&gt;-Step3 : VDD_SOC_IN (+1.35V)&lt;BR /&gt;-Step4 : NVCC_DRAM (+1.35V)&lt;BR /&gt;-Step5 : NVCC(*1) / VDDA_ADC_3P3 / ADC_VREF(+3.3V)&lt;BR /&gt; (*1)NVCC : NVCC_GPIO,NVCC_UART,NVCC_ENET,NVCC_SD1,NVCC_NAND,NVCC_CSI,NVCC_LCD&lt;/P&gt;&lt;P&gt;(*2)e.g. GPIO1 , GPIO2 , GPIO3 , GPIO4 , GPIO5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanking you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 08:09:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796472#M123249</guid>
      <dc:creator>mikitakashi</dc:creator>
      <dc:date>2018-10-16T08:09:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 ULL PowerUpSeuence</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796473#M123250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi miki&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. all other power supplies can be powered up in any order after step&lt;/P&gt;&lt;P&gt;described in i.MX6ULL Datasheet sect.4.2.1 Power-Up Sequence:&lt;/P&gt;&lt;P&gt;"VDD_HIGH_IN should be turned on before VDD_SOC_IN."&lt;/P&gt;&lt;P&gt;2. this is correct power up sequence&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 23:31:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796473#M123250</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-16T23:31:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 ULL PowerUpSeuence</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796474#M123251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 23:17:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-ULL-PowerUpSeuence/m-p/796474#M123251</guid>
      <dc:creator>mikitakashi</dc:creator>
      <dc:date>2018-10-17T23:17:19Z</dc:date>
    </item>
  </channel>
</rss>