<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART serial connection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796252#M123221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor. Thanks for the tip. I'll check it out today. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Dec 2018 18:21:50 GMT</pubDate>
    <dc:creator>info33</dc:creator>
    <dc:date>2018-12-16T18:21:50Z</dc:date>
    <item>
      <title>UART serial connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796250#M123219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone. i'm hoping i can get some help with something i have been working off and on for a while. I have a SABRESD i.MX 6Dual/6Quad on a custom board from some OEM manufacturer. A few of them actually. I want to follow &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-101842"&gt;this tutorial&lt;/A&gt; to put linux on it. Looks pretty straight fwd. The problem i'm having is im unable to connect to the serial port to stop the U-Boot process if there is one at all. Currently there is Android on it so it's probably Fastboot. I'm guessing that the custom board does not allow a serial connection so it's not tampered with. I found what i think is a tx/rx on the board that connects to the chip for development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70823i7DE50ACCC9212FD6/image-size/large?v=v2&amp;amp;px=999" title="freescaleSabresd.png" alt="freescaleSabresd.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the pinout of the connection to the chip. the far left and right are vcc and ground while the two in the center connect to the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70867i6737F400F23AF2B9/image-size/large?v=v2&amp;amp;px=999" title="20181213_123144-1.jpg" alt="20181213_123144-1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and the headers i soldered onto it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70913i86F9E63D5E3A34F2/image-size/large?v=v2&amp;amp;px=999" title="20181213_123033-1.jpg" alt="20181213_123033-1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the noob questions. This is all very new to me and this is all i have managed to put together. If there is indeed Fastboot on it, is there a way i can flash U-boot without access to the serial connection that will later have a serial connection for me to connect to?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Dec 2018 21:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796250#M123219</guid>
      <dc:creator>info33</dc:creator>
      <dc:date>2018-12-13T21:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: UART serial connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796251#M123220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Craig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can program images with mfg tool from below link using usb port,&lt;/P&gt;&lt;P&gt;serial connection is not needed.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Dec 2018 05:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796251#M123220</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-15T05:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: UART serial connection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796252#M123221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor. Thanks for the tip. I'll check it out today. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Dec 2018 18:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-serial-connection/m-p/796252#M123221</guid>
      <dc:creator>info33</dc:creator>
      <dc:date>2018-12-16T18:21:50Z</dc:date>
    </item>
  </channel>
</rss>