<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRunning EGL demos on Freescale's 12_09_01_oneiric release</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Running-EGL-demos-on-Freescale-s-12-09-01-oneiric-release/m-p/209143#M12320</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am successfully running this rootfs on the Sabrelite board and would like to run some GL demos.&lt;/P&gt;&lt;P&gt;Are there any per-packaged demos for A/V playback and GL rendering under X11 ?&lt;/P&gt;&lt;P&gt;I installed es2_info and when I run it console message says it is using software rendering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vasant&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 Dec 2012 06:32:29 GMT</pubDate>
    <dc:creator>Vasant</dc:creator>
    <dc:date>2012-12-15T06:32:29Z</dc:date>
    <item>
      <title>Running EGL demos on Freescale's 12_09_01_oneiric release</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-EGL-demos-on-Freescale-s-12-09-01-oneiric-release/m-p/209143#M12320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am successfully running this rootfs on the Sabrelite board and would like to run some GL demos.&lt;/P&gt;&lt;P&gt;Are there any per-packaged demos for A/V playback and GL rendering under X11 ?&lt;/P&gt;&lt;P&gt;I installed es2_info and when I run it console message says it is using software rendering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vasant&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Dec 2012 06:32:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-EGL-demos-on-Freescale-s-12-09-01-oneiric-release/m-p/209143#M12320</guid>
      <dc:creator>Vasant</dc:creator>
      <dc:date>2012-12-15T06:32:29Z</dc:date>
    </item>
    <item>
      <title>Re: Running EGL demos on Freescale's 12_09_01_oneiric release</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-EGL-demos-on-Freescale-s-12-09-01-oneiric-release/m-p/209144#M12321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is the answer from our engineer. If this is good answer, please click Correct Answer.&lt;/P&gt;&lt;P&gt;------------------------------------------------&lt;/P&gt;&lt;P&gt;-When you see white screen, then the DRI and GLX is not setup correctly. Please make sure the following present in the&amp;nbsp; /var/log/Xorg.0./log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[1623101.082] (II) [drm] DRM interface version 1.4&lt;/P&gt;&lt;P&gt;[1623101.082] (II) [drm] DRM open master succeeded.&lt;/P&gt;&lt;P&gt;[1623101.082] (II) VIVANTE(0): [drm] Using the DRM lock SAREA also for drawables.&lt;/P&gt;&lt;P&gt;[1623101.082] (II) VIVANTE(0): [drm] framebuffer handle = 0x18800000&lt;/P&gt;&lt;P&gt;[1623101.082] (II) VIVANTE(0): [drm] added 1 reserved context for kernel&lt;/P&gt;&lt;P&gt;[1623101.082] (II) VIVANTE(0): X context handle = 0x1&lt;/P&gt;&lt;P&gt;[1623101.082] (II) VIVANTE(0): [drm] installed DRM signal handler&lt;/P&gt;&lt;P&gt;[1623101.082] (II) VIVANTE(0): [DRI] installation complete&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Install Vivante GPU Base driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dpkg -i gpu-viv-bin-mx6q_&amp;lt;KERNEL VERSION&amp;gt;-&amp;lt;RELEASE VESRION&amp;gt;_armel.deb&lt;/P&gt;&lt;P&gt;2. Install Kernel module driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dpkg -i kernel_&amp;lt;KERNEL VERSION&amp;gt;-imx_&amp;lt;RELEASE VESRION&amp;gt;_armel.deb&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After this debian package is installed, please double check drm.ko and &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vivante.ko is properly installed.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you don't use prebuilt linux kernel, you need rebuild the kernel module &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; while build your own Linux kernel. Please refer to Linux reference manual &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for building DRM.&lt;/P&gt;&lt;P&gt;---------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2013 07:20:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-EGL-demos-on-Freescale-s-12-09-01-oneiric-release/m-p/209144#M12321</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-03-28T07:20:21Z</dc:date>
    </item>
  </channel>
</rss>