<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TAMPER DETECTION: WHICH PINS &amp; WHICH REGISTER? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TAMPER-DETECTION-WHICH-PINS-WHICH-REGISTER/m-p/795225#M123116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Project: Connect a wire onto the tamper Pins of the iMX6ULL-EVK Board and if you cut it, the board will detect it and &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; delete the security keys.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem: Do I connect the wire to a SNVS_TAMPER Pin and GND?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; If thats possible, what Registers do I have to set in order to delete the keys?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Aug 2018 07:28:24 GMT</pubDate>
    <dc:creator>imme_jakobeit</dc:creator>
    <dc:date>2018-08-17T07:28:24Z</dc:date>
    <item>
      <title>TAMPER DETECTION: WHICH PINS &amp; WHICH REGISTER?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TAMPER-DETECTION-WHICH-PINS-WHICH-REGISTER/m-p/795225#M123116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Project: Connect a wire onto the tamper Pins of the iMX6ULL-EVK Board and if you cut it, the board will detect it and &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; delete the security keys.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem: Do I connect the wire to a SNVS_TAMPER Pin and GND?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; If thats possible, what Registers do I have to set in order to delete the keys?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 07:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TAMPER-DETECTION-WHICH-PINS-WHICH-REGISTER/m-p/795225#M123116</guid>
      <dc:creator>imme_jakobeit</dc:creator>
      <dc:date>2018-08-17T07:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: TAMPER DETECTION: WHICH PINS &amp; WHICH REGISTER?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TAMPER-DETECTION-WHICH-PINS-WHICH-REGISTER/m-p/795226#M123117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Imme &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check answer on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/1027146?commentID=1027146#comment-1027146" title="https://community.nxp.com/message/1027146?commentID=1027146#comment-1027146"&gt;https://community.nxp.com/message/1027146?commentID=1027146#comment-1027146&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 23:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TAMPER-DETECTION-WHICH-PINS-WHICH-REGISTER/m-p/795226#M123117</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-17T23:22:14Z</dc:date>
    </item>
  </channel>
</rss>