<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx uart RS485 rx not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794481#M123027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if dte or dce mode used, please check&lt;/P&gt;&lt;P&gt;Table 86. UART I/O Configuration vs. Mode i.MX6DQ Datasheet&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf"&gt;http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and check signal on i.mx uart rx pad with oscilloscope.&lt;/P&gt;&lt;P&gt;Also may be useful to check i.mx uart module register settings with jtag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2018 00:00:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-06T00:00:31Z</dc:date>
    <item>
      <title>imx uart RS485 rx not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794480#M123026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working on the RS485, but the rx always couldnot work.&lt;/P&gt;&lt;P&gt;Hardware: imx6qsabresd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The dts is as:&lt;/P&gt;&lt;P&gt;&amp;amp;uart2 {&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; pinctrl-names = "default";&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; pinctrl-0=&amp;lt;&amp;amp;pinctrl_uart2&amp;gt;;&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; uart-has-rtscts;&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; linux,rs485-enabled-at-boot-time;&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; pinctrl_uart2: uart2grp {&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; fsl,pins = &amp;lt;&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; MX6QDL_PAD_EIM_D26__UART2_TX_DATA|&amp;nbsp; 0x1b0b1&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; MX6QDL_PAD_EIM_D27__UART2_RX_DATA|&amp;nbsp; 0x1b0b1&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; MX6QDL_PAD_EIM_D28__UART2_CTS_B||&amp;nbsp;&amp;nbsp; 0x1b0b1&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; &amp;gt;;&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I configure the rs485 flag as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; struct serial_rs485 rs485conf;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (ioctl (pf, TIOCGRS485, &amp;amp;rs485conf) &amp;lt; 0) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Error reading ioctl port");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;rs485conf.flags |= SER_RS485_ENABLED;&lt;/P&gt;&lt;P&gt;ioctl (pf, TIOCSRS485, &amp;amp;rs485conf);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I use microcom to debug(I add a print at rts active/inactive), it could send out data but couldnot receive.&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# microcom -s 115200 /dev/ttymxc1&lt;BR /&gt;imx-uart 21e8000.serial: imx_set_termios !!!!!&lt;BR /&gt;imx-uart 21e8000.serial: imx port rts active&lt;BR /&gt;imx-uart 21e8000.serial: imx_set_termios !!!!!&lt;BR /&gt;imx-uart 21e8000.serial: imx port rts active&lt;BR /&gt;imx-uart 21e8000.serial: imx rts inactive&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give a hand?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Wei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 07:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794480#M123026</guid>
      <dc:creator>chenwei45</dc:creator>
      <dc:date>2018-09-05T07:40:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx uart RS485 rx not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794481#M123027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if dte or dce mode used, please check&lt;/P&gt;&lt;P&gt;Table 86. UART I/O Configuration vs. Mode i.MX6DQ Datasheet&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf"&gt;http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and check signal on i.mx uart rx pad with oscilloscope.&lt;/P&gt;&lt;P&gt;Also may be useful to check i.mx uart module register settings with jtag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 00:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794481#M123027</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-06T00:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: imx uart RS485 rx not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794482#M123028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Many thanks for your help. The issue was resolved for the connector we use is not for 485 but 232. :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 03:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-uart-RS485-rx-not-working/m-p/794482#M123028</guid>
      <dc:creator>chenwei45</dc:creator>
      <dc:date>2018-09-06T03:00:44Z</dc:date>
    </item>
  </channel>
</rss>