<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 hdmi without ddc or i2c</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793891#M122964</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm work with imx6q custon board.&lt;/P&gt;&lt;P&gt;We made changes on Android O, using HDMI as the display output.&lt;/P&gt;&lt;P&gt;But we are not connected to I2C or DDC to HDMI, only TMDS and CLOCK, and there is no HPD signal and CEC signal.&lt;BR /&gt;We hope to force the output of the HDMI signal. What should we do?&lt;BR /&gt;I look forward to hearing from you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 07:31:52 GMT</pubDate>
    <dc:creator>xiaojun_huang</dc:creator>
    <dc:date>2018-09-25T07:31:52Z</dc:date>
    <item>
      <title>hdmi without ddc or i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793891#M122964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm work with imx6q custon board.&lt;/P&gt;&lt;P&gt;We made changes on Android O, using HDMI as the display output.&lt;/P&gt;&lt;P&gt;But we are not connected to I2C or DDC to HDMI, only TMDS and CLOCK, and there is no HPD signal and CEC signal.&lt;BR /&gt;We hope to force the output of the HDMI signal. What should we do?&lt;BR /&gt;I look forward to hearing from you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 07:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793891#M122964</guid>
      <dc:creator>xiaojun_huang</dc:creator>
      <dc:date>2018-09-25T07:31:52Z</dc:date>
    </item>
    <item>
      <title>Re: hdmi without ddc or i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793892#M122965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at tutorial from boundary devices&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/dvi-support-on-i-mx6-boards/" title="https://boundarydevices.com/dvi-support-on-i-mx6-boards/"&gt;DVI Support on i.MX6 boards - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 23:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793892#M122965</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-25T23:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: hdmi without ddc or i2c</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793893#M122966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your replay.&lt;/P&gt;&lt;P&gt;This patch uses HDMI_DVI_IH_STAT instead of HPD detection,&lt;/P&gt;&lt;P&gt;but I hope that the TMDS signal can be forced out without interrupt method.&lt;/P&gt;&lt;P&gt;Is this feasible?&lt;BR /&gt;How should I modify it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 04:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hdmi-without-ddc-or-i2c/m-p/793893#M122966</guid>
      <dc:creator>xiaojun_huang</dc:creator>
      <dc:date>2018-09-26T04:07:06Z</dc:date>
    </item>
  </channel>
</rss>