<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB Host in IMX6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793637#M122942</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chandra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Now I have to do the same thing with Android tab connected to IMX6UL board.&lt;/P&gt;&lt;P&gt;&amp;gt;Both charging and communication should happen as a Virtual com?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the same configuration is also possible, Android tablet acting as host and IMX6UL board&lt;/P&gt;&lt;P&gt;as USB Device configured as CDC. If both Android and IMX6UL board support charging&lt;/P&gt;&lt;P&gt;this is also feasible option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2018 10:36:56 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-12T10:36:56Z</dc:date>
    <item>
      <title>USB Host in IMX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793636#M122941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a I.MX6UL custom board, we are using one OTG port as Host with ID pin configured to charge the Android tablet connected to that port. Here my Android Tab USB acts like Device and IMX6UL usb port acts as Host. So i have emulated the USB as gadget serial and I am able to communicate to a Ubuntu machine via Serial read and write.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I have to do the same thing with Android tab connected to IMX6UL board. Both charging and communication should happen as a Virtual com?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 09:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793636#M122941</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2018-07-09T09:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: USB Host in IMX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793637#M122942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chandra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Now I have to do the same thing with Android tab connected to IMX6UL board.&lt;/P&gt;&lt;P&gt;&amp;gt;Both charging and communication should happen as a Virtual com?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the same configuration is also possible, Android tablet acting as host and IMX6UL board&lt;/P&gt;&lt;P&gt;as USB Device configured as CDC. If both Android and IMX6UL board support charging&lt;/P&gt;&lt;P&gt;this is also feasible option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 10:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793637#M122942</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-12T10:36:56Z</dc:date>
    </item>
    <item>
      <title>Re: USB Host in IMX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793638#M122943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you igor,&lt;/P&gt;&lt;P&gt;I will get back to you once the android application is done&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jul 2018 09:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-in-IMX6UL/m-p/793638#M122943</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2018-07-21T09:08:41Z</dc:date>
    </item>
  </channel>
</rss>