<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Inflexion Linux Application</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209056#M12294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I did it in ROM mode .... any ways what is the significance of ROM mode any Idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2012 12:23:15 GMT</pubDate>
    <dc:creator>Hitex</dc:creator>
    <dc:date>2012-02-06T12:23:15Z</dc:date>
    <item>
      <title>Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209053#M12291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I created a Linux GUI in inflexion as per the workshop documents given on mentor graphic website.&lt;/P&gt;&lt;P&gt;As per the document we have to create a complete microsd card for Inflexion.The PDF I am attaching.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now thw GUI works with the mmc card.However I want to run the final ARM executable directly into IMX53 Ubuntu.When I am trying to run the executable in Ubuntu it is giving errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How I can create a ARM executable in Inflexion which will run directly on IMX53&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2012 10:43:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209053#M12291</guid>
      <dc:creator>Hitex</dc:creator>
      <dc:date>2012-02-06T10:43:36Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209054#M12292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118794iFA300B6F64BB2DE3/image-size/large?v=v2&amp;amp;px=999" title="371-Error.JPG" alt="371-Error.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2012 10:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209054#M12292</guid>
      <dc:creator>Hitex</dc:creator>
      <dc:date>2012-02-06T10:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209055#M12293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You have to re-package theme in ROM mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2012 12:20:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209055#M12293</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2012-02-06T12:20:21Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209056#M12294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I did it in ROM mode .... any ways what is the significance of ROM mode any Idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2012 12:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209056#M12294</guid>
      <dc:creator>Hitex</dc:creator>
      <dc:date>2012-02-06T12:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209057#M12295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hitesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Ubuntu Linux bundled with the i.MX5 series does not have framebuffer support (fbdev). The Inflexion UI for Linux product only works with the LTIB Linux release.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The Ubuntu Linux for i.MX5 uses X11, porting to this is possible; however requires the purchase of the full Inflexion UI product.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Phil.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2012 09:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209057#M12295</guid>
      <dc:creator>PhilBrumby</dc:creator>
      <dc:date>2012-02-07T09:32:54Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209058#M12296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phil,&lt;/P&gt;&lt;P&gt;As per my understanding Inflexion is free for IMX53.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Hitesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2012 09:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209058#M12296</guid>
      <dc:creator>Hitex</dc:creator>
      <dc:date>2012-03-01T09:46:34Z</dc:date>
    </item>
    <item>
      <title>Re: Inflexion Linux Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209059#M12297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hitesh,&lt;/P&gt;&lt;P&gt;Inflexion UI is free for use with the iMX5x series under LTIB (using fbdev). However the use under Ubuntu requires an X11 porting layer for the runtime engine, and is not part of the Freescale pre-paid package of Inflexion it provides to it's down line customers.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Phil.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Mar 2012 13:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inflexion-Linux-Application/m-p/209059#M12297</guid>
      <dc:creator>PhilBrumby</dc:creator>
      <dc:date>2012-03-14T13:45:24Z</dc:date>
    </item>
  </channel>
</rss>