<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックVGA problem in IMX53 Sabre ARD</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VGA-problem-in-IMX53-Sabre-ARD/m-p/208977#M12284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone tried using VGA on the IMX53 sabre ard board (Board: MX53-ARD Rev. B&amp;nbsp; as per uboot)&lt;/P&gt;&lt;P&gt;I use LTIB 11.05.01 kernel but dont see anything coming on the monitor screen (montior LED keeps blinking)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried bootargs for the video as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;video=mxcdi1fb:GBR24,1024x768M-16@60 di1_primary ard-vga&lt;/P&gt;&lt;PRE&gt;video=mxcdi1fb:RGB666,XGA di1_primary ldb=di1 ard-vga&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: Also I observe when I have ard-vga in my bootags, then the ethernet doent come up (no eth0 device is reported when I do&amp;nbsp; ifconfig -a )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Madhu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Feb 2012 06:57:33 GMT</pubDate>
    <dc:creator>MadhusudhananRa</dc:creator>
    <dc:date>2012-02-07T06:57:33Z</dc:date>
    <item>
      <title>VGA problem in IMX53 Sabre ARD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-problem-in-IMX53-Sabre-ARD/m-p/208977#M12284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone tried using VGA on the IMX53 sabre ard board (Board: MX53-ARD Rev. B&amp;nbsp; as per uboot)&lt;/P&gt;&lt;P&gt;I use LTIB 11.05.01 kernel but dont see anything coming on the monitor screen (montior LED keeps blinking)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried bootargs for the video as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;video=mxcdi1fb:GBR24,1024x768M-16@60 di1_primary ard-vga&lt;/P&gt;&lt;PRE&gt;video=mxcdi1fb:RGB666,XGA di1_primary ldb=di1 ard-vga&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: Also I observe when I have ard-vga in my bootags, then the ethernet doent come up (no eth0 device is reported when I do&amp;nbsp; ifconfig -a )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Madhu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2012 06:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-problem-in-IMX53-Sabre-ARD/m-p/208977#M12284</guid>
      <dc:creator>MadhusudhananRa</dc:creator>
      <dc:date>2012-02-07T06:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: VGA problem in IMX53 Sabre ARD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VGA-problem-in-IMX53-Sabre-ARD/m-p/208978#M12285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Madhu,&lt;/P&gt;&lt;P&gt;Have a look at the i.MX53 ARD Linux BSP release notes on page 5&lt;/P&gt;&lt;P&gt;It says:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Support VGA output.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Due to the pin conflict with WEIM, please note the following steps when running VGA on MX53 ARD RevB board:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -add boot option "ard-vga" in kernel launch command line.&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For example &lt;STRONG&gt;video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga ard-vga ldb=off&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -Flash the images on SD or NAND and avoid to use Ethernet.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -HW configuration: Short PIN1-2 for J14 and J16 on CPU board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Hans-Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2012 13:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VGA-problem-in-IMX53-Sabre-ARD/m-p/208978#M12285</guid>
      <dc:creator>Hans-PeterRosin</dc:creator>
      <dc:date>2012-02-07T13:58:13Z</dc:date>
    </item>
  </channel>
</rss>