<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6UL ECSPI only sends 8 bits in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ECSPI-only-sends-8-bits/m-p/791907#M122669</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi justinwave&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check patch and community activities on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://patchwork.kernel.org/patch/9146065/" title="https://patchwork.kernel.org/patch/9146065/"&gt;spi-imx: imx6q add single burst transfer support - Patchwork&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309866"&gt;https://community.nxp.com/thread/309866&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you want the SS always be asserted during a transfer, you should configure the cs pin as gpio in the dts.&lt;BR /&gt;For example: &lt;BR /&gt;MX6SL_PAD_ECSPI1_SS0__GPIO4_IO11&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x80000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jun 2018 00:43:08 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-06-19T00:43:08Z</dc:date>
    <item>
      <title>IMX6UL ECSPI only sends 8 bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ECSPI-only-sends-8-bits/m-p/791906#M122668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a custom board modeled off the IMX6UL evk board and am using the 4.9.11 fsl release kernel. I have a device attached to ECSPI 1. The device registers and I am able to open the device from a user application. However, when I attempt to read or write to the device, I only see 8 bits are transfered, not the 32 bits that the device is expecting. So, for each read and write I perform, only the first byte of the message is actually sent. The clock and the chip select appear to be correct while the 8 bits are transferred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I need to set the ECSPI1_CONREG[20:31] burst length to 32 bits in a word? And if so, do you have any references or examples on how to do this? Or any other ideas that may be causing this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 18:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ECSPI-only-sends-8-bits/m-p/791906#M122668</guid>
      <dc:creator>justinwave</dc:creator>
      <dc:date>2018-06-18T18:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL ECSPI only sends 8 bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ECSPI-only-sends-8-bits/m-p/791907#M122669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi justinwave&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check patch and community activities on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://patchwork.kernel.org/patch/9146065/" title="https://patchwork.kernel.org/patch/9146065/"&gt;spi-imx: imx6q add single burst transfer support - Patchwork&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309866"&gt;https://community.nxp.com/thread/309866&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you want the SS always be asserted during a transfer, you should configure the cs pin as gpio in the dts.&lt;BR /&gt;For example: &lt;BR /&gt;MX6SL_PAD_ECSPI1_SS0__GPIO4_IO11&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x80000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2018 00:43:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-ECSPI-only-sends-8-bits/m-p/791907#M122669</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-19T00:43:08Z</dc:date>
    </item>
  </channel>
</rss>