<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debug UART selection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Debug-UART-selection/m-p/791775#M122659</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi prabhu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in uboot one can change uart port number in #define CONFIG_MXC_UART_BASE in uboot/include/configs/*board*.h file&lt;/P&gt;&lt;P&gt;please also check structure iomux_v3_cfg_t const uart1_pads[] in uboot/..mx6ul_14x14_evk/mx6ul_14x14_evk.c&lt;/P&gt;&lt;P&gt;and "console" parameter in Table 11. Common kernel boot parameters attached Release Notes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 23:50:23 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-25T23:50:23Z</dc:date>
    <item>
      <title>Debug UART selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debug-UART-selection/m-p/791774#M122658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi Sir,&lt;/P&gt;&lt;P&gt;Currently i am using&amp;nbsp;UART1_TX_DATA &amp;amp; UART1_RX_DATA as Debug UART instead of that can i use alternative pins(UART2_TX_DATA &amp;amp; UART2_RX_DATA, UART3_TX_DATA &amp;amp; UART3_RX_DATA, UART4_TX_DATA &amp;amp; UART4_RX_DATA, UART5_TX_DATA &amp;amp; UART5_RX_DATA) any of this for Debug UART ?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 09:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debug-UART-selection/m-p/791774#M122658</guid>
      <dc:creator>prabhu1</dc:creator>
      <dc:date>2018-09-25T09:14:46Z</dc:date>
    </item>
    <item>
      <title>Re: Debug UART selection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debug-UART-selection/m-p/791775#M122659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi prabhu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in uboot one can change uart port number in #define CONFIG_MXC_UART_BASE in uboot/include/configs/*board*.h file&lt;/P&gt;&lt;P&gt;please also check structure iomux_v3_cfg_t const uart1_pads[] in uboot/..mx6ul_14x14_evk/mx6ul_14x14_evk.c&lt;/P&gt;&lt;P&gt;and "console" parameter in Table 11. Common kernel boot parameters attached Release Notes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 23:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debug-UART-selection/m-p/791775#M122659</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-25T23:50:23Z</dc:date>
    </item>
  </channel>
</rss>