<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is i.MX28 MMU enabled during DDR test in the IMX_OBDS? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-i-MX28-MMU-enabled-during-DDR-test-in-the-IMX-OBDS/m-p/791497#M122622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torus1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is the MMU/d-cache enabled during DDR test of OBDS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is the MMU/d-cache enabled during normal boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mmu is configured by fuse HW_OCOTP_ROM7:0x8002C210:1 MMU_DISABLE&lt;/P&gt;&lt;P&gt;described in Table 12-9. General ROM Bit in ROM7 OCOTP Bank&lt;/P&gt;&lt;P&gt;i.MX28 Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Oct 2018 10:22:50 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-10-15T10:22:50Z</dc:date>
    <item>
      <title>Is i.MX28 MMU enabled during DDR test in the IMX_OBDS?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-i-MX28-MMU-enabled-during-DDR-test-in-the-IMX-OBDS/m-p/791496#M122621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to try DDR test in the IMX_OBDS for my custom i.MX28 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the MMU/d-cache enabled during DDR test of OBDS?&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;OBDS: On-Board Diagnostic Suit for the i.MX28(REV 1)&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fsps%2Fdownload%2Flicense.jsp%3FcolCode%3DIMX_OBDS" rel="nofollow" target="_blank"&gt;https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX_OBDS&lt;/A&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition,&lt;/P&gt;&lt;P&gt;I found following descriptions in the i.MX28 reference manual;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;- To accelerate the boot process, the MMU/d-cache is enabled during the time consuming&lt;BR /&gt;HAB authentication process (RSA).&lt;/P&gt;&lt;P&gt;- MMU and D-Cache are enabled in default to speed up HAB functions&lt;BR /&gt;execution speed.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the MMU/d-cache enabled during normal boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2018 08:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-i-MX28-MMU-enabled-during-DDR-test-in-the-IMX-OBDS/m-p/791496#M122621</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2018-10-15T08:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: Is i.MX28 MMU enabled during DDR test in the IMX_OBDS?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-i-MX28-MMU-enabled-during-DDR-test-in-the-IMX-OBDS/m-p/791497#M122622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torus1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is the MMU/d-cache enabled during DDR test of OBDS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is the MMU/d-cache enabled during normal boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mmu is configured by fuse HW_OCOTP_ROM7:0x8002C210:1 MMU_DISABLE&lt;/P&gt;&lt;P&gt;described in Table 12-9. General ROM Bit in ROM7 OCOTP Bank&lt;/P&gt;&lt;P&gt;i.MX28 Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2018 10:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-i-MX28-MMU-enabled-during-DDR-test-in-the-IMX-OBDS/m-p/791497#M122622</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-15T10:22:50Z</dc:date>
    </item>
  </channel>
</rss>