<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: cfimager windows 10 issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791303#M122589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically we are creating three partions for sdcard using cfimager for imx28 as follows :&lt;/P&gt;&lt;P&gt;1. VFAT partiton which contains firmware&lt;BR /&gt;2. Ext3 partiton for rootfs &lt;BR /&gt;3. another Ext3 partition for our rough work&lt;/P&gt;&lt;P&gt;The arguments for Creation of these patitons works well in windows 7 without any error and cfimager contains reformatting the drive for flashing files.&lt;/P&gt;&lt;P&gt;In windows 10 this is not happpening and error we are getting is as follows&lt;/P&gt;&lt;P&gt;Error -37 Failed to write sector&lt;/P&gt;&lt;P&gt;The above error we are getting while writing Extra data and to overcome this problem we formatted disk using diskpart and running cfimager works well.&lt;/P&gt;&lt;P&gt;Is There is a problem in windows or priveleged access in batch file/command prompt which is unknown for me.&lt;/P&gt;&lt;P&gt;Please let me know any solution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 25 Nov 2018 04:58:54 GMT</pubDate>
    <dc:creator>shashikanthirem</dc:creator>
    <dc:date>2018-11-25T04:58:54Z</dc:date>
    <item>
      <title>cfimager windows 10 issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791301#M122587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;cfimager.exe is not creating image properly in latest version of windows 10..please send me solution&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Nov 2018 04:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791301#M122587</guid>
      <dc:creator>shashikanthirem</dc:creator>
      <dc:date>2018-11-22T04:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager windows 10 issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791302#M122588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shashikant, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cfimager is not tested on windows 10, but which error are you seeing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2018 15:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791302#M122588</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-11-23T15:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager windows 10 issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791303#M122589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically we are creating three partions for sdcard using cfimager for imx28 as follows :&lt;/P&gt;&lt;P&gt;1. VFAT partiton which contains firmware&lt;BR /&gt;2. Ext3 partiton for rootfs &lt;BR /&gt;3. another Ext3 partition for our rough work&lt;/P&gt;&lt;P&gt;The arguments for Creation of these patitons works well in windows 7 without any error and cfimager contains reformatting the drive for flashing files.&lt;/P&gt;&lt;P&gt;In windows 10 this is not happpening and error we are getting is as follows&lt;/P&gt;&lt;P&gt;Error -37 Failed to write sector&lt;/P&gt;&lt;P&gt;The above error we are getting while writing Extra data and to overcome this problem we formatted disk using diskpart and running cfimager works well.&lt;/P&gt;&lt;P&gt;Is There is a problem in windows or priveleged access in batch file/command prompt which is unknown for me.&lt;/P&gt;&lt;P&gt;Please let me know any solution.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Nov 2018 04:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791303#M122589</guid>
      <dc:creator>shashikanthirem</dc:creator>
      <dc:date>2018-11-25T04:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager windows 10 issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791304#M122590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any updates on the solutions?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Dec 2018 15:59:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/791304#M122590</guid>
      <dc:creator>shashikanthirem</dc:creator>
      <dc:date>2018-12-02T15:59:38Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager windows 10 issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/1531018#M195860</link>
      <description>I occurred same issue when run cfimager with Win10,  see error as below.&lt;BR /&gt;C:\Users\NXA16874\git\try_env\flow\bin&amp;gt;cfimager -raw -offset 0x400 -f gpu1_sd_image.bin -d D&lt;BR /&gt;Exception found: -22 Failed to locate scsi device</description>
      <pubDate>Fri, 30 Sep 2022 09:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-windows-10-issue/m-p/1531018#M195860</guid>
      <dc:creator>PowerTian</dc:creator>
      <dc:date>2022-09-30T09:29:04Z</dc:date>
    </item>
  </channel>
</rss>