<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: root file system not properly installed? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system-not-properly-installed/m-p/790704#M122522</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Atis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to prevent mfg tool hanging when loading custom kernel it is necessary to&lt;/P&gt;&lt;P&gt;rebuild mfg tools firmware (files in /firmware folder) with new calibration settings&lt;/P&gt;&lt;P&gt;found from ddr test (put them in uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg)&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.92&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;using procedure in sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 00:27:03 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-25T00:27:03Z</dc:date>
    <item>
      <title>root file system not properly installed?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system-not-properly-installed/m-p/790703#M122521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear users,&lt;BR /&gt;&lt;BR /&gt;I have encountered a problem for i.mx6DL board. I have a custom kernel, dtb and rootfs. When I use tftpboot, I can install everything, and everything works. However, I would like to do this over USB, not internet, so I tried using MFGtool2. MFGtool successfully uploads U-boot and custom files, however, when I boot, it just says loading kernel and stays there. I found it that if I erase.part rootfs, and put it back on via tftp it boots and everything works again. Therefore I suspect something wrong with the way MFGtool installs the rootfs. I looked in the batch file of MFGtool, but I did not find anything that could help me. I tried changing the compression from .bz2 to .tgz since it accepts several formats, but so far no luck. It just stays at 'booting kernel' and that is about it.&amp;nbsp; Has anyone encountered this, or has an idea how to approach this problem?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Atis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Sep 2018 12:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/root-file-system-not-properly-installed/m-p/790703#M122521</guid>
      <dc:creator>a_cace</dc:creator>
      <dc:date>2018-09-24T12:43:30Z</dc:date>
    </item>
    <item>
      <title>Re: root file system not properly installed?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/root-file-system-not-properly-installed/m-p/790704#M122522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Atis&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to prevent mfg tool hanging when loading custom kernel it is necessary to&lt;/P&gt;&lt;P&gt;rebuild mfg tools firmware (files in /firmware folder) with new calibration settings&lt;/P&gt;&lt;P&gt;found from ddr test (put them in uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg)&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V2.92&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;using procedure in sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 00:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/root-file-system-not-properly-installed/m-p/790704#M122522</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-25T00:27:03Z</dc:date>
    </item>
  </channel>
</rss>