<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can not control GPIO after set it to pull high. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-not-control-GPIO-after-set-it-to-pull-high/m-p/789600#M122388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tsung&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if ODE (open drain) is set using jtag, or there is some external connection&lt;/P&gt;&lt;P&gt;to that pin, which may affect behavior, please check sect.36.4.433 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_NAND_CS2_B) i.MX6DQ Reference Manual &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Freference-manual%2FIMX6DQRM.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Sep 2018 23:31:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-04T23:31:24Z</dc:date>
    <item>
      <title>Can not control GPIO after set it to pull high.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-not-control-GPIO-after-set-it-to-pull-high/m-p/789599#M122387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I'm working on i.MX6 Quad sabre-SD platform and build Android 6 as my image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to control GPIO in u-boot.&lt;/P&gt;&lt;P&gt;According to my customize u-boot, I modify bootload/bootloader/u-boot/board/freescale/FX100/FX100.c like below.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define FX_GPIO_INIT (PAD_CTL_PUS_100K_DOWN)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void enable_lvds(struct display_info_t const *dev)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* LVDS_PWR_ON */&lt;BR /&gt; imx_iomux_v3_setup_pad(MX6_PAD_NANDF_CS2__GPIO6_IO15 | MUX_PAD_CTRL(FX_GPIO_INIT));&lt;BR /&gt; /* LVDS_BL_ON */&lt;BR /&gt; imx_iomux_v3_setup_pad(MX6_PAD_NANDF_CS3__GPIO6_IO16 | MUX_PAD_CTRL(FX_GPIO_INIT));&lt;BR /&gt; /* PAD_SD1_DAT3 for pwm ,GPIO mode */&lt;BR /&gt; imx_iomux_v3_setup_pad(MX6_PAD_SD1_DAT3__GPIO1_IO21 | MUX_PAD_CTRL(FX_GPIO_INIT));&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; gpio_direction_output(BL_PWM, 0);// winmate BL pwm to low level&lt;BR /&gt; gpio_direction_output(LVDS_PWR_ON, 0);//winmate Frank BL pwr off&lt;BR /&gt; gpio_direction_output(LVDS_BL_ON, 0);// winmate frank for panel pwr seq panel pwr off&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; gpio_set_value(BL_PWM, 0);&lt;BR /&gt; gpio_set_value(LVDS_PWR_ON, 0);&lt;BR /&gt; gpio_set_value(LVDS_BL_ON, 0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setup_display();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gpio_set_value(BL_PWM, 1);&lt;BR /&gt; gpio_set_value(LVDS_PWR_ON, 1);&lt;BR /&gt; gpio_set_value(LVDS_BL_ON, 1);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;As you can see, I tried to define&amp;nbsp;&lt;SPAN style="background-color: #f6f6f6;"&gt;FX_GPIO_INIT to change gpio to 100K PULL DOWN..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;But when I set&amp;nbsp;&lt;SPAN&gt;LVDS_PWR_ON to&amp;nbsp; 0 and set it back to 1, it won't work.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;SPAN&gt;I can not control it.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;SPAN&gt;Is there any possibility that I have to set other register mode for&amp;nbsp;NANDF_CS2 ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;SPAN&gt;Or what else can I do to solve this situation?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;&lt;SPAN&gt;Thanks in Advanced!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 11:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-not-control-GPIO-after-set-it-to-pull-high/m-p/789599#M122387</guid>
      <dc:creator>wangtsungli</dc:creator>
      <dc:date>2018-09-04T11:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: Can not control GPIO after set it to pull high.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-not-control-GPIO-after-set-it-to-pull-high/m-p/789600#M122388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tsung&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if ODE (open drain) is set using jtag, or there is some external connection&lt;/P&gt;&lt;P&gt;to that pin, which may affect behavior, please check sect.36.4.433 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_NAND_CS2_B) i.MX6DQ Reference Manual &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Freference-manual%2FIMX6DQRM.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 23:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-not-control-GPIO-after-set-it-to-pull-high/m-p/789600#M122388</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-04T23:31:24Z</dc:date>
    </item>
  </channel>
</rss>