<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 MIPI on Virtual Chanel 0 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788932#M122275</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i solved my problem, but i don't understand why it works.&lt;/P&gt;&lt;P&gt;I have set the Virtual Chanel in my Sensor to 0.&amp;nbsp; So the Sensor Data are forwarded to IPU0 CSI0.&lt;/P&gt;&lt;P&gt;There is an entry in the device tree file for the MIPI.&lt;/P&gt;&lt;P&gt;There i set:&amp;nbsp; ipu_id = &amp;lt;0&amp;gt;;&amp;nbsp; csi_id = &amp;lt;0&amp;gt;;&amp;nbsp;&amp;nbsp; v_channel = &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;&amp;lt;1&amp;gt;&lt;/STRONG&gt;&lt;/SPAN&gt;;&lt;/P&gt;&lt;P&gt;Now I get sensible sensor data, although the VC is not the same&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now i have e new problem.&amp;nbsp; I loose the frame synchronization.&lt;BR /&gt;I got the error :&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;The following information is written in data sheet:&lt;/P&gt;&lt;P&gt;New Frame before end-of-frame error indication of Channel interrupt.&lt;/P&gt;&lt;P&gt;This bit is the status bit of New IDMAC_ Frame before end-of-frame&lt;/P&gt;&lt;P&gt;error interrupt of Channel 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The senor frame don't start at the beginning of the buffer. So i get a half picture from frame n and a half picture from frame n+1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jun 2018 14:36:50 GMT</pubDate>
    <dc:creator>joachimjaehn</dc:creator>
    <dc:date>2018-06-22T14:36:50Z</dc:date>
    <item>
      <title>IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788928#M122271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi @all&lt;/P&gt;&lt;P&gt;I use the IMX.6QDL on an&amp;nbsp; DartMX6 Board from Varicite. I would like to use an MIPI CMOS Gray scale Senor (IMX290). I have&amp;nbsp;running an other Sensor on Virtual Chanel 1. It works without problems. But it is Impossible to change the Virtual Chanel from the IMX290. So i have to use the Virtual Chanel 0. Now i got problems if i change the virtual Chanel of the old Sensor to 0 and the new sensor will not work too.&amp;nbsp;See Attach.&amp;nbsp;If I darken the sensor the image will also darken. So the data comes from the sensor. But I don't get a stable picture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both sensors use MIPI with 4Lanes, a data rate of 594Mbps and the data format RAW10. I can't find the differences between VC0 and VC1.&lt;/P&gt;&lt;P&gt;VC0 &amp;gt;&amp;nbsp; MUX Parallel &amp;gt;&amp;nbsp; IPU0 CSI0 &amp;gt; SMFC&amp;nbsp; IDMAC &amp;gt; Memory&lt;/P&gt;&lt;P&gt;VC1 &amp;gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IPU0 CSI1 &amp;gt; SMFC &amp;gt; IDMAC &amp;gt; Memory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find the Problem. can anyone help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 15:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788928#M122271</guid>
      <dc:creator>joachimjaehn</dc:creator>
      <dc:date>2018-06-15T15:46:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788929#M122272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi joachim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can recheck port selection using IOMUXC_GPR13 and&lt;/P&gt;&lt;P&gt;Figure 19-1. CSI2IPU gasket connectivity i.MX6SDL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf" title="http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf"&gt;http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SDLRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Jun 2018 04:48:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788929#M122272</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-16T04:48:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788930#M122273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply, but i use the IMX6QDL not SDL. The registers you mean are IOMUXC_GPR1:MIPI_IPU1_MUX and IOMUXC_GPR1:MIPI_IPU2_MUX. They set the mux between parallel and MIPI. If i don't configure them, i get on data.&amp;nbsp;That's not my problem. I get data. These also come from the sensor. But I don't get a clean picture. It looks like the data is messed up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 08:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788930#M122273</guid>
      <dc:creator>joachimjaehn</dc:creator>
      <dc:date>2018-06-18T08:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788931#M122274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for usage different virtual channels one can look at example on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328548"&gt;iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 11:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788931#M122274</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-06-18T11:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788932#M122275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i solved my problem, but i don't understand why it works.&lt;/P&gt;&lt;P&gt;I have set the Virtual Chanel in my Sensor to 0.&amp;nbsp; So the Sensor Data are forwarded to IPU0 CSI0.&lt;/P&gt;&lt;P&gt;There is an entry in the device tree file for the MIPI.&lt;/P&gt;&lt;P&gt;There i set:&amp;nbsp; ipu_id = &amp;lt;0&amp;gt;;&amp;nbsp; csi_id = &amp;lt;0&amp;gt;;&amp;nbsp;&amp;nbsp; v_channel = &lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;&amp;lt;1&amp;gt;&lt;/STRONG&gt;&lt;/SPAN&gt;;&lt;/P&gt;&lt;P&gt;Now I get sensible sensor data, although the VC is not the same&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now i have e new problem.&amp;nbsp; I loose the frame synchronization.&lt;BR /&gt;I got the error :&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001&lt;/P&gt;&lt;P&gt;The following information is written in data sheet:&lt;/P&gt;&lt;P&gt;New Frame before end-of-frame error indication of Channel interrupt.&lt;/P&gt;&lt;P&gt;This bit is the status bit of New IDMAC_ Frame before end-of-frame&lt;/P&gt;&lt;P&gt;error interrupt of Channel 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The senor frame don't start at the beginning of the buffer. So i get a half picture from frame n and a half picture from frame n+1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2018 14:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788932#M122275</guid>
      <dc:creator>joachimjaehn</dc:creator>
      <dc:date>2018-06-22T14:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788933#M122276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you solve the frame_no_sync problem? I face the same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 04:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788933#M122276</guid>
      <dc:creator>leavs</dc:creator>
      <dc:date>2019-01-24T04:07:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788934#M122277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;no,sorry. &lt;BR /&gt;But i know a way to handle it. &lt;BR /&gt;I start the sensor with a very low frame rate(1-4fps). I grow up the frame rate after the first 5 frames. &lt;BR /&gt;Now i get clean frames. B&lt;SPAN class=""&gt;&lt;SPAN class="" title=""&gt;ut i still get the error message&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class="" title=""&gt;I hope that helps&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 09:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788934#M122277</guid>
      <dc:creator>joachimjaehn</dc:creator>
      <dc:date>2019-01-25T09:39:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 MIPI on Virtual Chanel 0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788935#M122278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day,&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="302116" data-username="joachimjaehn" href="https://community.nxp.com/people/joachimjaehn" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: none; font-size: 1.286rem;"&gt;joachim Jaehn&lt;/A&gt;.&amp;nbsp;You managed to start the camera?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 08:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-MIPI-on-Virtual-Chanel-0/m-p/788935#M122278</guid>
      <dc:creator>nesterovich2797</dc:creator>
      <dc:date>2020-06-22T08:13:49Z</dc:date>
    </item>
  </channel>
</rss>