<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX6 MIPI Virtual Chanel 0 Problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788900#M122264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; useful doc :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94312"&gt;https://community.nxp.com/docs/DOC-94312&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jul 2018 02:31:39 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-07-06T02:31:39Z</dc:date>
    <item>
      <title>I.MX6 MIPI Virtual Chanel 0 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788897#M122261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi @ all&lt;/P&gt;&lt;P&gt;I use the IMX.6QDL on an DartMX6 Board from Varicite. I would like to use an MIPI CMOS Gray scale Senor (IMX290). I have running an other Sensor on Virtual Chanel 1. It works without problems. But it is Impossible to change the Virtual Chanel from the IMX290. So i have to use the Virtual Chanel 0. Now i got problems if i change the virtual Chanel of the old Sensor to 0 and the new sensor will not work too. See Attach. If I darken the sensor the image will also darken. So the data comes from the sensor. But I don't get a stable picture.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Both sensors use MIPI with 4Lanes, a data rate of 594Mbps and the data format RAW10. I can't find the differences between VC0 and VC1.&lt;/P&gt;&lt;P&gt;VC0 = &amp;gt; MUX Parallel =&amp;gt; IPU0 CSI0 =&amp;gt; SMFC =&amp;gt; IDMAC =&amp;gt; Memory&lt;/P&gt;&lt;P&gt;VC1 =&amp;gt; IPU0 CSI1 =&amp;gt; SMFC =&amp;gt; IDMAC =&amp;gt; Memory&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I can't find the Problem. can anyone help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 15:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788897#M122261</guid>
      <dc:creator>joachimjaehn</dc:creator>
      <dc:date>2018-06-15T15:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 MIPI Virtual Chanel 0 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788898#M122262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joachim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also starting IMX290 driver development now. Do you care to collaborate with me? Two pair of eyes will see more!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Hendrik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jun 2018 07:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788898#M122262</guid>
      <dc:creator>hbeij</dc:creator>
      <dc:date>2018-06-30T07:06:03Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 MIPI Virtual Chanel 0 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788899#M122263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perhaps, the following from section&amp;nbsp;3.2 (MIPI CSI2 Virtual Channel Issue) of&amp;nbsp;i.MX6 IPU TVIN Application Note,&lt;/P&gt;&lt;P&gt;Rev. 0, helps to clarify the issue:&lt;/P&gt;&lt;P&gt;&amp;nbsp; "For some MIPI CSI2 TVIN chips, when software sets their virtual channel to not 0, they will only&lt;BR /&gt;send MIPI long packages (video data) to other virtual channel but keep MIPI short packages (timing data&lt;BR /&gt;such as frame start, frame end) on virtual channel 0. Such kind of TVIN chip can’t be supported by iMX6&lt;BR /&gt;with not 0 virtual channel. They must work at virtual channel 0.&lt;BR /&gt;With such TVIN chip, to hardware design, if parallel CSI0 is also used for another camera sensor,&lt;BR /&gt;then the two cameras will fail to work together."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332679"&gt;iMX6 IPU TVIN Application Notes&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2018 14:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788899#M122263</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-07-05T14:15:46Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 MIPI Virtual Chanel 0 Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788900#M122264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; useful doc :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94312"&gt;https://community.nxp.com/docs/DOC-94312&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jul 2018 02:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-MIPI-Virtual-Chanel-0-Problem/m-p/788900#M122264</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-07-06T02:31:39Z</dc:date>
    </item>
  </channel>
</rss>