<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Failed to mount rootfs from emmc in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788871#M122246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;may be useful to look on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.yoctoproject.org/pipermail/meta-freescale/2017-March/020307.html" title="https://lists.yoctoproject.org/pipermail/meta-freescale/2017-March/020307.html"&gt;[meta-freescale] [3rdparty PATCH 0/4] Allow easier use of mainline-based BSP on i.MX products (Nitrogen6x support)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Sep 2018 09:03:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-09-05T09:03:37Z</dc:date>
    <item>
      <title>Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788866#M122241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! I moved to latest BSP releas - imx_4.9.88_2.0.0_ga - and failed to boot with it.&lt;/P&gt;&lt;P&gt;Booting stops on mounting rootfs and after some time it prints sdhci register dumps and kernel panic stack. And while linux retrying to send commands to emmc, short blinks occures on display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I work with our custom board with imx6d, I haven't SD slots - only soldered emmc (samsung klmag2ge4a-a001). Bootloader boots from spi-nor, read kernel and device-tree from 1-st partition of emmc and try to mount rootfs from 2-nd partition of this emmc.&lt;BR /&gt;Kernel 4.9.11 works fine on this board. On sbresd board both 4.9.11 and 4.9.88 kernels works fine - boots from SD and from emmc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see in boot log that kernel can't open root device (mmcblk3p2) but u-boot works fine with it, I can map it to OTG by 'ums' command and write image from host machine without errors. And previous kernel 4.9.11 boots fine with the same configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov&lt;/A&gt;‌, can you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Jun 28 2018 - 18:35:30 +0500) &lt;BR /&gt; &lt;BR /&gt;CPU: Freescale i.MX6D rev1.5 at 792MHz &lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 29C &lt;BR /&gt;Reset cause: POR &lt;BR /&gt;Model: Freescale i.MX6 Dual Infratest Board &lt;BR /&gt;Board: MX6-Infratest &lt;BR /&gt;DRAM: 512 MiB &lt;BR /&gt;PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21 &lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2 &lt;BR /&gt;*** Warning - bad CRC, using default environment &lt;BR /&gt; &lt;BR /&gt;No panel detected: default to SVGA050 &lt;BR /&gt;Display: SVGA050 (800x600) &lt;BR /&gt;In: serial &lt;BR /&gt;Out: serial &lt;BR /&gt;Err: serial &lt;BR /&gt;switch to partitions #0, OK &lt;BR /&gt;mmc2(part 0) is current device &lt;BR /&gt;Net: No ethernet found. &lt;BR /&gt;Hit any key to stop autoboot: 0 &lt;BR /&gt;switch to partitions #0, OK &lt;BR /&gt;mmc2(part 0) is current device &lt;BR /&gt;reading zImage &lt;BR /&gt;7069608 bytes read in 201 ms (33.5 MiB/s) &lt;BR /&gt;Booting from mmc ... &lt;BR /&gt;reading imx6-infratest.dtb &lt;BR /&gt;42289 bytes read in 17 ms (2.4 MiB/s) &lt;BR /&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x6bdfa8 ] &lt;BR /&gt;## Flattened Device Tree blob at 18000000 &lt;BR /&gt; Booting using the fdt blob at 0x18000000 &lt;BR /&gt; Using Device Tree in place at 18000000, end 1800d530 &lt;BR /&gt; &lt;BR /&gt;Starting kernel ... &lt;BR /&gt; &lt;BR /&gt;Booting Linux on physical CPU 0x0 &lt;BR /&gt;Linux version 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #15 SMP PREEMPT Tue Se&lt;BR /&gt;p 4 14:24:16 +05 2018 &lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d &lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache &lt;BR /&gt;OF: fdt:Machine model: Freescale i.MX6 Dual Infratest Board &lt;BR /&gt;Reserved memory: created CMA memory pool at 0x80000000, size 256 MiB &lt;BR /&gt;OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool &lt;BR /&gt;Memory policy: Data cache writealloc &lt;BR /&gt;percpu: Embedded 14 pages/cpu @8efbc000 s25996 r8192 d23156 u57344 &lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130560 &lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk3p2 rootwait rw &lt;BR /&gt;PID hash table entries: 1024 (order: 0, 4096 bytes) &lt;BR /&gt;Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) &lt;BR /&gt;Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) &lt;BR /&gt;Memory: 242228K/524288K available (9216K kernel code, 490K rwdata, 3208K rodata, 1024K init, 464K bss, 19916K reserve&lt;BR /&gt;d, 262144K cma-reserved, 0K highmem) &lt;BR /&gt;Virtual kernel memory layout: &lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB) &lt;BR /&gt; fixmap : 0xffc00000 - 0xfff00000 (3072 kB) &lt;BR /&gt; vmalloc : 0x90800000 - 0xff800000 (1776 MB) &lt;BR /&gt; lowmem : 0x80000000 - 0x90000000 ( 256 MB) &lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) &lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB) &lt;BR /&gt; .text : 0x80008000 - 0x80a00000 (10208 kB) &lt;BR /&gt; .init : 0x80e00000 - 0x80f00000 (1024 kB) &lt;BR /&gt; .data : 0x80f00000 - 0x80f7a8e0 ( 491 kB) &lt;BR /&gt; .bss : 0x80f7c000 - 0x80ff03f8 ( 465 kB) &lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 &lt;BR /&gt;Preemptible hierarchical RCU implementation. &lt;BR /&gt; Build-time adjustment of leaf fanout to 32. &lt;BR /&gt; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2. &lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2 &lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16 &lt;BR /&gt;L2C-310 errata 752271 769419 enabled &lt;BR /&gt;L2C-310 enabling early BRESP for Cortex-A9 &lt;BR /&gt;L2C-310 full line of zeros enabled for Cortex-A9 &lt;BR /&gt;L2C-310 ID prefetch enabled, offset 16 lines &lt;BR /&gt;L2C-310 dynamic clock gating enabled, standby mode enabled &lt;BR /&gt;L2C-310 cache controller enabled, 16 ways, 1024 kB &lt;BR /&gt;L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001 &lt;BR /&gt;Switching to timer-based delay loop, resolution 333ns &lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns &lt;BR /&gt;clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns &lt;BR /&gt;Console: colour dummy device 80x30 &lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000) &lt;BR /&gt;pid_max: default: 32768 minimum: 301 &lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) &lt;BR /&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) &lt;BR /&gt;CPU: Testing write buffer coherency: ok &lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 &lt;BR /&gt;Setting up static identity map for 0x10100000 - 0x10100058 &lt;BR /&gt;CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 &lt;BR /&gt;Brought up 2 CPUs &lt;BR /&gt;SMP: Total of 2 processors activated (12.00 BogoMIPS). &lt;BR /&gt;CPU: All CPU(s) started in SVC mode. &lt;BR /&gt;devtmpfs: initialized &lt;BR /&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 &lt;BR /&gt;clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns &lt;BR /&gt;futex hash table entries: 512 (order: 3, 32768 bytes) &lt;BR /&gt;pinctrl core: initialized pinctrl subsystem &lt;BR /&gt;NET: Registered protocol family 16 &lt;BR /&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations &lt;BR /&gt;cpuidle: using governor menu &lt;BR /&gt;CPU identified as i.MX6Q, silicon rev 1.5 &lt;BR /&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. &lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 4 bytes. &lt;BR /&gt;imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver &lt;BR /&gt;imx-gpc 20dc000.gpc: Registered imx-gpc &lt;BR /&gt;mxs-dma 110000.dma-apbh: initialized &lt;BR /&gt;SCSI subsystem initialized &lt;BR /&gt;usbcore: registered new interface driver usbfs &lt;BR /&gt;usbcore: registered new interface driver hub &lt;BR /&gt;usbcore: registered new device driver usb &lt;BR /&gt;2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator &lt;BR /&gt;2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator &lt;BR /&gt;i2c i2c-2: IMX I2C adapter registered &lt;BR /&gt;i2c i2c-2: can't use DMA, using PIO instead. &lt;BR /&gt;Linux video capture interface: v2.00 &lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered &lt;BR /&gt;&lt;SPAN&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&lt;SPAN&gt;&amp;gt; &lt;/SPAN&gt;&lt;BR /&gt;PTP clock support registered &lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7) &lt;BR /&gt;MIPI CSI2 driver module loaded &lt;BR /&gt;imx rpmsg driver is registered. &lt;BR /&gt;Advanced Linux Sound Architecture Driver Initialized. &lt;BR /&gt;Bluetooth: Core ver 2.22 &lt;BR /&gt;NET: Registered protocol family 31 &lt;BR /&gt;Bluetooth: HCI device and connection manager initialized &lt;BR /&gt;Bluetooth: HCI socket layer initialized &lt;BR /&gt;Bluetooth: L2CAP socket layer initialized &lt;BR /&gt;Bluetooth: SCO socket layer initialized &lt;BR /&gt;clocksource: Switched to clocksource mxc_timer1 &lt;BR /&gt;VFS: Disk quotas dquot_6.6.0 &lt;BR /&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) &lt;BR /&gt;NET: Registered protocol family 2 &lt;BR /&gt;TCP established hash table entries: 2048 (order: 1, 8192 bytes) &lt;BR /&gt;TCP bind hash table entries: 2048 (order: 2, 16384 bytes) &lt;BR /&gt;TCP: Hash tables configured (established 2048 bind 2048) &lt;BR /&gt;UDP hash table entries: 256 (order: 1, 8192 bytes) &lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) &lt;BR /&gt;NET: Registered protocol family 1 &lt;BR /&gt;RPC: Registered named UNIX socket transport module. &lt;BR /&gt;RPC: Registered udp transport module. &lt;BR /&gt;RPC: Registered tcp transport module. &lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module. &lt;BR /&gt;hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available &lt;BR /&gt;Bus freq driver module loaded &lt;BR /&gt;workingset: timestamp_bits=30 max_order=17 bucket_order=0 &lt;BR /&gt;NFS: Registering the id_resolver key type &lt;BR /&gt;Key type id_resolver registered &lt;BR /&gt;Key type id_legacy registered &lt;BR /&gt;jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. &lt;BR /&gt;fuse init (API version 7.26) &lt;BR /&gt;bounce: pool size: 64 pages &lt;BR /&gt;io scheduler noop registered &lt;BR /&gt;io scheduler deadline registered &lt;BR /&gt;io scheduler cfq registered (default) &lt;BR /&gt;imx-weim 21b8000.weim: Driver registered. &lt;BR /&gt;mxc_sdc_fb fb@0: registered mxc display driver lcd &lt;BR /&gt;Console: switching to colour frame buffer device 100x37 &lt;BR /&gt;imx-sdma 20ec000.sdma: no iram assigned, using external mem &lt;BR /&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3 &lt;BR /&gt;pfuze100-regulator 2-0008: Full layer: 2, Metal layer: 1 &lt;BR /&gt;pfuze100-regulator 2-0008: FAB: 0, FIN: 0 &lt;BR /&gt;pfuze100-regulator 2-0008: pfuze100 found. &lt;BR /&gt;usb_otg_vbus: supplied by SWBST &lt;BR /&gt;usb_h1_vbus: supplied by SWBST &lt;BR /&gt;VGEN2: Bringing 800000uV into 1200000-1200000uV &lt;BR /&gt;VGEN4: Bringing 1800000uV into 2500000-2500000uV &lt;BR /&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 25, base_baud = 5000000) is a IMX &lt;BR /&gt;console [ttymxc0] enabled &lt;BR /&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 61, base_baud = 5000000) is a IMX &lt;BR /&gt;21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 62, base_baud = 5000000) is a IMX &lt;BR /&gt;21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 63, base_baud = 5000000) is a IMX &lt;BR /&gt;imx sema4 driver is registered. &lt;BR /&gt;[drm] Initialized &lt;BR /&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0 &lt;BR /&gt;brd: module loaded &lt;BR /&gt;loop: module loaded &lt;BR /&gt;libphy: Fixed MDIO Bus: probed &lt;BR /&gt;CAN device driver interface &lt;BR /&gt;usbcore: registered new interface driver kaweth &lt;BR /&gt;pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver &lt;BR /&gt;usbcore: registered new interface driver pegasus &lt;BR /&gt;usbcore: registered new interface driver rtl8150 &lt;BR /&gt;usbcore: registered new interface driver r8152 &lt;BR /&gt;usbcore: registered new interface driver asix &lt;BR /&gt;usbcore: registered new interface driver ax88179_178a &lt;BR /&gt;usbcore: registered new interface driver cdc_ether &lt;BR /&gt;usbcore: registered new interface driver net1080 &lt;BR /&gt;usbcore: registered new interface driver cdc_subset &lt;BR /&gt;usbcore: registered new interface driver zaurus &lt;BR /&gt;usbcore: registered new interface driver cdc_ncm &lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver &lt;BR /&gt;ehci-mxc: Freescale On-Chip EHCI Host driver &lt;BR /&gt;usbcore: registered new interface driver usb-storage &lt;BR /&gt;usbcore: registered new interface driver usb_ehset_test &lt;BR /&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator &lt;BR /&gt;ci_hdrc ci_hdrc.1: EHCI Host Controller &lt;BR /&gt;ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1 &lt;BR /&gt;ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00 &lt;BR /&gt;hub 1-0:1.0: USB hub found &lt;BR /&gt;hub 1-0:1.0: 1 port detected &lt;BR /&gt;mousedev: PS/2 mouse device common for all mice &lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0 &lt;BR /&gt;i2c /dev entries driver &lt;BR /&gt;IR NEC protocol handler initialized &lt;BR /&gt;IR RC5(x/sz) protocol handler initialized &lt;BR /&gt;IR RC6 protocol handler initialized &lt;BR /&gt;IR JVC protocol handler initialized &lt;BR /&gt;IR Sony protocol handler initialized &lt;BR /&gt;IR SANYO protocol handler initialized &lt;BR /&gt;IR Sharp protocol handler initialized &lt;BR /&gt;IR MCE Keyboard/mouse protocol handler initialized &lt;BR /&gt;IR XMP protocol handler initialized &lt;BR /&gt;mxc_v4l2_output v4l2_out: V4L2 device registered as video16 &lt;BR /&gt;mxc_v4l2_output v4l2_out: V4L2 device registered as video17 &lt;BR /&gt;Bluetooth: HCI UART driver ver 2.3 &lt;BR /&gt;Bluetooth: HCI UART protocol H4 registered &lt;BR /&gt;Bluetooth: HCI UART protocol BCSP registered &lt;BR /&gt;Bluetooth: HCI UART protocol ATH3K registered &lt;BR /&gt;usbcore: registered new interface driver bcm203x &lt;BR /&gt;usbcore: registered new interface driver btusb &lt;BR /&gt;usbcore: registered new interface driver ath3k &lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver &lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman &lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper &lt;BR /&gt;mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA &lt;BR /&gt;mxc_vpu 2040000.vpu_fsl: VPU initialized &lt;BR /&gt;mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed &lt;BR /&gt;caam 2100000.caam: ERA source: CAAMVID. &lt;BR /&gt;caam 2100000.caam: AXI pipeline throttling enabled. &lt;BR /&gt;caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4) &lt;BR /&gt;job rings = 2, qi = 0 &lt;BR /&gt;caam_jr 2101000.jr0: Entropy delay = 3200 &lt;BR /&gt;mmc3: new DDR MMC card at address 0001 &lt;BR /&gt;mmcblk3: mmc3:0001 MAG2GA 14.6 GiB &lt;BR /&gt;mmcblk3boot0: mmc3:0001 MAG2GA partition 1 2.00 MiB &lt;BR /&gt;mmcblk3boot1: mmc3:0001 MAG2GA partition 2 2.00 MiB &lt;BR /&gt;mmcblk3rpmb: mmc3:0001 MAG2GA partition 3 128 KiB &lt;BR /&gt; mmcblk3: p1 p2 &lt;BR /&gt;caam_jr 2101000.jr0: Instantiated RNG4 SH0. &lt;BR /&gt;caam_jr 2101000.jr0: Instantiated RNG4 SH1. &lt;BR /&gt;caam algorithms registered in /proc/crypto &lt;BR /&gt;caam_jr 2101000.jr0: registering rng-caam &lt;BR /&gt;platform caam_sm: blkkey_ex: 4 keystore units available &lt;BR /&gt;platform caam_sm: 64-bit clear key: &lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07 &lt;BR /&gt;platform caam_sm: 64-bit black key: &lt;BR /&gt;platform caam_sm: [0000] e0 f5 da 3b e9 d7 79 86 &lt;BR /&gt;platform caam_sm: [0008] f7 6e 39 23 c6 56 0a 56 &lt;BR /&gt;platform caam_sm: 128-bit clear key: &lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07 &lt;BR /&gt;platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f &lt;BR /&gt;platform caam_sm: 128-bit black key: &lt;BR /&gt;platform caam_sm: [0000] fd 06 99 38 58 0c 4a ac &lt;BR /&gt;platform caam_sm: [0008] 43 8b 2e 6b 42 67 8e 36 &lt;BR /&gt;platform caam_sm: 192-bit clear key: &lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07 &lt;BR /&gt;platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f &lt;BR /&gt;platform caam_sm: [0016] 10 11 12 13 14 15 16 17 &lt;BR /&gt;platform caam_sm: 192-bit black key: &lt;BR /&gt;platform caam_sm: [0000] dc 0a 30 5c 96 f2 42 a4 &lt;BR /&gt;platform caam_sm: [0008] 9c c0 e8 6e b0 97 60 9c &lt;BR /&gt;platform caam_sm: [0016] 21 0f 0d e9 21 d7 bc 19 &lt;BR /&gt;platform caam_sm: [0024] f0 a3 2f 67 4c 0e 4c 00 &lt;BR /&gt;platform caam_sm: 256-bit clear key: &lt;BR /&gt;platform caam_sm: [0000] 00 01 02 03 04 0f 06 07 &lt;BR /&gt;platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f &lt;BR /&gt;platform caam_sm: [0016] 10 11 12 13 14 15 16 17 &lt;BR /&gt;platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f &lt;BR /&gt;platform caam_sm: 256-bit black key: &lt;BR /&gt;platform caam_sm: [0000] 06 a9 15 3c aa 33 4e af &lt;BR /&gt;platform caam_sm: [0008] 41 7a 45 a8 00 19 f1 5b &lt;BR /&gt;platform caam_sm: [0016] 6e 61 a6 76 21 24 5d f1 &lt;BR /&gt;platform caam_sm: [0024] c8 30 3d f9 cc 67 3c 18 &lt;BR /&gt;platform caam_sm: 64-bit unwritten blob: &lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 128-bit unwritten blob: &lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 196-bit unwritten blob: &lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 256-bit unwritten blob: &lt;BR /&gt;platform caam_sm: [0000] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0008] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0016] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0024] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0032] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0040] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0048] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 64-bit black key in blob: &lt;BR /&gt;platform caam_sm: [0000] 40 28 3e b3 43 80 5b a8 &lt;BR /&gt;platform caam_sm: [0008] be c6 e7 a9 3d c2 e3 b2 &lt;BR /&gt;platform caam_sm: [0016] d8 18 83 cb 4d 02 bc 4f &lt;BR /&gt;platform caam_sm: [0024] e2 47 8c 70 5e 6f cf 40 &lt;BR /&gt;platform caam_sm: [0032] 19 90 76 69 2a 87 2d d2 &lt;BR /&gt;platform caam_sm: [0040] 5a 24 51 ef 37 ec 84 0d &lt;BR /&gt;platform caam_sm: [0048] c3 6c 36 f4 c3 c9 f5 5e &lt;BR /&gt;platform caam_sm: [0056] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 128-bit black key in blob: &lt;BR /&gt;platform caam_sm: [0000] f6 05 1b 5a be d7 a8 a7 &lt;BR /&gt;platform caam_sm: [0008] f0 a0 e4 c9 b7 b9 cc 5d &lt;BR /&gt;platform caam_sm: [0016] a2 41 bb c3 ac 11 7a ed &lt;BR /&gt;platform caam_sm: [0024] bc c3 f2 26 49 16 db 14 &lt;BR /&gt;platform caam_sm: [0032] 72 43 cd 51 34 5e 46 e8 &lt;BR /&gt;platform caam_sm: [0040] 11 30 71 de 92 19 26 08 &lt;BR /&gt;platform caam_sm: [0048] 69 e8 26 06 cc 7c 76 57 &lt;BR /&gt;platform caam_sm: [0056] 56 2f c2 bd 74 a0 7b d5 &lt;BR /&gt;platform caam_sm: [0064] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 192-bit black key in blob: &lt;BR /&gt;platform caam_sm: [0000] 41 6f 26 a8 0b 37 10 5e &lt;BR /&gt;platform caam_sm: [0008] 66 ad 4e 68 70 be 3c f1 &lt;BR /&gt;platform caam_sm: [0016] 18 10 d3 49 9f 12 ec 82 &lt;BR /&gt;platform caam_sm: [0024] 31 c5 fa 54 cd 99 dd 55 &lt;BR /&gt;platform caam_sm: [0032] 85 57 25 4a 49 44 db d2 &lt;BR /&gt;platform caam_sm: [0040] a7 6f a8 51 80 12 62 10 &lt;BR /&gt;platform caam_sm: [0048] bc fb 82 2c a2 0d 89 4c &lt;BR /&gt;platform caam_sm: [0056] 9f 5f 5c 56 ec 59 86 b4 &lt;BR /&gt;platform caam_sm: [0064] 26 f6 82 02 aa 8d 8d 84 &lt;BR /&gt;platform caam_sm: [0072] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: 256-bit black key in blob: &lt;BR /&gt;platform caam_sm: [0000] ce f9 9e 95 c3 2a 27 02 &lt;BR /&gt;platform caam_sm: [0008] 06 49 f1 9c 31 8a 01 09 &lt;BR /&gt;platform caam_sm: [0016] 12 97 11 2e b5 05 11 96 &lt;BR /&gt;platform caam_sm: [0024] 9c 86 18 cf 16 b5 72 db &lt;BR /&gt;platform caam_sm: [0032] 99 66 64 2f 13 8d 27 bd &lt;BR /&gt;platform caam_sm: [0040] 7b 25 a5 b0 9a ca 9f b0 &lt;BR /&gt;platform caam_sm: [0048] c5 06 1a 7b 85 38 57 09 &lt;BR /&gt;platform caam_sm: [0056] 3c 24 be 5f 6d ea 35 53 &lt;BR /&gt;platform caam_sm: [0064] 60 d1 53 8e e6 ad 97 54 &lt;BR /&gt;platform caam_sm: [0072] 9e d0 da 33 a9 62 80 da &lt;BR /&gt;platform caam_sm: [0080] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: [0088] 00 00 00 00 00 00 00 00 &lt;BR /&gt;platform caam_sm: restored 64-bit black key: &lt;BR /&gt;platform caam_sm: [0000] 64 d9 e3 88 8e 34 d6 1a &lt;BR /&gt;platform caam_sm: [0008] 57 55 56 af 6c ff e1 a8 &lt;BR /&gt;platform caam_sm: restored 128-bit black key: &lt;BR /&gt;platform caam_sm: [0000] fd 06 99 38 58 0c 4a ac &lt;BR /&gt;platform caam_sm: [0008] 43 8b 2e 6b 42 67 8e 36 &lt;BR /&gt;platform caam_sm: restored 192-bit black key: &lt;BR /&gt;platform caam_sm: [0000] dc 0a 30 5c 96 f2 42 a4 &lt;BR /&gt;platform caam_sm: [0008] 9c c0 e8 6e b0 97 60 9c &lt;BR /&gt;platform caam_sm: [0016] 34 8f 98 23 80 3c 1a 16 &lt;BR /&gt;platform caam_sm: [0024] b9 c2 62 45 da 2f ae 4b &lt;BR /&gt;platform caam_sm: restored 256-bit black key: &lt;BR /&gt;platform caam_sm: [0000] 06 a9 15 3c aa 33 4e af &lt;BR /&gt;platform caam_sm: [0008] 41 7a 45 a8 00 19 f1 5b &lt;BR /&gt;platform caam_sm: [0016] 6e 61 a6 76 21 24 5d f1 &lt;BR /&gt;platform caam_sm: [0024] c8 30 3d f9 cc 67 3c 18 &lt;BR /&gt;caam-snvs 20cc000.caam-snvs: can't get snvs clock &lt;BR /&gt;caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state &lt;BR /&gt;usbcore: registered new interface driver usbhid &lt;BR /&gt;usbhid: USB HID core driver &lt;BR /&gt;NET: Registered protocol family 26 &lt;BR /&gt;NET: Registered protocol family 10 &lt;BR /&gt;sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver &lt;BR /&gt;NET: Registered protocol family 17 &lt;BR /&gt;can: controller area network core (rev 20120528 abi 9) &lt;BR /&gt;NET: Registered protocol family 29 &lt;BR /&gt;can: raw protocol (rev 20120528) &lt;BR /&gt;can: broadcast manager protocol (rev 20161123 t) &lt;BR /&gt;can: netlink gateway (rev 20130117) max_hops=1 &lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized &lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized &lt;BR /&gt;Bluetooth: RFCOMM ver 1.11 &lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3 &lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast &lt;BR /&gt;Bluetooth: BNEP socket layer initialized &lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2 &lt;BR /&gt;Bluetooth: HIDP socket layer initialized &lt;BR /&gt;8021q: 802.1Q VLAN Support v1.8 &lt;BR /&gt;lib80211: common routines for IEEE802.11 drivers &lt;BR /&gt;Key type dns_resolver registered &lt;BR /&gt;cpu cpu0: Registered imx6q-cpufreq &lt;BR /&gt;imx_thermal 2000000.aips-bus:tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C &lt;BR /&gt;input: gpio-keys as /devices/soc0/gpio-keys/input/input0 &lt;BR /&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1) &lt;BR /&gt;usb_otg_vbus: disabling &lt;BR /&gt;SW4: disabling &lt;BR /&gt;VGEN1: disabling &lt;BR /&gt;ALSA device list: &lt;BR /&gt; No soundcards found. &lt;BR /&gt;EXT4-fs (mmcblk3p2): couldn't mount as ext3 due to feature incompatibilities &lt;BR /&gt;random: fast init done &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1efd8000 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Argument: 0x000061a0 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000031 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x0000001f &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00000900 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;� *��ҽ�Ɂ-110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;mmc3: tried to reset card, got error -110 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24992 &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1efd8400 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000004 &lt;BR /&gt;mmc3: sdhci: Argument: 0x000061a2 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24994 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24996 &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1efd8c00 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000038 &lt;BR /&gt;mmc3: sdhci: Argument: 0x000061a6 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24998 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25000 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25002 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25004 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25006 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25008 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25010 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25012 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25014 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 25016 &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1f1f7800 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Argument: 0x0000619c | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: 18 callbacks suppressed &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24988 &lt;BR /&gt;EXT4-fs error (device mmcblk3p2): __ext4_get_inode_loc:4363: inode #8: block 206: comm swapper/0: unable to read itab&lt;BR /&gt;le block &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1c5ad600 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Argument: 0x00006002 | Trn mode: 0x0000002b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000193a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;mmc3: tried to reset card, got error -110 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24578 &lt;BR /&gt;Buffer I/O error on dev mmcblk3p2, logical block 1, lost sync page write &lt;BR /&gt;EXT4-fs (mmcblk3p2): no journal found &lt;BR /&gt;VFS: Dirty inode writeback failed for block device mmcblk3p2 (err=-5). &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1f1f7400 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Argument: 0x00006002 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24578 &lt;BR /&gt;EXT2-fs (mmcblk3p2): error: unable to read superblock &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24576 &lt;BR /&gt;FAT-fs (mmcblk3p2): unable to read boot sector &lt;BR /&gt;VFS: Cannot open root device "mmcblk3p2" or unknown-block(179,2): error -5 &lt;BR /&gt;Please append a correct "root=" boot option; here are the available partitions: &lt;BR /&gt;0100 65536 ram0 (driver?) &lt;BR /&gt;0101 65536 ram1 (driver?) &lt;BR /&gt;0102 65536 ram2 (driver?) &lt;BR /&gt;0103 65536 ram3 (driver?) &lt;BR /&gt;0104 65536 ram4 (driver?) &lt;BR /&gt;0105 65536 ram5 (driver?) &lt;BR /&gt;0106 65536 ram6 (driver?) &lt;BR /&gt;0107 65536 ram7 (driver?) &lt;BR /&gt;0108 65536 ram8 (driver?) &lt;BR /&gt;0109 65536 ram9 (driver?) &lt;BR /&gt;010a 65536 ram10 (driver?) &lt;BR /&gt;010b 65536 ram11 (driver?) &lt;BR /&gt;010c 65536 ram12 (driver?) &lt;BR /&gt;010d 65536 ram13 (driver?) &lt;BR /&gt;010e 65536 ram14 (driver?) &lt;BR /&gt;010f 65536 ram15 (driver?) &lt;BR /&gt;b300 15267840 mmcblk3 driver: mmcblk &lt;BR /&gt; b301 8192 mmcblk3p1 253db6b6-01 &lt;BR /&gt; b302 49152 mmcblk3p2 253db6b6-02 &lt;BR /&gt;b318 128 mmcblk3rpmb (driver?) &lt;BR /&gt;b310 2048 mmcblk3boot1 (driver?) &lt;BR /&gt;b308 2048 mmcblk3boot0 (driver?) &lt;BR /&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2) &lt;BR /&gt;CPU1: stopping &lt;BR /&gt;CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #15 &lt;BR /&gt;Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree) &lt;BR /&gt;[&amp;lt;8010ecb4&amp;gt;] (unwind_backtrace) from [&amp;lt;8010b394&amp;gt;] (show_stack+0x10/0x14) &lt;BR /&gt;[&amp;lt;8010b394&amp;gt;] (show_stack) from [&amp;lt;803c144c&amp;gt;] (dump_stack+0x78/0x8c) &lt;BR /&gt;[&amp;lt;803c144c&amp;gt;] (dump_stack) from [&amp;lt;8010db04&amp;gt;] (handle_IPI+0x198/0x1ac) &lt;BR /&gt;[&amp;lt;8010db04&amp;gt;] (handle_IPI) from [&amp;lt;80101510&amp;gt;] (gic_handle_irq+0x88/0x8c) &lt;BR /&gt;[&amp;lt;80101510&amp;gt;] (gic_handle_irq) from [&amp;lt;8010bd8c&amp;gt;] (__irq_svc+0x6c/0xa8) &lt;BR /&gt;Exception stack(0x8c089f60 to 0x8c089fa8) &lt;BR /&gt;9f60: 00000000 7fffffff 00000001 8c088000 692272d1 00000010 8efcef40 00000001 &lt;BR /&gt;9f80: 6406bc13 00000010 00000000 80f03144 00000000 8c089fb0 80953e7c 806a4870 &lt;BR /&gt;9fa0: 20000013 ffffffff &lt;BR /&gt;[&amp;lt;8010bd8c&amp;gt;] (__irq_svc) from [&amp;lt;806a4870&amp;gt;] (cpuidle_enter_state+0x13c/0x2cc) &lt;BR /&gt;[&amp;lt;806a4870&amp;gt;] (cpuidle_enter_state) from [&amp;lt;80167f68&amp;gt;] (cpu_startup_entry+0x168/0x228) &lt;BR /&gt;[&amp;lt;80167f68&amp;gt;] (cpu_startup_entry) from [&amp;lt;101015ac&amp;gt;] (0x101015ac) &lt;BR /&gt;---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 11:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788866#M122241</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-04T11:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788867#M122242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maxim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;issue may be caused by mmc numbering, as in linux there is mmcblk3,&lt;/P&gt;&lt;P&gt;while in uboot only "SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2", one can check&lt;/P&gt;&lt;P&gt;sect.Table 37. Linux uSDHC relationships attached Linux Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2018 23:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788867#M122242</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-04T23:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788868#M122243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor! Thank you for reply!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Issue is not solved yet.&lt;/P&gt;&lt;P&gt;In our boad only uSDHC 4 is present, so mmcroot configured as mmcblk3. In u-boot "mmc dev 2" = "mmcblk3" in linux, as I can see in u-boot sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uSDHC configuration from device tree:&amp;nbsp;&lt;/P&gt;&lt;P&gt;usdhc4: usdhc@0219c000 {&lt;BR /&gt;&amp;nbsp; &amp;nbsp;compatible = "fsl,imx6q-usdhc";&lt;BR /&gt;&amp;nbsp; &amp;nbsp;reg = &amp;lt;0x0219c000 0x4000&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;interrupts = &amp;lt;0 25 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;clocks = &amp;lt;&amp;amp;clks IMX6QDL_CLK_USDHC4&amp;gt;,&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;lt;&amp;amp;clks IMX6QDL_CLK_USDHC4&amp;gt;,&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&amp;lt;&amp;amp;clks IMX6QDL_CLK_USDHC4&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;clock-names = "ipg", "ahb", "per";&lt;BR /&gt;&amp;nbsp; &amp;nbsp;bus-width = &amp;lt;4&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;status = "disabled";&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&amp;amp;usdhc4 {&lt;BR /&gt;&amp;nbsp; &amp;nbsp;pinctrl-names = "default";&lt;BR /&gt;&amp;nbsp; &amp;nbsp;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_usdhc4&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;bus-width = &amp;lt;8&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;non-removable;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;no-1-8-v;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;keep-power-in-suspend;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;pinctrl_usdhc4: usdhc4grp {&lt;BR /&gt;&amp;nbsp; &amp;nbsp;fsl,pins = &amp;lt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;MX6QDL_PAD_SD4_CMD__SD4_CMD 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_CLK__SD4_CLK 0x10059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT0__SD4_DATA0 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT1__SD4_DATA1 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT2__SD4_DATA2 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT3__SD4_DATA3 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT4__SD4_DATA4 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT5__SD4_DATA5 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT6__SD4_DATA6 0x17059&lt;BR /&gt; &lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;MX6QDL_PAD_SD4_DAT7__SD4_DATA7 0x17059&lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;Other uSDHC are disabled.&lt;/P&gt;&lt;P&gt;Previous kernel (4.9.11) boots fine&amp;nbsp;with the same u-boot and device-tree. May be in new kernel there are any changes in mmc configuration? Something like hardcoded offsets or dma configurations or something else... How blinks on display may&amp;nbsp;be explained? May be I should try to compile kernel from special commit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 06:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788868#M122243</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-05T06:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788869#M122244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maxim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you mean that uSDHC 4 is visible as "mmc dev 2"in uboot.&lt;/P&gt;&lt;P&gt;NXP linux sources are located on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 07:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788869#M122244</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-05T07:31:55Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788870#M122245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;mmc info:&lt;/P&gt;&lt;P&gt;Device: FSL_SDHC &lt;BR /&gt;Manufacturer ID: 15 &lt;BR /&gt;OEM: 100 &lt;BR /&gt;Name: MAG2G &lt;BR /&gt;Tran Speed: 52000000 &lt;BR /&gt;Rd Block Len: 512 &lt;BR /&gt;MMC version 4.4.1 &lt;BR /&gt;High Capacity: Yes &lt;BR /&gt;Capacity: 14.6 GiB &lt;BR /&gt;Bus Width: 8-bit &lt;BR /&gt;Erase Group Size: 512 KiB &lt;BR /&gt;HC WP Group Size: 32 MiB &lt;BR /&gt;User Capacity: 14.6 GiB WRREL &lt;BR /&gt;Boot Capacity: 2 MiB ENH &lt;BR /&gt;RPMB Capacity: 128 KiB ENH&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By commands "ls mmc 2:1" and "ls mmc 2:2" I can see files on kernel and rootfs partitions.&lt;/P&gt;&lt;P&gt;In the end of boot log I can see that kernel see mmcblk3 device and both partitions but can't mount it:&lt;/P&gt;&lt;P&gt;mmc3: tried to reset card, got error -110&lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24580&lt;BR /&gt;EXT4-fs (mmcblk3p2): can't read group descriptor 0&lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt.&lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP ===========&lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1f1f7400 | Version: 0x00000002&lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000002&lt;BR /&gt;mmc3: sdhci: Argument: 0x00006002 | Trn mode: 0x0000003b&lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011&lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080&lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff&lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000&lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b&lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003&lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007&lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff&lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff&lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900&lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000&lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80047204&lt;BR /&gt;mmc3: sdhci: ============================================&lt;BR /&gt;lmcblk3: error -110 sending status command, retrying&lt;BR /&gt;mmcblk3: error -110 sending status command, retrying&lt;BR /&gt;mmcblk3: error -110 sending status command, aborting&lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24578&lt;BR /&gt;EXT2-fs (mmcblk3p2): error: unable to read superblock&lt;BR /&gt;mmcblk3: error -110 sending status command, retrying&lt;BR /&gt;mmcblk3: error -110 sending status command, retrying&lt;BR /&gt;mmcblk3: error -110 sending status command, aborting&lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 24576&lt;BR /&gt;FAT-fs (mmcblk3p2): unable to read boot sector&lt;BR /&gt;VFS: Cannot open root device "mmcblk3p2" or unknown-block(179,2): error -5&lt;BR /&gt;Please append a correct "root=" boot option; here are the available partitions:&lt;BR /&gt;0100 65536 ram0 (driver?)&lt;BR /&gt;0101 65536 ram1 (driver?)&lt;BR /&gt;0102 65536 ram2 (driver?)&lt;BR /&gt;0103 65536 ram3 (driver?)&lt;BR /&gt;0104 65536 ram4 (driver?)&lt;BR /&gt;0105 65536 ram5 (driver?)&lt;BR /&gt;0106 65536 ram6 (driver?)&lt;BR /&gt;0107 65536 ram7 (driver?)&lt;BR /&gt;0108 65536 ram8 (driver?)&lt;BR /&gt;0109 65536 ram9 (driver?)&lt;BR /&gt;010a 65536 ram10 (driver?)&lt;BR /&gt;010b 65536 ram11 (driver?)&lt;BR /&gt;010c 65536 ram12 (driver?)&lt;BR /&gt;010d 65536 ram13 (driver?)&lt;BR /&gt;010e 65536 ram14 (driver?)&lt;BR /&gt;010f 65536 ram15 (driver?)&lt;BR /&gt;b300 15267840 mmcblk3 driver: mmcblk&lt;BR /&gt; b301 8192 mmcblk3p1 253db6b6-01&lt;BR /&gt; b302 49152 mmcblk3p2 253db6b6-02&lt;BR /&gt;b318 128 mmcblk3rpmb (driver?)&lt;BR /&gt;b310 2048 mmcblk3boot1 (driver?)&lt;BR /&gt;b308 2048 mmcblk3boot0 (driver?)&lt;BR /&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)&lt;BR /&gt;CPU1: stopping&lt;BR /&gt;CPU: 1 PID: 0 Comm: swapper/1 Not tainted 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #21&lt;BR /&gt;Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree) &lt;BR /&gt;[&amp;lt;8010ecb4&amp;gt;] (unwind_backtrace) from [&amp;lt;8010b394&amp;gt;] (show_stack+0x10/0x14) &lt;BR /&gt;[&amp;lt;8010b394&amp;gt;] (show_stack) from [&amp;lt;803c144c&amp;gt;] (dump_stack+0x78/0x8c) &lt;BR /&gt;[&amp;lt;803c144c&amp;gt;] (dump_stack) from [&amp;lt;8010db04&amp;gt;] (handle_IPI+0x198/0x1ac) &lt;BR /&gt;[&amp;lt;8010db04&amp;gt;] (handle_IPI) from [&amp;lt;80101510&amp;gt;] (gic_handle_irq+0x88/0x8c) &lt;BR /&gt;[&amp;lt;80101510&amp;gt;] (gic_handle_irq) from [&amp;lt;8010bd8c&amp;gt;] (__irq_svc+0x6c/0xa8) &lt;BR /&gt;Exception stack(0x8c089f60 to 0x8c089fa8) &lt;BR /&gt;9f60: 00000000 8efd26c0 00000001 8c088000 beb36c99 00000003 8efcef40 00000001 &lt;BR /&gt;9f80: bcdac499 00000003 00000000 80f03144 00000001 8c089fb0 809b7eec 80707a40 &lt;BR /&gt;9fa0: 20000013 ffffffff &lt;BR /&gt;[&amp;lt;8010bd8c&amp;gt;] (__irq_svc) from [&amp;lt;80707a40&amp;gt;] (cpuidle_enter_state+0x13c/0x2cc) &lt;BR /&gt;[&amp;lt;80707a40&amp;gt;] (cpuidle_enter_state) from [&amp;lt;80167f68&amp;gt;] (cpu_startup_entry+0x168/0x228) &lt;BR /&gt;[&amp;lt;80167f68&amp;gt;] (cpu_startup_entry) from [&amp;lt;101015ac&amp;gt;] (0x101015ac) &lt;BR /&gt;---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 07:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788870#M122245</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-05T07:38:28Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788871#M122246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;may be useful to look on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.yoctoproject.org/pipermail/meta-freescale/2017-March/020307.html" title="https://lists.yoctoproject.org/pipermail/meta-freescale/2017-March/020307.html"&gt;[meta-freescale] [3rdparty PATCH 0/4] Allow easier use of mainline-based BSP on i.MX products (Nitrogen6x support)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 09:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788871#M122246</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-05T09:03:37Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788872#M122247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the link but problrm is not to properly give root device to kernel. Problem is to mount given root device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tryed to set root device by UUID - kernel can find mmcblk3p2 by this uuid but cant mount it.&lt;/P&gt;&lt;P&gt;Getting device idx by&amp;nbsp;mmc_get_reserved_index() not helped too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 10:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788872#M122247</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-05T10:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788873#M122248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you try to reproduce issue on nxp imx6q sabre sd reference board with nxp demo images from&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 11:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788873#M122248</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-05T11:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788874#M122249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On sabresd it can boot both from SD and from emmc, but on sabresd another emmc chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diference in mounting: on sabresd to rootfs partition assign block device 179:10, on custom board - 179:2. Kernel 4.9.11 create block device 179:34.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 11:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788874#M122249</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-05T11:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788875#M122250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how image was programmed to emmc, recommended to use mfg tool for this L4.9.88_2.0.0 -&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=IMX6_L4.9.88_2.0.0_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=IMX6_L4.9.88_2.0.0_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=IMX6_L4.9.88_2.0.0_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 12:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788875#M122250</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-05T12:37:29Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788876#M122251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;from u-boot "ums mmc 2" - export mmc device via OTG&lt;BR /&gt;from host dd image.sdcard to this device&lt;BR /&gt;On sabresd I flashed image to emmc by the same way - boot is ok.&lt;BR /&gt;Will try mfgtool tomorrow.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 12:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788876#M122251</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-05T12:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788877#M122252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;With MFGtool I have another problem: it cant find device. Neither sabresd, nor custom board.&lt;/P&gt;&lt;P&gt;On linux it prints:&lt;/P&gt;&lt;P&gt;./linux-runvbs.sh mfgtool2-yocto-mx-sabresd-emmc.vbs&lt;BR /&gt;mfgtool2-yocto-mx-sabresd-emmc.vbs&lt;BR /&gt;Executing: ./mfgtoolcli -l eMMC -s board=sabresd -s sxdtb=sdb -s mmc=3&lt;BR /&gt;Your Options:&lt;BR /&gt;board: sabresd&lt;BR /&gt;sxdtb: sdb&lt;BR /&gt;mmc: 3&lt;BR /&gt;Ready to flash.&lt;BR /&gt;init op Failed code# 24 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Windows (under Virtual Box) it cant find device, but "HID compatable device" with proper VID/PID appears in device manager. Should I somehow install mfgtool or is it permissions issue? I cant find anything about it in documentation.&amp;nbsp;Start MFGTool after connecting device, as mentioned in user guide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 11:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788877#M122252</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-06T11:35:43Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788878#M122253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On Windows if connect device&amp;nbsp;when MFGTool started it crashes.&lt;/P&gt;&lt;P&gt;From log:&lt;/P&gt;&lt;P&gt;DLL version: 2.7.0&lt;BR /&gt;Thursday, September 06, 2018 17:40:01 Start new logging&lt;BR /&gt;ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[1]: new MxHidDeviceClass&lt;BR /&gt;ModuleID[2] LevelID[10]: Device Manager thread is running&lt;BR /&gt;ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop&lt;/P&gt;&lt;P&gt;ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - DEVICE_ARRIVAL_EVT(\\?\USB#VID_15A2&amp;amp;PID_0054#5&amp;amp;c1e6cce&amp;amp;0&amp;amp;1#{a5dcbf10-6530-11d2-901f-00c04fb951ed})&lt;BR /&gt;ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - end&lt;BR /&gt;ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - DEVICE_ARRIVAL_EVT(\\?\USB#VID_15A2&amp;amp;PID_0054#5&amp;amp;c1e6cce&amp;amp;0&amp;amp;1#{a5dcbf10-6530-11d2-901f-00c04fb951ed})&lt;BR /&gt;ModuleID[2] LevelID[10]: DeviceClass::FindDeviceByUsbPath--DeviceListType_Current, _devices.size: 0&lt;BR /&gt;ModuleID[2] LevelID[1]: DeviceClass::FindDeviceByUsbPath() - DeviceListType_New--index: 0&lt;BR /&gt;ModuleID[2] LevelID[1]: DeviceClass::FindDeviceByUsbPath() - DeviceListType_New--devPath: \\?\hid#vid_15a2&amp;amp;pid_0054#6&amp;amp;22d0f36a&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;ModuleID[2] LevelID[10]: new MxHidDevice[008BB0C0]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 11:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788878#M122253</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-06T11:43:04Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788879#M122254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On phisical machine MFGTool works. Will try to flash custom board...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 12:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788879#M122254</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-06T12:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788880#M122255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;With MFGTool it failes with the same error on partitioning stage&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;End of log from debug console:&lt;/P&gt;&lt;P&gt;Mass Storage Function, version: 2009/09/11 &lt;BR /&gt;LUN: removable file: (no medium) &lt;BR /&gt;Start UTP at ci_hdrc.0 &lt;BR /&gt;uuc /dev/utp &lt;BR /&gt;uuc 0.5 [built May 1 2018 14:29:24] &lt;BR /&gt;UTP: Waiting for /dev/utp to appear &lt;BR /&gt;UTP: file/device node /dev/utp already exists &lt;BR /&gt;cpu_id is 0 &lt;BR /&gt;configfs-gadget gadget: high-speed config #1: c &lt;BR /&gt;random: fast init done &lt;BR /&gt;UTP: received command '$ sleep 1 ' &lt;BR /&gt;UTP: executing "sleep 1 " &lt;BR /&gt;UTP: sending Success to kernel for command $ sleep 1 . &lt;BR /&gt;utp_poll: pass returned. &lt;BR /&gt;UTP: received command 'send' &lt;BR /&gt;UTP: sending Success to kernel for command send. &lt;BR /&gt;UTP: received command '$ tar xf $FILE ' &lt;BR /&gt;UTP: executing "tar xf $FILE " &lt;BR /&gt;UTP: sending Success to kernel for command $ tar xf $FILE . &lt;BR /&gt;utp_poll: pass returned. &lt;BR /&gt;UTP: received command '$ sh mksdcard.sh /dev/mmcblk3' &lt;BR /&gt;UTP: executing "sh mksdcard.sh /dev/mmcblk3" &lt;BR /&gt;mmcblk3: error -110 requesting status &lt;BR /&gt;1+0 records in &lt;BR /&gt;1+0 records out &lt;BR /&gt;1024 bytes (1.0 kB, 1.0 KiB) copied, 0.0132633 s, 77.2 kB/s &lt;BR /&gt;mmc3: tried to reset card, got error -110 &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1c74a000 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000008 &lt;BR /&gt;mmc3: sdhci: Argument: 0x00000000 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80049204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;mmc3: tried to reset card, got error -110 &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 0 &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1c74a000 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000008 &lt;BR /&gt;mmc3: sdhci: Argument: 0x00000000 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host ctl: 0x00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80049204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 0 &lt;BR /&gt;Buffer I/O error on dev mmcblk3, logical block 0, async page read &lt;BR /&gt;mmc3: Timeout waiting for hardware interrupt. &lt;BR /&gt;mmc3: sdhci: ============ SDHCI REGISTER DUMP =========== &lt;BR /&gt;mmc3: sdhci: Sys addr: 0x1c74a000 | Version: 0x00000002 &lt;BR /&gt;mmc3: sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000008 &lt;BR /&gt;mmc3: sdhci: Argument: 0x00000000 | Trn mode: 0x0000003b &lt;BR /&gt;mmc3: sdhci: Present: 0x01fd8009 | Host 00000011 &lt;BR /&gt;mmc3: sdhci: Power: 0x00000002 | Blk gap: 0x00000080 &lt;BR /&gt;mmc3: sdhci: Wake-up: 0x00000008 | Clock: 0x000010ff &lt;BR /&gt;mmc3: sdhci: Timeout: 0x0000008f | Int stat: 0x00000000 &lt;BR /&gt;mmc3: sdhci: Int enab: 0x107f100b | Sig enab: 0x107f100b &lt;BR /&gt;mmc3: sdhci: AC12 err: 0x00000082 | Slot int: 0x00000003 &lt;BR /&gt;mmc3: sdhci: Caps: 0x07eb0000 | Caps_1: 0x0000a007 &lt;BR /&gt;mmc3: sdhci: Cmd: 0x0000123a | Max curr: 0x00ffffff &lt;BR /&gt;mmc3: sdhci: Resp[0]: 0x00ff8080 | Resp[1]: 0xfff6dbff &lt;BR /&gt;mmc3: sdhci: Resp[2]: 0x320f5903 | Resp[3]: 0x00000900 &lt;BR /&gt;mmc3: sdhci: Host ctl2: 0x00000000 &lt;BR /&gt;mmc3: sdhci: ADMA Err: 0x00000003 | ADMA Ptr: 0x80049204 &lt;BR /&gt;mmc3: sdhci: ============================================ &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, retrying &lt;BR /&gt;mmcblk3: error -110 sending status command, aborting &lt;BR /&gt;blk_update_request: I/O error, dev mmcblk3, sector 0 &lt;BR /&gt;Buffer I/O error on dev mmcblk3, logical block 0, async page read &lt;BR /&gt;sfdisk: cannot open /dev/mmcblk3: Input/output error &lt;BR /&gt;UTP: sending Non-success to kernel for command $ sh mksdcard.sh /dev/mmcblk3. &lt;BR /&gt;utp_poll: exit with status 256&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2018 07:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788880#M122255</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-07T07:24:59Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788881#M122256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tried to boot up another board. It fails the same way. Issue is definitely in kernel with this emmc chip.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2018 07:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788881#M122256</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-07T07:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788882#M122257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can try to replace this emmc with one on sabre sd board to narrow down issue.&lt;/P&gt;&lt;P&gt;If you think issue is definitely in kernel, please provide steps how it can be&lt;/P&gt;&lt;P&gt;reproduced on sabre sd board. Also may be useful to check&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/332110"&gt;eMMC 8GB to 4GB - crash on linux (yocto) boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2018 11:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788882#M122257</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-09-07T11:16:43Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788883#M122258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think that issue in kernel because older versions (nxp 4.9.11, fslc 4.1) works fine with the same hardware, bootloader, rootfs and device tree.&lt;/P&gt;&lt;P&gt;What am I doing is:&lt;/P&gt;&lt;P&gt;- get build environment from NXP repo, as discribed in Yocto project manual (branch imx_4.9.88+2.0.0_ga)&lt;/P&gt;&lt;P&gt;- build core-image-minimal&amp;nbsp;&lt;/P&gt;&lt;P&gt;- connect board to host PC via OTG&lt;/P&gt;&lt;P&gt;- boot up board, enter&amp;nbsp;u-boot shell, run command 'ums mmc 2'&lt;/P&gt;&lt;P&gt;- on host PC flash image.sdcard to emmc by 'dd' command or manualy partition disk and copy files&lt;/P&gt;&lt;P&gt;- sync and umount disk, Ctrl+C on u-boot shell&lt;/P&gt;&lt;P&gt;- setenv mmcdev 2&lt;/P&gt;&lt;P&gt;- setenv mmcroot /dev/mmcblk3p2 rootwait rw&lt;/P&gt;&lt;P&gt;- boot&lt;/P&gt;&lt;P&gt;On sabresd it works, on custom board it failes to mount rootfs.&lt;/P&gt;&lt;P&gt;Our emmc chip is Samsung KLMAG2GE4A-A001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mmc info&lt;BR /&gt;Device: FSL_SDHC&lt;BR /&gt;Manufacturer ID: 15&lt;BR /&gt;OEM: 100&lt;BR /&gt;Name: MAG2G &lt;BR /&gt;Tran Speed: 52000000&lt;BR /&gt;Rd Block Len: 512&lt;BR /&gt;MMC version 4.4.1&lt;BR /&gt;High Capacity: Yes&lt;BR /&gt;Capacity: 14.6 GiB&lt;BR /&gt;Bus Width: 8-bit&lt;BR /&gt;Erase Group Size: 512 KiB&lt;BR /&gt;HC WP Group Size: 32 MiB&lt;BR /&gt;User Capacity: 14.6 GiB WRREL&lt;BR /&gt;Boot Capacity: 2 MiB ENH&lt;BR /&gt;RPMB Capacity: 128 KiB ENH&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2018 12:45:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788883#M122258</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-07T12:45:30Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788884#M122259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thans for the link, will check it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, our customer tell me that they built new kernel and boot it successful. There are SD slots on their version of board. So I think, the issue may be in device-tree configurations.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2018 07:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788884#M122259</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-10T07:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to mount rootfs from emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788885#M122260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems I solved the problem. Regulator SW4 was disabling before mounting rootfs and everything hangs. I found in when tested another board and that board hanged exactly on disabling regulators. I add "regulator-always-on;" parameter to it in device tree and can boot up the board now. But why old kernel worked with disabled SW4 on the same hardware?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2018 12:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failed-to-mount-rootfs-from-emmc/m-p/788885#M122260</guid>
      <dc:creator>maximkuk</dc:creator>
      <dc:date>2018-09-10T12:59:07Z</dc:date>
    </item>
  </channel>
</rss>