<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx35 embedded TT limitations?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx35-embedded-TT-limitations/m-p/208546#M12215</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to debug a problem supporting usb dacs with the imx35 usb ports.&amp;nbsp; The issue appears to be related to the embedded transaction translator as when an external hub is attached without any kernel changes the devices work using the hubs TT.&lt;/P&gt;&lt;P&gt;I see description of restricted TT pipe line and the constant:&lt;/P&gt;&lt;P&gt;VUSB_HS_TT_PERIODIC_CONTEXTS&lt;/P&gt;&lt;P&gt;Although the reference manual suggests this can be set lower than 16, can someone confirm whether it is set lower for the imx35.&amp;nbsp; (its not referenced in the linux 2.6.31 kernel drivers I'm using)&lt;/P&gt;&lt;P&gt;Also does this constant restrict the number of separate transactions or individual start/complete splits which can occur within a frame.&lt;/P&gt;&lt;P&gt;My problem case is support of async usb audio dacs which requires one out iso sitd per frame with 4 start splits and one in iso sitd per frame with 1 start split + 3 complete splits.&amp;nbsp; With the embedded TT the in sitds never complete, but they do work with the external hub.&amp;nbsp; [there is also one async QH per 1ms frame]&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Feb 2012 22:36:45 GMT</pubDate>
    <dc:creator>Triode</dc:creator>
    <dc:date>2012-02-06T22:36:45Z</dc:date>
    <item>
      <title>imx35 embedded TT limitations?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx35-embedded-TT-limitations/m-p/208546#M12215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to debug a problem supporting usb dacs with the imx35 usb ports.&amp;nbsp; The issue appears to be related to the embedded transaction translator as when an external hub is attached without any kernel changes the devices work using the hubs TT.&lt;/P&gt;&lt;P&gt;I see description of restricted TT pipe line and the constant:&lt;/P&gt;&lt;P&gt;VUSB_HS_TT_PERIODIC_CONTEXTS&lt;/P&gt;&lt;P&gt;Although the reference manual suggests this can be set lower than 16, can someone confirm whether it is set lower for the imx35.&amp;nbsp; (its not referenced in the linux 2.6.31 kernel drivers I'm using)&lt;/P&gt;&lt;P&gt;Also does this constant restrict the number of separate transactions or individual start/complete splits which can occur within a frame.&lt;/P&gt;&lt;P&gt;My problem case is support of async usb audio dacs which requires one out iso sitd per frame with 4 start splits and one in iso sitd per frame with 1 start split + 3 complete splits.&amp;nbsp; With the embedded TT the in sitds never complete, but they do work with the external hub.&amp;nbsp; [there is also one async QH per 1ms frame]&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2012 22:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx35-embedded-TT-limitations/m-p/208546#M12215</guid>
      <dc:creator>Triode</dc:creator>
      <dc:date>2012-02-06T22:36:45Z</dc:date>
    </item>
  </channel>
</rss>