<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to test USB2/3 eye pattern on iMX8m? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-test-USB2-3-eye-pattern-on-iMX8m/m-p/788118#M122095</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to test USB2/3 eye patten on iMX8m on android os or linux os?&amp;nbsp; Thanks!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Oct 2018 08:19:50 GMT</pubDate>
    <dc:creator>kevincheng</dc:creator>
    <dc:date>2018-10-12T08:19:50Z</dc:date>
    <item>
      <title>How to test USB2/3 eye pattern on iMX8m?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-test-USB2-3-eye-pattern-on-iMX8m/m-p/788118#M122095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to test USB2/3 eye patten on iMX8m on android os or linux os?&amp;nbsp; Thanks!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 08:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-test-USB2-3-eye-pattern-on-iMX8m/m-p/788118#M122095</guid>
      <dc:creator>kevincheng</dc:creator>
      <dc:date>2018-10-12T08:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to test USB2/3 eye pattern on iMX8m?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-test-USB2-3-eye-pattern-on-iMX8m/m-p/788119#M122096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;The USB3 ports have a USB2 PHY and a USB3 PHY for backward compatibility. The USB2 PHY in this USB3 interface will use the same test procedures as for the USB2 port. &lt;BR /&gt;Below you could find reference material from the Community:&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/606950"&gt;https://community.nxp.com/message/606950&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-94460"&gt;https://community.nxp.com/docs/DOC-94460&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB3 (Superspeed) tests are totally different from USB2 and required different USB test equipment. &lt;BR /&gt;All USB test related information is available from the USB-IF web site at &lt;A href="http://www.usb.org/compliance"&gt;www.usb.org/compliance&lt;/A&gt;&lt;BR /&gt;At the bottom of the page there are links to pages with test specifications and procedures. Note also that i.MX USB testing is not specific. The test procedures are universal. Therefore, customers may be better served by contacting a USB test house for information. These test houses can perform the testing for the customer as USB3.x test equipment is quite specific and still very expensive.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2018 19:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-test-USB2-3-eye-pattern-on-iMX8m/m-p/788119#M122096</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-10-18T19:35:36Z</dc:date>
    </item>
  </channel>
</rss>