<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787781#M122048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that the pre-built Linux SDcard image for the #i.MX 8M evaluation kit downloaded from the NXP website fails with a kernel panic.&amp;nbsp; Is anyone else seeing the same thing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recently purchased the&amp;nbsp;MCIMX8M-EVK: Evaluation Kit for the i.MX 8M Applications Processor, downloaded the pre-built Linux BSP (&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=license&amp;amp;Parent_nodeId=1513109797983730444282&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=license&amp;amp;Parent_nodeId=1513109797983730444282&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=license&amp;amp;Parent_nodeId=1513109797983730444282&amp;amp;Par…&lt;/A&gt;&amp;nbsp;), and performed the following, according to the documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;extracted the&amp;nbsp;L4.9.88_2.0.0_images_MX8MQ.tar.gz tarball (md5sum:&amp;nbsp;e7fd9c911d12bf3807bba3b040eb0f2a)&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;tar zxvf L4.9.88_2.0.0_images_MX8MQ.tar.gz&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/LI&gt;&lt;LI&gt;decompressed the SD card image:&amp;nbsp;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;cd&amp;nbsp;L4.9.88_2.0.0_images_MX8MQ&lt;/P&gt;&lt;P&gt;bunzip2 fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/LI&gt;&lt;LI&gt;Copied the image to an SD card:&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;sudo dd if=fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard of=/dev/mmcblk0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I placed the SDcard in the evaluation board, set the jumpers for the proper boot, and applied power to the card.&amp;nbsp; I found two problems.&amp;nbsp; First, the monitor showed nothing on the screen (the monitor indicated that it received no signal).&amp;nbsp; "systemctl status" indicated no error with any processes. 2. The kernel panicked about 4 minutes into the boot process (output of serial port is attached):&lt;/P&gt;&lt;P&gt;[ 242.786648] INFO: task systemd-udevd:2801 blocked for more than 120 seconds.&lt;BR /&gt;[ 242.793723] Tainted: G O 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1&lt;BR /&gt;[ 242.801430] "echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message.&lt;BR /&gt;[ 242.809452] systemd-udevd D 0 2801 1771 0x0000020d&lt;BR /&gt;[ 242.815083] Call trace:&lt;BR /&gt;[ 242.817544] [&amp;lt;ffff000008085e98&amp;gt;] __switch_to+0x90/0xc0&lt;BR /&gt;[ 242.822810] [&amp;lt;ffff000008c653f0&amp;gt;] __schedule+0x178/0x590&lt;BR /&gt;[ 242.828159] [&amp;lt;ffff000008c65844&amp;gt;] schedule+0x3c/0xa8&lt;BR /&gt;[ 242.833157] [&amp;lt;ffff000008c688e4&amp;gt;] schedule_timeout+0x174/0x248&lt;BR /&gt;[ 242.839025] [&amp;lt;ffff000008c67680&amp;gt;] __down+0x58/0x90&lt;BR /&gt;[ 242.843852] [&amp;lt;ffff000008102e74&amp;gt;] down+0x4c/0x68&lt;BR /&gt;[ 242.849478] [&amp;lt;ffff000000f4155c&amp;gt;] HIFExchangeBMIMsg+0x20c/0x330 [wlan]&lt;BR /&gt;[ 242.856971] [&amp;lt;ffff000000f47ac4&amp;gt;] bmi_download_firmware+0x64/0x130 [wlan]&lt;BR /&gt;[ 242.864708] [&amp;lt;ffff000000edff9c&amp;gt;] vos_open+0x174/0x6c0 [wlan]&lt;BR /&gt;[ 242.871378] [&amp;lt;ffff000000d9bca4&amp;gt;] hdd_wlan_startup+0x5ac/0x12e0 [wlan]&lt;BR /&gt;[ 242.878462] [&amp;lt;ffff000000f45cc8&amp;gt;] hif_pci_probe+0x5f8/0x858 [wlan]&lt;BR /&gt;[ 242.884685] [&amp;lt;ffff000008486c4c&amp;gt;] pci_device_probe+0x9c/0x140&lt;BR /&gt;[ 242.890461] [&amp;lt;ffff000008649a40&amp;gt;] driver_probe_device+0x1d0/0x2c8&lt;BR /&gt;[ 242.896580] [&amp;lt;ffff000008649bf4&amp;gt;] __driver_attach+0xbc/0xc0&lt;BR /&gt;[ 242.902181] [&amp;lt;ffff000008647b34&amp;gt;] bus_for_each_dev+0x4c/0x98&lt;BR /&gt;[ 242.907867] [&amp;lt;ffff0000086493b8&amp;gt;] driver_attach+0x20/0x28&lt;BR /&gt;[ 242.913294] [&amp;lt;ffff000008648fa8&amp;gt;] bus_add_driver+0x1b8/0x228&lt;BR /&gt;[ 242.918976] [&amp;lt;ffff00000864a578&amp;gt;] driver_register+0x60/0xf8&lt;BR /&gt;[ 242.924576] [&amp;lt;ffff0000084857a8&amp;gt;] __pci_register_driver+0x38/0x40&lt;BR /&gt;[ 242.931321] [&amp;lt;ffff000000f45630&amp;gt;] hif_register_driver+0x18/0x38 [wlan]&lt;BR /&gt;[ 242.938482] [&amp;lt;ffff000000d93d80&amp;gt;] hdd_hif_register_driver+0x30/0x78 [wlan]&lt;BR /&gt;[ 242.946002] [&amp;lt;ffff0000012010b4&amp;gt;] hdd_module_init+0xb4/0x1000 [wlan]&lt;BR /&gt;[ 242.952416] [&amp;lt;ffff000008083a50&amp;gt;] do_one_initcall+0x38/0x130&lt;BR /&gt;[ 242.958110] [&amp;lt;ffff0000081767d8&amp;gt;] do_init_module+0x5c/0x1bc&lt;BR /&gt;[ 242.963714] [&amp;lt;ffff000008139650&amp;gt;] load_module+0x1c50/0x20f8&lt;BR /&gt;[ 242.969315] [&amp;lt;ffff000008139d78&amp;gt;] SyS_finit_module+0xa8/0xc0&lt;BR /&gt;[ 242.975003] [&amp;lt;ffff0000080838d8&amp;gt;] __sys_trace_return+0x0/0x4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone seen this problem?&amp;nbsp; Incidentally, a co-worker independently found the same problem.&amp;nbsp; It would be nice to know if I'm either mis-reading the instructions or the image has an error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Glen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Aug 2018 15:44:25 GMT</pubDate>
    <dc:creator>glen_m_cornell</dc:creator>
    <dc:date>2018-08-14T15:44:25Z</dc:date>
    <item>
      <title>Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787781#M122048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that the pre-built Linux SDcard image for the #i.MX 8M evaluation kit downloaded from the NXP website fails with a kernel panic.&amp;nbsp; Is anyone else seeing the same thing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We recently purchased the&amp;nbsp;MCIMX8M-EVK: Evaluation Kit for the i.MX 8M Applications Processor, downloaded the pre-built Linux BSP (&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=license&amp;amp;Parent_nodeId=1513109797983730444282&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=license&amp;amp;Parent_nodeId=1513109797983730444282&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=license&amp;amp;Parent_nodeId=1513109797983730444282&amp;amp;Par…&lt;/A&gt;&amp;nbsp;), and performed the following, according to the documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;extracted the&amp;nbsp;L4.9.88_2.0.0_images_MX8MQ.tar.gz tarball (md5sum:&amp;nbsp;e7fd9c911d12bf3807bba3b040eb0f2a)&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;tar zxvf L4.9.88_2.0.0_images_MX8MQ.tar.gz&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/LI&gt;&lt;LI&gt;decompressed the SD card image:&amp;nbsp;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;cd&amp;nbsp;L4.9.88_2.0.0_images_MX8MQ&lt;/P&gt;&lt;P&gt;bunzip2 fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/LI&gt;&lt;LI&gt;Copied the image to an SD card:&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;sudo dd if=fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard of=/dev/mmcblk0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I placed the SDcard in the evaluation board, set the jumpers for the proper boot, and applied power to the card.&amp;nbsp; I found two problems.&amp;nbsp; First, the monitor showed nothing on the screen (the monitor indicated that it received no signal).&amp;nbsp; "systemctl status" indicated no error with any processes. 2. The kernel panicked about 4 minutes into the boot process (output of serial port is attached):&lt;/P&gt;&lt;P&gt;[ 242.786648] INFO: task systemd-udevd:2801 blocked for more than 120 seconds.&lt;BR /&gt;[ 242.793723] Tainted: G O 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1&lt;BR /&gt;[ 242.801430] "echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message.&lt;BR /&gt;[ 242.809452] systemd-udevd D 0 2801 1771 0x0000020d&lt;BR /&gt;[ 242.815083] Call trace:&lt;BR /&gt;[ 242.817544] [&amp;lt;ffff000008085e98&amp;gt;] __switch_to+0x90/0xc0&lt;BR /&gt;[ 242.822810] [&amp;lt;ffff000008c653f0&amp;gt;] __schedule+0x178/0x590&lt;BR /&gt;[ 242.828159] [&amp;lt;ffff000008c65844&amp;gt;] schedule+0x3c/0xa8&lt;BR /&gt;[ 242.833157] [&amp;lt;ffff000008c688e4&amp;gt;] schedule_timeout+0x174/0x248&lt;BR /&gt;[ 242.839025] [&amp;lt;ffff000008c67680&amp;gt;] __down+0x58/0x90&lt;BR /&gt;[ 242.843852] [&amp;lt;ffff000008102e74&amp;gt;] down+0x4c/0x68&lt;BR /&gt;[ 242.849478] [&amp;lt;ffff000000f4155c&amp;gt;] HIFExchangeBMIMsg+0x20c/0x330 [wlan]&lt;BR /&gt;[ 242.856971] [&amp;lt;ffff000000f47ac4&amp;gt;] bmi_download_firmware+0x64/0x130 [wlan]&lt;BR /&gt;[ 242.864708] [&amp;lt;ffff000000edff9c&amp;gt;] vos_open+0x174/0x6c0 [wlan]&lt;BR /&gt;[ 242.871378] [&amp;lt;ffff000000d9bca4&amp;gt;] hdd_wlan_startup+0x5ac/0x12e0 [wlan]&lt;BR /&gt;[ 242.878462] [&amp;lt;ffff000000f45cc8&amp;gt;] hif_pci_probe+0x5f8/0x858 [wlan]&lt;BR /&gt;[ 242.884685] [&amp;lt;ffff000008486c4c&amp;gt;] pci_device_probe+0x9c/0x140&lt;BR /&gt;[ 242.890461] [&amp;lt;ffff000008649a40&amp;gt;] driver_probe_device+0x1d0/0x2c8&lt;BR /&gt;[ 242.896580] [&amp;lt;ffff000008649bf4&amp;gt;] __driver_attach+0xbc/0xc0&lt;BR /&gt;[ 242.902181] [&amp;lt;ffff000008647b34&amp;gt;] bus_for_each_dev+0x4c/0x98&lt;BR /&gt;[ 242.907867] [&amp;lt;ffff0000086493b8&amp;gt;] driver_attach+0x20/0x28&lt;BR /&gt;[ 242.913294] [&amp;lt;ffff000008648fa8&amp;gt;] bus_add_driver+0x1b8/0x228&lt;BR /&gt;[ 242.918976] [&amp;lt;ffff00000864a578&amp;gt;] driver_register+0x60/0xf8&lt;BR /&gt;[ 242.924576] [&amp;lt;ffff0000084857a8&amp;gt;] __pci_register_driver+0x38/0x40&lt;BR /&gt;[ 242.931321] [&amp;lt;ffff000000f45630&amp;gt;] hif_register_driver+0x18/0x38 [wlan]&lt;BR /&gt;[ 242.938482] [&amp;lt;ffff000000d93d80&amp;gt;] hdd_hif_register_driver+0x30/0x78 [wlan]&lt;BR /&gt;[ 242.946002] [&amp;lt;ffff0000012010b4&amp;gt;] hdd_module_init+0xb4/0x1000 [wlan]&lt;BR /&gt;[ 242.952416] [&amp;lt;ffff000008083a50&amp;gt;] do_one_initcall+0x38/0x130&lt;BR /&gt;[ 242.958110] [&amp;lt;ffff0000081767d8&amp;gt;] do_init_module+0x5c/0x1bc&lt;BR /&gt;[ 242.963714] [&amp;lt;ffff000008139650&amp;gt;] load_module+0x1c50/0x20f8&lt;BR /&gt;[ 242.969315] [&amp;lt;ffff000008139d78&amp;gt;] SyS_finit_module+0xa8/0xc0&lt;BR /&gt;[ 242.975003] [&amp;lt;ffff0000080838d8&amp;gt;] __sys_trace_return+0x0/0x4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone seen this problem?&amp;nbsp; Incidentally, a co-worker independently found the same problem.&amp;nbsp; It would be nice to know if I'm either mis-reading the instructions or the image has an error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Glen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 15:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787781#M122048</guid>
      <dc:creator>glen_m_cornell</dc:creator>
      <dc:date>2018-08-14T15:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787782#M122049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GLENN&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;currently fully functional and tested is&amp;nbsp; Linux L4.9.51 for i.MX 8MQuad GA :&lt;/P&gt;&lt;P&gt;Demo&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_GA&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_GA&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.51_IMX8MQ_GA&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=13376994810717…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;as stated in documentation (Release Notes) on i.MX software web page&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW" title="https://www.nxp.com/support/developer-resources/software-development-tools/i.mx-developer-resources/i.mx-software-and-development-tool:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to attached Release Notes L4.9.88 has i.MX8M support in "Beta Quality".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 23:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787782#M122049</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-14T23:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787783#M122050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am seeing the EXACT same thing!!!&amp;nbsp; Since 4.9.88 is a ga release it was my understanding it was safe to use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx8mqevk:~# [ 242.787553] INFO: task systemd-udevd:2850 blocked for more than 120 seconds.&lt;BR /&gt;[ 242.794685] Tainted: G O 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1&lt;BR /&gt;[ 242.802443] "echo 0 &amp;gt; /proc/sys/kernel/hung_task_timeout_secs" disables this message.&lt;BR /&gt;[ 242.810431] systemd-udevd D 0 2850 1726 0x0000020d&lt;BR /&gt;[ 242.816113] Call trace:&lt;BR /&gt;[ 242.818609] [&amp;lt;ffff000008085e98&amp;gt;] __switch_to+0x90/0xc0&lt;BR /&gt;[ 242.823925] [&amp;lt;ffff000008c653f0&amp;gt;] __schedule+0x178/0x590&lt;BR /&gt;[ 242.829302] [&amp;lt;ffff000008c65844&amp;gt;] schedule+0x3c/0xa8&lt;BR /&gt;[ 242.834341] [&amp;lt;ffff000008c688e4&amp;gt;] schedule_timeout+0x174/0x248&lt;BR /&gt;[ 242.840242] [&amp;lt;ffff000008c67680&amp;gt;] __down+0x58/0x90&lt;BR /&gt;[ 242.845112] [&amp;lt;ffff000008102e74&amp;gt;] down+0x4c/0x68&lt;BR /&gt;[ 242.851364] [&amp;lt;ffff000000ec255c&amp;gt;] HIFExchangeBMIMsg+0x20c/0x330 [wlan]&lt;BR /&gt;[ 242.859362] [&amp;lt;ffff000000ec8ac4&amp;gt;] bmi_download_firmware+0x64/0x130 [wlan]&lt;BR /&gt;[ 242.867967] [&amp;lt;ffff000000e60f9c&amp;gt;] vos_open+0x174/0x6c0 [wlan]&lt;BR /&gt;[ 242.874797] [&amp;lt;ffff000000d1cca4&amp;gt;] hdd_wlan_startup+0x5ac/0x12e0 [wlan]&lt;BR /&gt;[ 242.882346] [&amp;lt;ffff000000ec6cc8&amp;gt;] hif_pci_probe+0x5f8/0x858 [wlan]&lt;BR /&gt;[ 242.888633] [&amp;lt;ffff000008486c4c&amp;gt;] pci_device_probe+0x9c/0x140&lt;BR /&gt;[ 242.894459] [&amp;lt;ffff000008649a40&amp;gt;] driver_probe_device+0x1d0/0x2c8&lt;BR /&gt;[ 242.900629] [&amp;lt;ffff000008649bf4&amp;gt;] __driver_attach+0xbc/0xc0&lt;BR /&gt;[ 242.906271] [&amp;lt;ffff000008647b34&amp;gt;] bus_for_each_dev+0x4c/0x98&lt;BR /&gt;[ 242.911993] [&amp;lt;ffff0000086493b8&amp;gt;] driver_attach+0x20/0x28&lt;BR /&gt;[ 242.917520] [&amp;lt;ffff000008648fa8&amp;gt;] bus_add_driver+0x1b8/0x228&lt;BR /&gt;[ 242.923245] [&amp;lt;ffff00000864a578&amp;gt;] driver_register+0x60/0xf8&lt;BR /&gt;[ 242.928975] [&amp;lt;ffff0000084857a8&amp;gt;] __pci_register_driver+0x38/0x40&lt;BR /&gt;[ 242.936369] [&amp;lt;ffff000000ec6630&amp;gt;] hif_register_driver+0x18/0x38 [wlan]&lt;BR /&gt;[ 242.944255] [&amp;lt;ffff000000d14d80&amp;gt;] hdd_hif_register_driver+0x30/0x78 [wlan]&lt;BR /&gt;[ 242.952412] [&amp;lt;ffff0000011790b4&amp;gt;] hdd_module_init+0xb4/0x1000 [wlan]&lt;BR /&gt;[ 242.958877] [&amp;lt;ffff000008083a50&amp;gt;] do_one_initcall+0x38/0x130&lt;BR /&gt;[ 242.964611] [&amp;lt;ffff0000081767d8&amp;gt;] do_init_module+0x5c/0x1bc&lt;BR /&gt;[ 242.970249] [&amp;lt;ffff000008139650&amp;gt;] load_module+0x1c50/0x20f8&lt;BR /&gt;[ 242.975884] [&amp;lt;ffff000008139d78&amp;gt;] SyS_finit_module+0xa8/0xc0&lt;BR /&gt;[ 242.981603] [&amp;lt;ffff0000080838d8&amp;gt;] __sys_trace_return+0x0/0x4&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 21:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787783#M122050</guid>
      <dc:creator>ryanpabis</dc:creator>
      <dc:date>2018-08-16T21:56:08Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787784#M122051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One other thing I would like to mention now that I realize it's in beta is that sysVinit does not seem to work either.&amp;nbsp; If you comment out the systemd section in fsl-imx-preferred-env.inc the boot times are incredibly slow and you get a lot of udevd errors.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 14:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787784#M122051</guid>
      <dc:creator>ryanpabis</dc:creator>
      <dc:date>2018-08-17T14:46:24Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Panic on Pre-Built Linux SDCard image for MCIMX8M-EVK: Evaluation Kit?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787785#M122052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am seeing the same problem.&amp;nbsp; So I have to use 4.9.51 instead of 4.9.88?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 00:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Panic-on-Pre-Built-Linux-SDCard-image-for-MCIMX8M-EVK/m-p/787785#M122052</guid>
      <dc:creator>lingguan</dc:creator>
      <dc:date>2018-09-11T00:53:08Z</dc:date>
    </item>
  </channel>
</rss>