<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic configure usb phy transmitter control linux kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/configure-usb-phy-transmitter-control-linux-kernel/m-p/787323#M121982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to figure out how to set the USB PHY Tx Control Reg via the device tree. If I have to do from userspace, I have to (ideas on this are appreciated also) but I think I should be able to define a register address (0x020CA010 for the i.MX6) and value to be loaded (0xC). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The POR default value for D_CAL may be insufficient to allow the on-chip PHY to drive a signal w/ all cables.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any assistance is appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Aug 2018 20:46:54 GMT</pubDate>
    <dc:creator>hchristo</dc:creator>
    <dc:date>2018-08-14T20:46:54Z</dc:date>
    <item>
      <title>configure usb phy transmitter control linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/configure-usb-phy-transmitter-control-linux-kernel/m-p/787323#M121982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to figure out how to set the USB PHY Tx Control Reg via the device tree. If I have to do from userspace, I have to (ideas on this are appreciated also) but I think I should be able to define a register address (0x020CA010 for the i.MX6) and value to be loaded (0xC). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The POR default value for D_CAL may be insufficient to allow the on-chip PHY to drive a signal w/ all cables.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any assistance is appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2018 20:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/configure-usb-phy-transmitter-control-linux-kernel/m-p/787323#M121982</guid>
      <dc:creator>hchristo</dc:creator>
      <dc:date>2018-08-14T20:46:54Z</dc:date>
    </item>
    <item>
      <title>Re: configure usb phy transmitter control linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/configure-usb-phy-transmitter-control-linux-kernel/m-p/787324#M121983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harland&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at tx-d-cal optional property in&lt;/P&gt;&lt;P&gt;linux/Documentation/devicetree/bindings/usb/mxs-phy.txt&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/usb/mxs-phy.txt?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/usb/mxs-phy.txt?h=imx_4.1.15_2.0.0_ga"&gt;mxs-phy.txt\usb\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 23:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/configure-usb-phy-transmitter-control-linux-kernel/m-p/787324#M121983</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-16T23:06:36Z</dc:date>
    </item>
  </channel>
</rss>